Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog See what could happen to your design even with a big insulation distance but with too much condensation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Würth Elektronik
  • Date Created: 29 Aug 2023 11:14 AM Date Created
  • Views 950 views
  • Likes 9 likes
  • Comments 1 comment
  • pcb
  • design_tips
  • würth elektronik
  • pcb design
Related
Recommended

See what could happen to your design even with a big insulation distance but with too much condensation

Würth Elektronik
Würth Elektronik
29 Aug 2023
See what could happen to your design even with a big insulation distance but with too much condensation

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

>Video Link<

by Alexandre Chaillet

Between each pole of an electrical product standards give insulation distances. This is mainly called “Creepage and clearance”. This will avoid to have short circuits or breakdown (sparks) in case of overvoltage and thus for all the life of the product.

These distances are influenced by altitude, moisture, pollution and some other parameters.

If designers does not respect these distances, the worst case could happen: they think it is working because when they powered their system everything is ok. It is ok now but for how many time ?

The video shows a special phenomena called “partial discharge”. This could happen when homogeneity of the plastic molding of a connector for example is not properly done and in this case when there is too much moisture (that’s easier to realize :) ).

Between plastic and air or in his case air and moisture, there is a modification a permittivity that under overvoltage (due to thunder for example), a franc spark will not appear but partial discharges just where are small drops. Each small spark will carbonized a little bit the plastic. And spark after spark, it will create a “carbon path” between 2 poles that is comparable to a copper wire (carbon is a conductor for electricity).

And even if the distances was correct between 2 poles, a big sparks occurs that could bring a lot of trouble in your full system !!

The video shows is at very fast but this phenomena could happen in several weeks or months.

You think it is working but it is not !

Respect creepage and clearance standards and avoid low cost material :) 

  • Sign in to reply
  • DAB
    DAB over 3 years ago

    Basic electrical conductivity issues with open air gaps can be quite dangerous.

    There is a reason why most electronic devices have gone to predictable insulation and open contact enclosures.

    In high humidity environments, you must always worry about unintentional paths to ground. Especially with higher voltages.