Würth Elektronik
  • Products & Partners
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog The World's First Peak Current Load SMD Ferrite - The Multilayer Power Suppression Bead
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sleuz
  • Date Created: 23 May 2016 1:40 PM Date Created
  • Views 1473 views
  • Likes 3 likes
  • Comments 2 comments
  • pulse shape
  • current peak
  • filtering
  • electric motor
  • filter;
  • switch mode power supply
  • emc filter
  • peak current
  • pulse current
  • pulse strength
Related
Recommended

The World's First Peak Current Load SMD Ferrite - The Multilayer Power Suppression Bead

sleuz
sleuz
23 May 2016

The World's First Peak Current Load SMD Ferrite - The Multilayer Power Suppression Beadimage

 

 

 

 

ANP028 BY MARKUS HOLZBRECHER

 

 

1. Background

A chip bead ferrite´s inductance is established by using a screen printing process. They are optimised for maximum losses for use as a filter. Therefore, it consists of a nickel-zinc-ferrite mixture and a very fine superimposed inner silver layer with thickness of a few micrometres. This structure makes the classic SMD ferrite more vulnerable for current spikes above its maximum rated current load and in special cases results in degenerative or also immediate destruction of the component.

 

1.1. Application

A typical application is shown in Figure 1. The multilayer ferrite is used as longitudinal filter at the input of the circuit. Due to the low on-resistance of the capacitor, a very high pulse current flows for a short time at switch-on.

This pulse current temporarily loads the SMD ferrite with a multiple of the current that exceeds the maximum specified rated current. In this example, the optimised multilayer ferrite, that is designated by Würth Elektronik eiSos as Multilayer Power Suppression Bead (MPSB), has an impedance of 600 ohms for a maximum permissible rated current load of 2.1 A. The one-time current peak in this constellation has a peak value of approx. 19 A and has an overall

pulse length of 0.8 ms until it has been reduced to the rated current of the circuit.

image

Figure 1: Application with peak current at switch-on (5 A / DIV | 100 μs / DIV)

 

It generally applies for the SMD ferrites that the maximum rated current also defines the maximum current amplitude for temporary load. However, using the new WE-MPSB series with pulse load, multilayer ferrites now also consider the peak current in the data sheet.

 

1.2. Background of the application

Current peaks occur frequently, for example at switch-on of diverse switch mode power supplies and for electric motors. Known applications with recurring pulses are, for example, windscreen wiper motors in vehicles. But also ballasts of luminaires can produce a high current peak at switch-on of the light. In particular, the input capacitor in a switch mode power supply can produce a high peak current that the upstream EMC filter must withstand. Pulses in this context are understood as temporary current peaks with a time limitation less than 8 ms until complete reduction to the DC current of the circuit. The appropriate approach in the search for a common standard for the measurement of pulse load capacity for SMD ferrites has been found in the definition of the melting integral for fuses. A pulse of 8 ms duration, according to the standard, is applied to the fuse to "give the current time" to heat the fuse for the determination of the I²t value of the fuses. If the fuse withstands this, the current is increased until the increase results in destruction of the fuse. In doing so, a pause of 10 s between the pulses is required to give the component the necessary time to regenerate (cooling down).

Würth Elektronik eiSos has developed an adapted test routine based on this fuse standard for the multilayer ferrites. Based on the 8 ms pulse, current with increasing pulses is applied to the multilayer ferrite until destruction. The components are loaded with iteratively increasing pulse currents starting from 1 A. The pulse rectangle shown in Figure 2 was selected as pulse shape for all tests as this loads the component with the highest possible energy for the pulse duration ݈although it will only very rarely be applicable in practice at switch-on.

 

image

Figure 2: Possible pulse shapes at switch-on

 

2. Pulse Strength

In comparison with the fuse, it is not possible for the multilayer SMD ferrite to specify any generally applicable formula with which conclusions can be drawn for the various current peaks for different pulse lengths using the calculation of the melt integral. The empirically determined data sheet values can be traced back to long term test series with different parameters.

The following shows an example for clarification of the non-applicability of the melt integral for the multilayer ferrites using the example of the article 74279220601 (Z = 600 Ω, IR = 2.1 A, RDC,typ = 43 mΩ).

The WE-MPSB has a maximum peak current load capability of 18 A with a pulse length of 8 ms. This produces an I²t value of 2.592 A²ms (18 A @ 8 ms (5 sec pause, 24 °C) I²t = 2.592 A²s).

 

The following result is obtained, if the current for a pulse length of 2 ms based on the I²t value for 8 ms is calculated:

 

image

 

However, the data sheet value shown in Figure 3 is specified as max. 24 A. The calculated I²t value deviates significantly from the measured values. Consequently, due to this different behaviour of the SMD ferrite from the fuse, it is not possible to apply the known calculation of the melt integral I²t to a multilayer ferrite.

 

image

Figure 3: Specified peak current load capability

 

 

 

2.1. Optimisations for the WE-MPSB

Due to its silver layers with a thickness of only 8 - 20 μm, the multilayer ferrite is not constructively designed for high pulse currents. Würth Elektronik eiSos has developed a new, optimised design with a perfect mixture of high currents, up to 75% smaller RDC and as high as possible impedance over the complete frequency spectrum. Depending on the impedance and current level, the optimum design is used individually for each article.

 

2.2. Definition of the pulse strength

The pulse strength is considered in more detail using the example of the article  7427922060174279220601 The current pulse curve shown in Figure 5a shows the maximum permitted peak current for the respective tested pulse lengths The tested range covers the time range of 0.5 ms to 8 ms pulse length This curve is measured individually for each article and is only permissible for any consideration with one-time pulse

 

imageimage

Figure 4: Display of the current as dependence on pulse length and the number of pulses

 

The consideration of the permitted maximum pulse current visible in Figure 4b for a repeating pulse is possible using the second curve in the data sheet. This curve is a limit value consideration of the maximum peak current for repeating pulses. A maximum pulse length of 8 ms was selected for determination of the curve.

 

2.3. Tnt triangle influencing factors

The influencing factors are

  • The pulse lengths t that are tested as standard from 0.5 ms to 8 ms. The longer the pulse, the smaller is the maximum pulse load capability.
  • The number of pulses that are tested from 10 to 100,000 pulses (see Figure 5b). The maximum permissible pulse load capability drops as the pulse frequency increases.
  • The temperature should be noted as third reducing influencing factor; as the temperature increases, RDC increases which results in further reduction of the maximum pulse load.

 

Each of these interlinked systems is burdened with the dependency on the underlying pause between the individual pulses. In order to carry out an analysis of the linked system with a smaller pause time, it is necessary

to measure the temperature [T], pulse repetitions [n] and pulse length [t] influencing factors again.

 

2.4. Comparison of the WE-MPSB with the WE-CBF series

The objective of the WE-MPSB series is to achieve a comparable impedance as for the WE-CBF Series with additionally optimised resistance and load capability with pulse currents.

Using the example of the 600 Ω models in size 0805 shown in Figure 5, the WE-MPSB series with almost the same impedance has a higher rated current due to the smaller resistance.

 

imageimage

Figure 5: Comparison of the impedance and rated current load capability of the WE-CBF and WE-MPSB 600 Ω

 

The WE-MPSB series has significantly higher pulse load capability than a comparable WE-CBF Series model. Figure 6 shows the maximum pulse level of the 600 Ω model on the graph on the left and the maximum pulse level of the comparable WE-MPSB 600 Ω model on the graph on the right.

 

image

Figure 6: Comparison of the different pulse load capability of the WE-CBF and WE-MPSB series

 

3. Summary

The WE-MPSB series has been developed based on the requirements of circuits that load the multilayer ferrites with temporary peak currents exceeding the rated current. The maximum pulse load capabilities of the multilayer ferrites have been determined by measurement using an in-house test routine that is different from that of the fuses. In comparison with existing multilayer structures, the layer structure has been optimised to generate higher current load capability using lower resistances. The WE-MPSB series is thus ideally suitable for use in circuits with pulse currents.

 

IMPORTANT NOTICE

The Application Note is based on our knowledge and experience of typical requirements concerning these areas. It serves as general guidance and should not be construed as a commitment for the suitability for customer applications by Würth Elektronik eiSos GmbH & Co. KG. The information in the Application Note is subject to change without notice. This document and parts thereof must not be reproduced or copied without written permission, and contents thereof must not be imparted to a third party nor be used for any unauthorized purpose.

Würth Elektronik eiSos GmbH & Co. KG and its subsidiaries and affiliates (WE) are not liable for application assistance of any kind. Customers may use WE’s assistance and product recommendations for their applications and design. The

responsibility for the applicability and use of WE Products in a particular customer design is always solely within the authority of the customer. Due to this fact it is up to the customer to evaluate and investigate, where appropriate, and decide whether the device with the specific product characteristics described in the product specification is valid and suitable for the respective customer application or not.

The technical specifications are stated in the current data sheet of the products. Therefore the customers shall use the data sheets and are cautioned to verify that data sheets are current. The current data sheets can be downloaded at

www.we-online.com. Customers shall strictly observe any product-specific notes, cautions and warnings. WE reserves the right to make corrections, modifications, enhancements, improvements, and other changes to its products and services.

WE DOES NOT WARRANT OR REPRESENT THAT ANY LICENSE, EITHER EXPRESS OR IMPLIED, IS GRANTED UNDER ANY PATENT RIGHT, COPYRIGHT, MASK WORK RIGHT, OR OTHER INTELLECTUAL PROPERTY RIGHT RELATING TO ANY COMBINATION, MACHINE, OR PROCESS INWHICHWE PRODUCTS OR SERVICES ARE USED. INFORMATION PUBLISHED BY WE REGARDING THIRD-PARTY PRODUCTS OR SERVICES DOES NOT CONSTITUTE A LICENSE FROM WE TO USE SUCH PRODUCTS OR SERVICES OR A WARRANTY OR ENDORSEMENT THEREOF.

WE products are not authorized for use in safety-critical applications, or where a failure of the product is reasonably expected to cause severe personal injury or death. Moreover, WE products are neither designed nor intended for use in

areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc. Customers shall inform WE about the intent of such usage before design-in stage. In certain customer applications requiring a very high level of safety and in which the malfunction or failure of an electronic component could endanger human life or health, customers must ensure that they have all necessary expertise in the safety and regulatory ramifications of their applications.

Customers acknowledge and agree that they are solely responsible for all legal, regulatory and safety-related requirements concerning their products and any use ofWE products in such safety-critical applications, notwithstanding any applicationsrelated information or support that may be provided by WE. CUSTOMERS SHALL INDEMNIFY WE AGAINST ANY DAMAGES ARISING OUT OF THE USE OF WE PRODUCTS IN SUCH SAFETY-CRITICAL APPLICATIONS.

 

USEFUL LINKS

Application Notes:

http://www.we-online.com/app-notes

REDEXPERT Design Tool: http://www.we-online.com/redexpert

Toolbox: http://www.we-online.com/toolbox

Product Catalog: http://katalog.we-online.de/en/

 

CONTACT INFORMATION

Würth Elektronik eiSos GmbH & Co. KG

Max-Eyth-Str. 1, 74638 Waldenburg, Germany

Tel.: +49 (0) 7942 / 945 – 0

Email: appnotes@we-online.de

Web: http://www.we-online.com

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Interesting device. Have they run any lifetime tests? I am curious to see if the parameters change over time. DAB
  • sleuz
    sleuz over 10 years ago in reply to DAB

    Hi DAB

     

    Yes, lifetime tests have been done.

    We ran 100k pulses on the component over a 10-day duration.

     

    And yes, the parameters can change. The RDC can be increasing. Acceptable is an increase below 8% of the RDC.

     

    Hope this helps.

     

     

    Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Interesting device.

     

    Have they run any lifetime tests?

    I am curious to see if the parameters change over time.

     

    DAB