PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs Scrutinize my FPGA PCB Layout
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 Jul 2022 3:23 PM Date Created
  • Views 7988 views
  • Likes 12 likes
  • Comments 33 comments
  • bga
  • pcb
  • fpga
Related
Recommended

Scrutinize my FPGA PCB Layout

shabaz
shabaz
12 Jul 2022


Since cstanton alerted everyone to the PCB Forum, I thought I’d make use of it and try to get some help.

I’ve never done a ball grid array (BGA) layout, and I wished to have an FPGA board that I’d created myself, for some experimentation and general FPGA learning.

I’m planning to create a board using a Lattice Semiconductor part, because it is available in a sensible TQFP package which I am comfortable with. However, I thought I’d also give a Xilinx part a shot too, but it’s only offered in physically smaller packages; the simplest of which is what Xilinx calls an FTGB196 package. The part I’m using is Xilinx XC7S15 (PDF data sheet overview). However, since I've started the design, the chip is unobtainable! nevertheless, I thought it would be still useful to continue the design, and build it when the parts become available again.

image

The balls are spaced 1.0 mm apart, so it’s perhaps as friendly as such a type of package can get, I guess. I wish to use this with a 4-layer board, using low-cost PCB services from China.

I’ve gone with the following pad dimensions:

image

Here is each layer of the board, in the FPGA region.

image

This is what the board currently looks like zoomed-out(ground plane not shown), everything is still in the process of being routed, but basically I’m using layer 2 for ground plane, and layer 3 has some power planes.

image

Top and bottom layers (red and blue respectively) are for signal traces, and for all DC-DC converter traces, so I’ll use lots of vias when I pass the power to the power plane layer.

This is what the traces look like underneath the FPGA:

image

I need three supply voltages, and I’ve routed the DC-DC converter sections as visible in the screenshot above, but they still need to be positioned better. There is a basic power sequencing IC, not laid out on the PCB yet, it is LM3881, which too is now hard to obtain, but I have a few for now. Perhaps I can swap that out to a microcontroller if the LM3881 is inadequate, but it seemed fine. There's no JTAG programmer on-board; instead there will be a socket for the Xilinx programmer, just to keep things fairly minimal currently.

For additional memory, the FPGA is connected to a RAM chip (SRAM) on the right side. This is easier than DRAM. It’s messily routed currently.

I still need to route most of the signals in the IO banks; all that is done is the supplies, and the IO used for the SRAM.

Schematic

The schematics are incomplete, I still need to add connectors for the I/O. The project will be ported to KiCAD ideally (I started in EAGLE, but now I believe I can import it into KiCAD 6). The three sheets are shown below.

image

image

image

 

Anyway, that’s as far as I have got. Feel free to discuss/criticize etc : ) I’ll try to take on board any comments, however, I don’t want to re-do too much of it unless there’s a functional risk of it not working – for instance, some of the design admittedly looks anachronistic, like the massive DC-DC converters, and relatively physically large SRAM chip, but I really didn’t want to use tiny package devices except where I have no choice, i.e. the FPGA. I’d rather make the rest of it as large and serviceable as possible.

Thanks for reading!

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 4 years ago +1
    Checking if rachaelp can chime in. She's been doing FPGA design and BGA fanout as a job.
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago in reply to shabaz +1
    Hello shabaz, Thanks for the updated info. to see which I/O Vivado preferred, and then played with moving some around in the pin assignment file to see if Vivado was still ok with them, because I…
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    (can't edit). Maybe this is an opportunity to try the EAGLE import, since KiCAD has that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    The length matching capability in KiCAD is nicer than in EAGLE, but EAGLE can do it too. Unfortunately I started this project last year prior to learning KiCAD. I would have liked to start it in KiCAD. I'm not capable of routing in one go, usually I rip up traces for a second pass, but I suspect I'll need to rip traces several times before I hit on the ideal distance for the traces to be matched to. That will be interesting for sure... I bet there's a trick to it that I need to discover. Maybe the trick is to deliberately put a bit more distance between the FPGA chip and the SRAM, so that there is more real-estate for the traces that need more wiggles!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    the FPGA is connected to a RAM chip (SRAM) on the right side. This is easier than DRAM. It’s messily routed currently.

    You may have to length-match the RAM data lines (it may limit the achievable data rate if you don't), and the sets of balanced analogue inputs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    That would be very helpful! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to dougw

    Hi Doug,

    Thanks for the link! Very interesting article, and that's an impressively tiny part! Although the Xilinx chip has twice as many pads, the Xilinx part is a lot larger, whereas they had to resort to via-in-pad due to the tininess, With via-in-pad I cannot use the normal China PCB service, so instead, I placed separate vias, which isn't as good, but cheaper. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>