PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum What Do You Do With Bad/Extra PCBs?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 162 subscribers
  • Views 3759 views
  • Users 0 members are here
  • mistakes
  • pcb
  • sustainability
  • learning
Related

What Do You Do With Bad/Extra PCBs?

Gough Lui
Gough Lui over 4 years ago

Recently, I posted this blog about inexpensive PCBs being a boon for hobbyists. I myself have benefited greatly from being able to turn my designs into reality and learn-as-I-go.

But there is a flip-side to everything - as it is so cheap, I often do end up making mistakes (unintentionally, of course) and they get manufactured and shipped all the way to me. Other times, the minimum order quantity means I have an extra few boards of a design I might not ever rebuild as it may have deficiencies or is just a one-off design to solve a one-off problem.

That brings me to the obvious question - what does one do with this ever-growing mountain of PCBs filled with paints, copper, fibreglass, etc?

Sometimes I have "bodge-wired" elements from boards to turn them into inelegant breakout boards, rewired certain sections to turn them into a new project. Or perhaps used them as spacers/shims for wobbly tables, as art, or as a piece of scrap to protect my bench. But even these applications quickly run out if one makes quite a few boards ...

So is there a better thing to do with them? I'm not sure they're really recycled? I know ENIG/ENEPIG boards often get coveted by those looking to extract gold, but what about the humble low-cost HASL boards? It would just feel a bit of a shame to be contributing to the "e-waste" problem, even if it wasn't immediately financially ruinous.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +3
    I keep them in the "job box" for that project. I have job boxes going back 20 years. Just recently someone asked me if I could help with a board I designed 10 years ago and I was able to offer them…
  • misaz
    misaz over 4 years ago +3
    Last time I reused bad PCBs for evaluating SMD (0603 in my case) LEDs. I solder LED instead of decoupling capacitor and pinhead for power pins. Then I was able to connect wires between power pinheads and…
  • Jan Cumps
    Jan Cumps over 4 years ago +2
    The ones that can be bodged to perform well, I usually keep. All other ones get dumped. I am not a museum.
Parents
  • shabaz
    shabaz over 4 years ago

    I have a few in the shed to use as scrap material or shim, but the rest get junked (I might only use a couple from the 5 or so that the PCB factory will send).

    It's very rare a board is completely unusable, ordinarily it can be fixed with some bodge wires. The worst I recall was around 2014, so 8 years ago, when I accidentally numbered a high density (0.4 mm pitch) connector with pins ordered like an IC, but they were supposed to be odd numbers and even numbers on opposite sides! I couldn't stop the soldering of the parts (the time was already scheduled, it had to be done then), and bodge wires would have been a pain with the large volume of connections on the 5 prototype boards, so I had to then design a "correcting board" to take the messed up pinout using a mating connector, and then fix it on another connector! Total mess. Since then, I'm a lot more careful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to shabaz

    I do like the "bodge adapter" idea ... much better than bodge wires for that kinda issue ... I once mucked up MOSFET connections on a schematic which translated into PCB carnage. As they were SOT-23, I didn't fancy trying to bodge wire 10 of those in close confines and just span a new board. Been feeling a bit guilty ever since and keep telling myself to sleep on a design before sending it in, in case I figure out something is wrong in that time.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 4 years ago in reply to shabaz

    I do like the "bodge adapter" idea ... much better than bodge wires for that kinda issue ... I once mucked up MOSFET connections on a schematic which translated into PCB carnage. As they were SOT-23, I didn't fancy trying to bodge wire 10 of those in close confines and just span a new board. Been feeling a bit guilty ever since and keep telling myself to sleep on a design before sending it in, in case I figure out something is wrong in that time.

    - Gough