PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Forum What Do You Do With Bad/Extra PCBs?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 135 subscribers
  • Views 2997 views
  • Users 0 members are here
  • mistakes
  • pcb
  • sustainability
  • learning
Related

What Do You Do With Bad/Extra PCBs?

Gough Lui
Gough Lui over 3 years ago

Recently, I posted this blog about inexpensive PCBs being a boon for hobbyists. I myself have benefited greatly from being able to turn my designs into reality and learn-as-I-go.

But there is a flip-side to everything - as it is so cheap, I often do end up making mistakes (unintentionally, of course) and they get manufactured and shipped all the way to me. Other times, the minimum order quantity means I have an extra few boards of a design I might not ever rebuild as it may have deficiencies or is just a one-off design to solve a one-off problem.

That brings me to the obvious question - what does one do with this ever-growing mountain of PCBs filled with paints, copper, fibreglass, etc?

Sometimes I have "bodge-wired" elements from boards to turn them into inelegant breakout boards, rewired certain sections to turn them into a new project. Or perhaps used them as spacers/shims for wobbly tables, as art, or as a piece of scrap to protect my bench. But even these applications quickly run out if one makes quite a few boards ...

So is there a better thing to do with them? I'm not sure they're really recycled? I know ENIG/ENEPIG boards often get coveted by those looking to extract gold, but what about the humble low-cost HASL boards? It would just feel a bit of a shame to be contributing to the "e-waste" problem, even if it wasn't immediately financially ruinous.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    I keep them in the "job box" for that project. I have job boxes going back 20 years. Just recently someone asked me if I could help with a board I designed 10 years ago and I was able to offer them…
  • misaz
    misaz over 3 years ago +3
    Last time I reused bad PCBs for evaluating SMD (0603 in my case) LEDs. I solder LED instead of decoupling capacitor and pinhead for power pins. Then I was able to connect wires between power pinheads and…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    The ones that can be bodged to perform well, I usually keep. All other ones get dumped. I am not a museum.
  • Jan Cumps
    Jan Cumps over 3 years ago

    The ones that can be bodged to perform well, I usually keep. All other ones get dumped. I am not a museum.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    I have a few in the shed to use as scrap material or shim, but the rest get junked (I might only use a couple from the 5 or so that the PCB factory will send).

    It's very rare a board is completely unusable, ordinarily it can be fixed with some bodge wires. The worst I recall was around 2014, so 8 years ago, when I accidentally numbered a high density (0.4 mm pitch) connector with pins ordered like an IC, but they were supposed to be odd numbers and even numbers on opposite sides! I couldn't stop the soldering of the parts (the time was already scheduled, it had to be done then), and bodge wires would have been a pain with the large volume of connections on the 5 prototype boards, so I had to then design a "correcting board" to take the messed up pinout using a mating connector, and then fix it on another connector! Total mess. Since then, I'm a lot more careful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to Jan Cumps

    Fair enough ... is there any specific way that you use to dump them? Or do you just throw it into the household rubbish collection?

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to shabaz

    I do like the "bodge adapter" idea ... much better than bodge wires for that kinda issue ... I once mucked up MOSFET connections on a schematic which translated into PCB carnage. As they were SOT-23, I didn't fancy trying to bodge wire 10 of those in close confines and just span a new board. Been feeling a bit guilty ever since and keep telling myself to sleep on a design before sending it in, in case I figure out something is wrong in that time.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    I keep my extra PCBs. They pretty much all work, but I buy them 10 at a time and only use about 20% in the project they were designed for. I find a lot of uses for spare PCBs - structural components in mechanical builds, breakout boards, insulator material, conductor material, prototyping, etc.

    I still collect it way faster than I use it. It is useful to design your cards for re-use, add breakout pads and connectors, connector adapter circuitry, structural mounting holes, prototype areas, etc.

    I have coined a term for it - DFR "design for re-purpose". Maybe I'll do a blog on it sometime.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago

    I’ve given quite a few sets of PCBs to the museum to put in their shop and sell as coasters.  TBH, they’re a bit sloppy for that purpose but they actually do sell, albeit slowly.  Those that I’ve used and scavenged parts off I would dump in the e-waste recycling.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    When I have one of these botched PCB sessions I first weep, gnash my teeth, swear (A LOT, depending on the faux pas !) and at times go outside to experiment with the board's aerodynamic properties.

    I tend to hang onto them, moving them from location to location hoping to discover something they can be used for in order to gain some absolution. Creating the occasional bullet-holed riddled mistake helps but is not sustainable.

    This a great question to which I do not have an answer outside of the emotional release. Hanging on to them because hope springs eternal is usually the case.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    I keep them in the "job box" for that project.

    I have job boxes going back 20 years.

    Just recently someone asked me if I could help with a board I designed 10 years ago and I was able to offer them 2 half built examples.

    Every now and again I pillage the boxes for parts and very occasionally a board (rather than just the parts) is actually useful.

    More often I use them as spacers, glue stirrers etc.

    Eventually, when I have enough, I'll send them along with other E-waste to be re-processed but its not economical to get rid of less than 100kg at a time.

    I use PCBCART who have a delightful habbit of (almost) always sending more boards than you asked for or paid for.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Gough Lui

    In the household bin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 3 years ago in reply to michaelkellett

    I tend to do the same, but I don't have so many PCB projects that this is a problem. I think that it's definitely worth keeping one of each example - even if it's just a reminder of what you worked on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>