PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Good PCB design practices
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 161 subscribers
  • Views 3526 views
  • Users 0 members are here
  • kicad
  • pcb
  • pcb prototyping
  • pcb design
Related

Good PCB design practices

rsjawale24
rsjawale24 over 3 years ago

I'm working on an oscillator design using an off the shelf integrated circuit-based oscillator.

I have made two large gnd planes in the PCB, the top layer as well as the bottom layer. 

Is this a good practice esp. for making PCBs for applications like oscillators?

I have also added plenty of vias to connect the two layers. 

I just wanted suggestions (if any) before I send the PCB for fabrication. 

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    If you have top and bottom ground plane, it is essential to stitch them together with a lot of vias, so that is good. They should be positioned all the way up to the edge of the board. Also more vias at…
  • shabaz
    shabaz over 3 years ago in reply to shabaz +2
    EDIT: In fact, it looks like your project is doing a similar thing to mine, except for the sharper edges. Also, I'm using a multi-position slide-switch instead of a DIP switch, but it's all fairly similar…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    Some more ideas: 1) If you rotate C2 clockwise 90deg and move it closer to pins 1,2 of U2, the power trace could stay on the top layer. Also the power trace should be much thicker, 1mm (25 mil) as a…
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    If you have top and bottom ground plane, it is essential to stitch them together with a lot of vias, so that is good. They should be positioned all the way up to the edge of the board. Also more vias at the top copper island between SW1 and U2.

    For your design, I assume the clock signal is from U2 pin5 the SMA connector. If you are using a 50 Ohm coax cable, the trace on the board should be 50 Ohm impedance as well. The ground plane on the bottom under the trance is absolutely required to make it a microstrip conductor for a controlled impedance signal. The ground plane on top is tricky in this case. In your layout, it is close enough to the signal trance to make it a co-planar waveguide. If you want to top ground plane have no impact on your impedance calculation it should be pulled bck from the trace >5x trace height over the bottom ground plane. 

    Saturn PCB calculator is a good tool for impadance calculation.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to wolfgangfriedrich

    Thanks, I'll add more vias new SW1 and U2.
    No, I'm not looking for 50ohms impedance match. I'm aware about the transmission line designs Slight smile

    This osc. LTC1799 goes max upto 33MHz. I'll be using it just as a signal generator and to experiment with my new USB oscilloscope.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsjawale24
    rsjawale24 over 3 years ago in reply to wolfgangfriedrich

    Thanks, I'll add more vias new SW1 and U2.
    No, I'm not looking for 50ohms impedance match. I'm aware about the transmission line designs Slight smile

    This osc. LTC1799 goes max upto 33MHz. I'll be using it just as a signal generator and to experiment with my new USB oscilloscope.