PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Good PCB design practices
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 161 subscribers
  • Views 3526 views
  • Users 0 members are here
  • kicad
  • pcb
  • pcb prototyping
  • pcb design
Related

Good PCB design practices

rsjawale24
rsjawale24 over 3 years ago

I'm working on an oscillator design using an off the shelf integrated circuit-based oscillator.

I have made two large gnd planes in the PCB, the top layer as well as the bottom layer. 

Is this a good practice esp. for making PCBs for applications like oscillators?

I have also added plenty of vias to connect the two layers. 

I just wanted suggestions (if any) before I send the PCB for fabrication. 

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    If you have top and bottom ground plane, it is essential to stitch them together with a lot of vias, so that is good. They should be positioned all the way up to the edge of the board. Also more vias at…
  • shabaz
    shabaz over 3 years ago in reply to shabaz +2
    EDIT: In fact, it looks like your project is doing a similar thing to mine, except for the sharper edges. Also, I'm using a multi-position slide-switch instead of a DIP switch, but it's all fairly similar…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    Some more ideas: 1) If you rotate C2 clockwise 90deg and move it closer to pins 1,2 of U2, the power trace could stay on the top layer. Also the power trace should be much thicker, 1mm (25 mil) as a…
Parents
  • shabaz
    shabaz over 3 years ago

    For RF boards usually there would be vias right at the edge of the board as Wolfgang says, because the electric field can be terminated toward it (probably requires a textbook for a better explanation!). 

    The chip you're using (LTC1799) doesn't have particularly fast edges or clock rate, so I think you'll be OK, but worth adding in vias. 

    If it helps, there's a project using that chip here:  Building a Fast Edge Square Wave Generator 

    (the output was connected to buffers to sharpen up the edges for that project). As you can see, I did as Wolfgang refers to, with the top ground plane pulled back where it wasn't needed. The top plane is really useful for preventing the board from warping, but occasionally gets in the way. I have the tiniest 50 ohm trace because the rest of it wasn't 50 ohm characteristic impedance.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago in reply to shabaz

    I agree with everything shabaz said. If fact, after seeing his board, you should check your through holes of the SMA footprint if they match the connector that you have selected. Their diameter looks very small for every SMA part I have ever seen. But then, maybe it is not SMA; could also be right angle BNC and my concern is not valid at all. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to wolfgangfriedrich

    Yes, I have used a BNC connector

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsjawale24
    rsjawale24 over 3 years ago in reply to wolfgangfriedrich

    Yes, I have used a BNC connector