Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Add a second Task to the Multi-core FreeRTOS SMP Project with the Raspberry Pi Pico: ADC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 29 Sep 2022 4:57 PM Date Created
  • Views 1963 views
  • Likes 7 likes
  • Comments 1 comment
Related
Recommended
  • raspberry
  • pico_freertos_smp
  • pico
  • smp
  • freertos

Add a second Task to the Multi-core FreeRTOS SMP Project with the Raspberry Pi Pico: ADC

Jan Cumps
Jan Cumps
29 Sep 2022
Add a second Task to the Multi-core FreeRTOS SMP Project with the Raspberry Pi Pico: ADC

FreeRTOS Symmetric Multiprocessing (SMP) is a recent version of the RTOS that can schedule tasks across multiple controller cores. It's currently in test phase, and they have a version for the RP2040. In this blog post, I add a second task to my own little SMP project in VSCode: measure the on-package temperature.
image
image source: online AI image creator using the keywords raspberry pico temperature
Prerequisite is that you are able to run the single task blinky project from the previous post.

Create a Temperature task

On the Pico, ADC channel 4 is used to measure onboard temperature. In the pico-examples distribution, there is a ready-to-use temperature project. I've translated it into a FreeRTOS task.

#include "hardware/adc.h"

#define mainTEMPERATURE_TASK_PRIORITY (tskIDLE_PRIORITY +1)
#define mainTEMPERATURE_TASK_FREQUENCY_MS (5000 / portTICK_PERIOD_MS)

#define TEMPERATURE_UNITS 'C'

static void prvTemperatureTask(void *pvParameters)
{
    (void)pvParameters;
    TickType_t xNextWakeTime;

    /* Initialise xNextWakeTime - this only needs to be done once. */
    xNextWakeTime = xTaskGetTickCount();

    /* Enable onboard temperature sensor and
     *   select its channel (do this once for efficiency, but beware that this
     *   is a global operation). */
    adc_set_temp_sensor_enabled(true);
    for (;;)
    {
        // TODO set a semaphore

        // switch to the temperature mux if needed
        if (adc_get_selected_input() != 4)
        {
            adc_select_input(4);
        }
        float temperature = read_onboard_temperature(TEMPERATURE_UNITS);
        printf("Onboard temperature = %.02f %c\n", temperature, TEMPERATURE_UNITS);
        xTaskDelayUntil(&xNextWakeTime, mainTEMPERATURE_TASK_FREQUENCY_MS);
    }
}

The read_onboard_temperature() function is exactly the same as in pico-examples:

/* References for this implementation:
 * raspberry-pi-pico-c-sdk.pdf, Section '4.1.1. hardware_adc'
 * pico-examples/adc/adc_console/adc_console.c */
float read_onboard_temperature(const char unit) {
    
    /* 12-bit conversion, assume max value == ADC_VREF == 3.3 V */
    const float conversionFactor = 3.3f / (1 << 12);

    float adc = (float)adc_read() * conversionFactor;
    float tempC = 27.0f - (adc - 0.706f) / 0.001721f;

    if (unit == 'C') {
        return tempC;
    } else if (unit == 'F') {
        return tempC * 9 / 5 + 32;
    }

    return -1.0f;
}

I had two places in the code where I could enable the adc peripherals. I could do it in the initialisation part of the temperature task, or in the existing prvSetupHardware() procedure. I chose the procedure, because I prefer a style where hardware initialisation is part of the board setup.

static void prvSetupHardware( void )
{
    stdio_init_all();
    gpio_init(PICO_DEFAULT_LED_PIN);
    gpio_set_dir(PICO_DEFAULT_LED_PIN, 1);
    gpio_put(PICO_DEFAULT_LED_PIN, 0);
    // Initialize hardware AD converter, for the temperature sensor
    adc_init();
}

The last line is my addition. This code is called at the start of main(). That's also where the new task gets registered:

int main( void )
{
    /* Configure the hardware ready to run the demo. */
    prvSetupHardware();

    xTaskCreate(prvBlinkTask, "blink", configMINIMAL_STACK_SIZE, NULL, mainBLINK_TASK_PRIORITY, NULL);
    xTaskCreate(prvTemperatureTask, "temperature", configMINIMAL_STACK_SIZE, NULL, mainTEMPERATURE_TASK_PRIORITY, NULL);

    /* Start the tasks and timer running. */
    vTaskStartScheduler();
    // ...

Not Thread Safe

In the temperature task, you'll see a TODO: set a semaphore. In a multi-threaded system, you have to guard resources that you're using. In my case, I'm switching the ADC channel, then reading its value. If another task switches the channel in the meantime, I'm reading a wrong value. Or if another task is busy reading another channel, I interfere with its operation. This is not an issue in the current design, because there's only one adc task. But it's good to be forward looking. That's why in the next post, I'll add a guard around the adc. In FreeRTOS lingo: a semaphore.

image

Show All Blog Posts

  • Sign in to reply
  • DAB
    DAB over 4 years ago

    Good walk through Jan.