• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Add external SPI Flash Memory to Raspberry Pico - 3: structure the Flash c++ class before proceding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Dec 2022 12:06 PM Date Created
  • Views 1732 views
  • Likes 5 likes
  • Comments 1 comment
Related
Recommended
  • pico
  • pico_m25
  • pico_eurocard

Add external SPI Flash Memory to Raspberry Pico - 3: structure the Flash c++ class before proceding

Jan Cumps
Jan Cumps
2 Dec 2022
Add external SPI Flash Memory to Raspberry Pico - 3: structure the Flash c++ class before proceding

A projects to learn the SPI API of the RP2040 C SDK, and to use it to control an external Flash IC. In this post, I refine the m25 c++ class from previous post. 

image

What will Change and What Not?

The class initially only knew the SPI device and chip select pins. SPI and pin initialisation was done in main().

// m25.h
class m25 {
public:
  m25(spi_inst_t * spi, uint cs) : _spi(spi), _cs(cs) {}
  // ...
}

// ...

// main file:
void setSPI() {
    spi_init(M25_SPI, 1000 * 1000);
    gpio_set_function(M25_SPI_RX_PIN, GPIO_FUNC_SPI);
    gpio_set_function(M25_SPI_SCK_PIN, GPIO_FUNC_SPI);
    gpio_set_function(M25_SPI_TX_PIN, GPIO_FUNC_SPI);

    // Chip select is active-low, so we'll initialise it to a driven-high state
    gpio_init(M25_SPI_CSN_PIN);
    gpio_put(M25_SPI_CSN_PIN, 1);
    gpio_set_dir(M25_SPI_CSN_PIN, GPIO_OUT);
}


int main() {
    // ...
    setSPI();
    eeprom = new m25(M25_SPI, M25_SPI_CSN_PIN);
    // ...

Constants used in the c++ class were done with #define.

#define FLASH_CMD_RDID         0x9F

I will not (yet) create a more generic spi class, and derive from that (or use it). I hope that one day some volunteer writes a good c++ library for the RP2040. I will then piggyback on that.

Why and How?

"Why" for a few reasons, and they are all debatable.

The define turns into a private class-scope enum. I've also given it the right type.  It belongs to the class, does not have to be used outside it, and this is now also where it's defined.
I could have used a class constant definition, but chose for enum because there will be a number of them that are all related.

I've decided to let the class handle all pins. And then learn the class how to initialise them, instead of doing that in main(). Exception: I haven't told the class about the ~hold and ~write pins yet. I'll do that when (if) I introduce support for protection.

This is how the changed parts of m25.h looks like:

class m25 {
public:
  m25(spi_inst_t * spi, uint sclk, uint mosi, uint miso, uint ncs) : 
    spi(spi), sclk(sclk), mosi(mosi), miso(miso), ncs(ncs) {}
  /// ...
  uint8_t init();
  uint8_t rdid();
  uint8_t rdsr();

private:
  enum commands : uint8_t { 
    RDID = 0x9F,
    RDSR = 0x05 };
  // ...
  uint sclk, mosi, miso, ncs;

And m25.cpp:

// ...

uint8_t m25::init() {
    spi_init(spi, 1000 * 1000);
    gpio_set_function(miso, GPIO_FUNC_SPI);
    gpio_set_function(sclk, GPIO_FUNC_SPI);
    gpio_set_function(mosi, GPIO_FUNC_SPI);

    // Chip select is active-low, so we'll initialise it to a driven-high state
    gpio_init(ncs);
    gpio_put(ncs, 1);
    gpio_set_dir(ncs, GPIO_OUT);
    return 0U; 
}

uint8_t m25::rdid() {
    uint8_t retval = 0U;
    uint8_t buf[3];
    // command
    uint8_t cmdbuf[] = {
            RDID,
    };
    setDataBits(8);
    select();
    spi_write_blocking(spi, cmdbuf, 1);
    spi_read_blocking(spi, 0, buf, 1); // Manufacturer Identification
    spi_read_blocking(spi, 0, buf + sizeof buf[0], 2); // Device Identification (Memory Type || Memory Capacity)
    deselect();
    return retval;
}

uint8_t m25::rdsr() {
    uint8_t retval = 0U;
    uint8_t buf[1];
    // command
    uint8_t cmdbuf[] = {
            RDSR,
    };
    this->setDataBits(8);
    this->select();
    spi_write_blocking(spi, cmdbuf, 1);
    spi_read_blocking(spi, 0, buf, 1); // Read Status Register
    this->deselect();
    return retval;
}

The main():

int main() {
    m25 *eeprom = nullptr;
    setGPIO();

    eeprom = new m25(M25_SPI, 
      M25_SPI_SCK_PIN, M25_SPI_TX_PIN, M25_SPI_RX_PIN, M25_SPI_CSN_PIN);
    uint8_t retval;
    retval = eeprom->init();
    retval = eeprom->rdid();
    retval = eeprom->rdsr();
    delete eeprom;
    eeprom = nullptr;
// ...

As usual, the VSCode project (also directly importable into CLion - see shabaz ' comment in post 2). It contains the compiled uf2, if you're not into building from source:

spi_flash_20221202.zip

link to all posts in this series

  • Sign in to reply
  • flyingbean
    flyingbean over 3 years ago

    I am going to follow your blogs on this topic. Need to make time for that.