• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Android controlled Raspberry Pi and Arduino Robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: anujaapte
  • Date Created: 15 Aug 2014 6:52 PM Date Created
  • Views 1319 views
  • Likes 1 like
  • Comments 0 comments
Related
Recommended
  • raspberry
  • pi
  • ardexpert
  • matlab
  • arduino
  • simulink

Android controlled Raspberry Pi and Arduino Robot

anujaapte
anujaapte
15 Aug 2014

I had previously shared a video which talked about a robot which included both, a Raspberry Pi and an Arduino and was used to track a green ball. The robot used computer vision algorithms available with Simulink to detect and track the green ball. I came across a similar robot created by a colleague which is controlled by an Android app!

 

The robot runs on a Raspberry Pi and an Arduino Mega 2560. The Arduino Mega is used to control the individual motors of the robot, whereas the Raspberry Pi is used to communicate with the Android phone over wi-fi. The robot has a 4 motors (one for each wheel) and one servo motor connected to a webcam. The servo motor can be oriented from 0 to 180 degrees. The Raspberry Pi transmits video data to the Android device, and receives control signals from the phone. These signals are then passed onto the Arduino Mega which then drives the 4 motors and the servo motor.

 

The algorithms to program the Raspberry Pi and Arduino Mega were developed in Simulink and then deployed onto the microcontrollers using the 'Run on Target Hardware' option in Simulink. The project requires the use of Raspberry Pi support from Simulink, and Arduino Support from Simulink

 

image

                              Simulink Blocks used for the Raspberry Pi

 

Check out the video to see the robot in action!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is the third robot that I have seen that uses a combination of both Arduino, and Raspberry Pi with the earlier ones being the Rapiro and the Rasduino. Reach out if you have built a similar robot and would like to share it us!