Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Announcing the Raspberry Pi 5 with 16GB RAM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 9 Jan 2025 9:50 AM Date Created
  • Views 24396 views
  • Likes 14 likes
  • Comments 6 comments
Related
Recommended
  • new raspberry pi
  • Raspberry pi 5 16gb
  • RPI 5 16GB Specs
  • raspberry pi 5
  • Raspberry Pi 16gb Specs
  • raspberry pi
  • RPI 5 16gb

Announcing the Raspberry Pi 5 with 16GB RAM

e14phil
e14phil
9 Jan 2025

This morning we are excited to announce the Raspberry Pi 5 with 16GB of RAM

We first announced Raspberry Pi 5 back in the autumn of 2023, with just two choices of memory density: 4GB and 8GB.
Last summer, we released the 2GB variant, aimed at cost-sensitive applications. And today we’re launching its bigger sibling, the 16GB variant, priced at $120.

image

Why 16GB, and why now?

Raspberry Pi's Eben Upton Explains: image

" We’re continually surprised by the uses that people find for our hardware. Many of these fit into 8GB (or even 2GB) of SDRAM, but the threefold step up in performance between Raspberry Pi 4 and Raspberry Pi 5 opens up use cases like large language models and computational fluid dynamics, which benefit from having more storage per core.

And while Raspberry Pi OS has been tuned to have low base memory requirements, heavyweight distributions like Ubuntu benefit from additional memory capacity for desktop use cases.

The optimised D0 stepping of the Broadcom BCM2712 application processor includes support for memories larger than 8GB. And our friends at Micron were able to offer us a single package containing eight of their 16Gbit LPDDR4X die, making a 16GB product feasible for the first time."

image

Raspberry Pi 5 16GB Specifications

  • SoC – Broadcom BCM2712 “D0” stepping
    • CPU – Quad-core Arm Cortex-A76 processor @ 2.4 GHz with crypto extensions, 512KB per-core L2 caches, 2MB shared L3 cache
    • GPU – VideoCore VII GPU @ 800 MHz with support for OpenGL ES 3.1, Vulkan 1.2, 4Kp60 HEVC decoder
  • System Memory – 16GB LPDDR4X-4267 SDRAM
  • Storage – MicroSD card slot with support for high-speed SDR104 mode
  • Video Output/Input
    • 2x HDMI port up to 4Kp60 with HDR support
    • 2x 4-lane MIPI camera/display transceivers
  • Networking
    • Gigabit Ethernet RJ45 port via Broadcom BCM54213PE transceiver; optional PoE+ support through Raspberry Pi PoE+ HAT
    • Dual-band 802.11ac Wi-Fi 5
    • Bluetooth 5.0 / Bluetooth Low Energy (BLE)
  • USB – 2x USB 3.0 ports supporting simultaneous 5Gbps operation, 2x USB 2.0 ports
  • Expansion
    • 40-pin Raspberry Pi GPIO header
    • PCIe 2.0/3.0 x1 FFC interface
  • Misc – Real-time clock (RTC) powered from an external battery, power button, UART debug connector
  • Power Supply – 5V/5A DC power via USB-C, with Power Delivery support
  • Dimensions – 85 x 56 mm

The Raspberry Pi 5 16GB is being added to our online stores as we speak. 

Raspberry Pi 5 - 16GB

  • Sign in to reply
  • DAB
    DAB over 1 year ago

    I like it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 1 year ago

    saweet 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 1 year ago in reply to mp2100

    Beelink do some amazingly priced NUCs too. We use them at work in some situations we have previously used a Pi. In fact we have an internal product where we use either. It's a touch-screen that allows presenters at conferences to control various things like video switching, asking for technical assistance, etc. If we want small and self-contained then the software runs on a Pi 3 with 7" touchscreen. I f we want something bigger with more features, we use a NUC and 14" widescreen touchscreen.

    There are definitely situations that fit a NUC over a Pi or vice versa though. They're comparable in some ways but not in others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mp2100
    mp2100 over 1 year ago

    At that price, I’d buy an Intel NUC.  Quick check on Amazon, Intel N150, 8 GB ram, $140.  That includes the power supply and a case. Apples vs. Oranges comparison, yes. Sure, no GPIO, but still useful for many things.

    Don’t get me wrong, I love my Pi 1, Pi 2, Pi 3, Pi 0, then 3b, 4, and 5.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 1 year ago

    I can see that it may suits some people perfectly, but once you start bumping the specs and price up that high it may be better to grab a cheap desktop PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>