• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Build an Intruder detector with Raspberry Pi and robomq.io
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 17 Mar 2015 1:57 PM Date Created
  • Views 1284 views
  • Likes 2 likes
  • Comments 4 comments
Related
Recommended
  • rpi_intermediate
  • rpiintermediate
  • raspberry_pi
  • iot
  • burglar_alarm

Build an Intruder detector with Raspberry Pi and robomq.io

e14 Contributor
e14 Contributor
17 Mar 2015

Build an Intruder detector with Raspberry Pi and robomq.io


Device, sensors and systems connecting together are driving the next generation of applications creating the Internet of Things (IoT). robomq.io provides an open standard based platform to connect your devices and sensors to the back end applications, systems, processes and people, enabling you to build the next big thing.


Raspberry Pi, a popular programmable device, is a good representative example for device integration. The Raspberry Pi is a credit-card sized microcomputer that plugs into your HDMI monitor or a TV and a keyboard. It is a popular prototyping platform similar to other microprocessors like BeagleBone, Arduino etc.  The instruction below can be used with these other platforms as well.


image

Figure 1: Raspberry Pi Microprocessor

If you are new to Raspberry Pi, there may be few setup steps before you can integrate it with robomq.io. You’ll need an input device, a keyboard, a USB power supply and a monitor (this is optional, since you can still operate it using ssh). Figure 1 is a picture of the Raspberry Pi model B+, with a case for protection.

 


After you have finished setting up your raspberry pi, you’ll start to play with the 40 GPIO pins on it. These pins can be used to provide power (+5V or +3.3V), read data (signal pins) or read voltage level (for analog components), write data (for digital components) or write voltage level (for analog components) and provide ground wiring (GND pins). Using these pins, you can plug in electronic components like sensors, LED lights, matrix display modules etc. And with an electric relay, you can even control larger electrical components like servomotors and heavy machinery.  The request-reply messaging model of robomq.io can be used to monitor the sensor environment and react to it via control message.


 

image

Figure 2: PIR Motion Sensor

We are going to build a basic intruder detection system using PIR motion sensor and camera. PIR sensor is a simple analog sensor which gives a high voltage output when something moves in its range. Figure 2 and 3 are the PIR motion sensor and a 5MP camera that can be used with Raspberry Pi. Just a reminder, if you never tried to run a camera on your raspberry pi before, you may need to enable the camera module.


image

Figure 3: Raspberry Pi Camera Module

To do this, open the “raspi-config” tool from the Terminal:

$ sudo raspi-config

 


Select “Enable camera” and hit “Enter”, then go to “Finish” and you'll be prompted to reboot.


The principle of the intruder detection system is that when a moving object gets detected by the motion sensor, it will trigger the camera to take a picture. Then the “sensorProducer “ module (we will talk about this module in detail later in this blog) will send this picture to robomq.io. On the receiving side, we will create an HTML consumer which will subscribe to robomq.io and receive messages from it. The receiver will be embedded in a HTML webpage and will display the picture as and when the intruder is detected. It is a very simple interuder detector app. The emphasis is not on a fancy app but the demonstration of the fact that robomq.io can enable building complex applications, while it taks care of middleware plumbing.

The whole project is divided into several steps. But don’t worry, each step will be explained in the detail as we progress. Let’s have a quick listing of the steps to get the big picture first:


1. Wire up PIR motion sensor and camera to the Raspberry Pi

2. Install necessary libraries on Raspberry Pi

3. Write the intruder detection program and Integrate the intruder detection program with robomq.io

4. Create an HTML page to  display intruder’s picture

 


Without further adieu, let’s dive into these steps:

 

1. Wire up PIR motion sensor and camera to raspberry pi


image

Figure 5: Basic Intruder Detector

It is quite easy to connect the camera. Look carefully on the Raspberry Pi and look for word “CAMERA” beside a port. Simply plug in the camera cable to the port. For the PIR motion sensor,  connect  the following using connector wires:

1) “vcc” pin on PIR sensor to +5V pin on Raspberry Pi

2) “OUT” pin on PIR sensor to #6 pin on Raspberry Pi

3) “GND” pin on PIR sensor to GND on Raspberry Pi

Figure 4 is the schematic diagram of how to wire the PIR motion sensor. The finished basic intruder detector may look something like the Figure 5 on the right.


image

Figure 4: Wring the Motion Sensor

 

 

2. Install necessary libraries on Raspberry Pi


You need to install three libraries on the Raspberry Pi, which are not installed by default.

First is the “RPi.GPIO” module, which is the library to work with GPIO pins on Raspberry Pi. Second is “picamera” module  to control camera operations. The third library, “sensorProducer”, is needed to integrate the intruder detection program with robomq.io. This is a very small client side library provided by robomq.io. It takes care of sending messages to robomq.io hub on the cloud using industry standard protocols.


Run the command below to install “RPi.GPIO” module:

$ sudo pip install RPi.GPIO


Run the command below to install “picamera” module:

$ sudo pip install picamera


To install “sensorProducer” module , run the following command:

$ sudo pip install https://s3.amazonaws.com/public.robomq/packages/sensorProducer.tar.gz


3. Write the intruder detection program which is integrated with robomq.io


Before you proceed further, you will need a free trial account on robomq.io. If you don’t have one, click here to get one for free now!


We have a documentation page and a GitHub repository to provide you with the explanation and the example code on how to get your devices and applications integrated with robomq.io.

Docs page: http://robomq.readthedocs.org/en/latest/deviceIntegration/

GitHub page: https://github.com/robomq/robomq.io


For this step you will configure the “sensorProducer” module, that you installed in step 2, with your trial account credentials to enable connection and communication with the robomq.io hub.

Edit the producer.config file, which is located in the directory where sensorProducer is installed:

$ sudo vi /usr/local/lib/python2.7/dist-packages/sensorProducer/producer.config 


Change “host” to “trial.robomq.io”, set “vhost” to your free trial account vhost name, “username” to your username, and “password” to your password. All of this information is provided as part of your trial account.  You will see two other attributes in the config file,  “Device ID” and “Coordinate”.  These attributes are used to give an ID and the location to the intruder detection device. For this example,  just give “Device ID” a random name of your choice like “Device123”, and for “coordinate” give a random pair of latitude and longitude coordinate like [46,-79].


Now let’s write a program to collect data from the PIR motion sensor and the camera.  For Raspberry Pi programming, we recommend Python, as it is easy to read and to get started even for novice programmers.


Let’s first import the necessary modules; “time” for getting the timestamp,  “RPi.GPIO” for controlling GPIO pins,  “picamera” for controlling the camera,  and “base64” to encode and decode the taken picture into a base64 encoding format. Module “sensorProducer” is in charge of connecting to the robomq.io broker and provides utility functions to send and receive data. We also need to the “io” module is for handling input-output for the image stream.

import time
 import RPi.GPIO as gpio
 import picamera
 import base64
 from sensorProducer import producerMQTT as producer
 import io


In this example we have used MQTT (MQ for Telemetry) protocol for messaging. You also have the options of using AMQP (Advanced Message Queue Protocol) or STOMP (Simple Text Oriented Message Protocol). The “sensorProducer” module has utilities for these protocols as well. If you are interested in trying those other two protocols, simply add “from sensorProducer import producerAMQP as producer” or “from sensorProducer import producerSTOMP as producer” for AMQP and STOMP respectively instead of importing producerMQTT as shown above.


Now we are going to define the pin number of the PIR motion sensor, which should be #6 since we plugged the motion sensor OUT pin to #6 on Raspberry Pi (see step 1). We will set this pin to read mode to get notified of the intrusion events. After this define the camera and its resolution.

gpio.setmode(gpio.BCM)
 mpin = 6
 gpio.setup(mpin,gpio.IN)
 camera=picamera.PiCamera()
 camera.resolution=(350, 200)


Finally, we define the logic in the main while loop. “gpio.wait_for_edge” takes cares of detecting the voltage rise and fall on pin #6. When motion is detected in motion sensor’s range, the voltage on Pin #6 changes from “low” to “high”.  At that point the program gets the timestamp, and triggers the camera to take a picture to send it as stream to robomq.io. The “base64” module will transform the image to base64 format then put it as an element of the JSON object being sent to robomq.io. The “producer” module will send this JSON message to the robomq.io broker. The program also prints the message on the console for debugging or verification when the intrusion event is detected.

while True:
 gpio.wait_for_edge(mpin, gpio.RISING)
 t=time.strftime('%Y-%m-%d %H:%M:%S')
 print('Intruder detected'),'----------',t
 imgStream=io.BytesIO()
 camera.capture(imgStream, ‘jpeg’)
 gpio.remove_event_detect(mpin)
 timeStamp = time.time() * 1000
 msgImg = {"time": timeStamp}
 msgImg["image"] = base64.b64encode(imgStream.getvalue()) 
 try:
 producer.send(msgImg, routingKey="image")
 except:
 print "Error: failed to send data through producer"
 gpio.wait_for_edge(mpin, gpio.FALLING)
 t=time.strftime('%Y-%m-%d %H:%M:%S')
 print('Intruder left or froze'),'-----',t
 gpio.remove_event_detect(mpin)


Note the “routingKey” parameter in the send function. This parameter is used by the robomq.io to correctly route the message to the consumer. You will later see in the consumer code that this value is used to retrieve the message.


Putting it all together, your intruder detector program should look like the below:

import time
 import RPi.GPIO as gpio
 import picamera
 import base64
 from sensorProducer import producerMQTT as producer
 import io
 gpio.setmode(gpio.BCM)
 mpin = 6
 gpio.setup(mpin,gpio.IN)
 camera=picamera.PiCamera()
 camera.resolution=(350, 200)
 while True:
 gpio.wait_for_edge(mpin, gpio.RISING)
 t=time.strftime('%Y-%m-%d %H:%M:%S')
 print('Intruder detected'),'----------',t
 imgStream=io.BytesIO()
 camera.capture(imgStream, ‘jpeg’) 
 print('intruder captured!')
 gpio.remove_event_detect(mpin)
 timeStamp = time.time() * 1000
 msgImg = {"time": timeStamp}
 msgImg["image"] = base64.b64encode(imgStream.getvalue()) 
 try:
 producer.send(msgImg, type="image")
 except:
 print "Error: failed to send data through producer"
 gpio.wait_for_edge(mpin, gpio.FALLING)
 t=time.strftime('%Y-%m-%d %H:%M:%S')
 print('Intruder left or froze'),'-----',t
 gpio.remove_event_detect(mpin)


Now, you are all set with the code on Raspberry Pi and should able to send the intruder pictures to the robomq.io hub on the cloud.


4. Create a HTML page to  display intruder’s picture


Your intruder detector is integrated into robomq.io. But all that you see are the notifications on the terminal, right? To really make it cool, write a simple consumer using HTML and JavaScript, which will display the intruder picture on a webpage.


Lets create an HTML file. First we need to import the necessary library for building the consumer:

<script src="https://cdnjs.cloudflare.com/ajax/libs/stomp.js/2.3.3/stomp.js"></script>
 <script src="http://cdn.sockjs.org/sockjs-0.3.min.js"></script>


These are the WebSTOMP client libraries. If you are interested to learn more, please go to http://jmesnil.net/stomp-websocket/doc/ for details. In a nutshell, the WebSTOMP is a messaging protocol supported by robomq.io that allows you to run a consumer or a producer in the browser without the need for a server side code.


We connect to robomq.io on loading of the HTML file by putting the code in the “window.onload” JavaScript callback function.

window.onload = function() {
 var websocket=new SockJS("https"+"://"+"trial.robomq.io"+":"+"15673"+"/stomp");
 client = Stomp.over(websocket);
 client.connect(username, password, onConnect, onError, vhost);
 };

 

In this function we are going to use host name as trial.robomq.io, port as 15673, and connect to robomq.io with your credential (username and password) from your free trial account. Please replace username, password and vhost with the credential provided upon your free trial signup. The other two parameters in client.connect() function are callback function, onConnect and onError, which we will define below:

function onError(error) {
 alert(error);
 }


The “onError” function will be triggered when something wrong happened with the connection, and it will give a pop up notification.

function onConnect() { 
 subscription = client.subscribe("/topic/" + image, onMessage, {ack: "auto"});
 }

 


This “onConnect” function is pretty easy to read. It will subscribe to a topic named “image”  (which matches with the routingKey provided by producer in step 3) with acknowlegement option as “auto”. You may also be curious about the other parameter called “onMessage” in the “onConnect” function. This callback is the heart of the message processing which receives the message from the subscribed topic on robomq.io. With in this callback we will write the code to display the intruder image and the timestamp of the intrusion event.

function onMessage(message) {
 msgJson = JSON.parse(message.body);
 var info = document.createElement("h1");
 info.innerHTML = "Time: " + new Date(msgJson.time).toString();
 var photo = document.createElement("img");
 photo.src = "data:image/jpg;base64," + msgJson.image;
 var hr = document.createElement("hr");
 var container = document.createElement("div");
 container.appendChild(info);
 container.appendChild(photo);
 container.appendChild(hr);
 container.align = "center";
 document.body.insertBefore(container, document.getElementById("imageStartHere").nextSibling);
 }

 


Below is the complete listing of your HTML page:

<!DOCTYPE html>
 <html>
 <body onunload="close()">
 <div id="imageStartHere"></div>
 </body>
 <script src="https://cdnjs.cloudflare.com/ajax/libs/stomp.js/2.3.3/stomp.js"></script>
 <script src="http://cdn.sockjs.org/sockjs-0.3.min.js"></script>
 <script>
 var client, subscription;
 window.onload = function() {
 var websocket=
 new SockJS("https"+"://"+"trial.robomq.io"+":"+"15673"+"/stomp");
 client = Stomp.over(websocket);
 client.connect("WaterSupply", "admin", onConnect, onError, "WaterSupply");
 client.heartbeat.outgoing = 0;
 client.heartbeat.incoming = 0;
 };
 function onConnect() { 
 subscription =
 client.subscribe("/topic/" + "image", onMessage, {ack: "auto"});
 }
 function onMessage(message) {
 msgJson = JSON.parse(message.body);
 var info = document.createElement("h1");
 info.innerHTML = "Time: " + new Date(msgJson.time).toString();
 var photo = document.createElement("img");
 photo.src = "data:image/jpeg;base64," + msgJson.image;
 var hr = document.createElement("hr");
 var container = document.createElement("div");
 container.appendChild(info);
 container.appendChild(photo);
 container.appendChild(hr);
 container.align = "center";
 document.body.insertBefore(container, document.getElementById("imageStartHere").nextSibling);
 }
 function onError(error) {
 alert(error);
 }
 function close() {
 subscription.unsubscribe();
 client.disconnect();
 }
 </script>
 </html>

 

Now you can run your Raspberry Pi. Look at the terminal and make sure it’s running. Go ahead and open the HTML consumer page in browser. Once the consumer file is opened it will automatically connect to robomq.io and subscribe to it. Try to move in front of the motion sensor, you should see your picture showing up in the browser, something like the below:


image


Found it interesting? Make one yourself!!

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dtsartsanis +1
    why don't just buy one... since it's so cheap
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dtsartsanis

    Alright...good luck with your competition. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dtsartsanis
    dtsartsanis over 11 years ago in reply to e14 Contributor

    My country and me at the moment faces a big economic crisis. RIght now in Greece, Raspberry Pi 2 costs about 50 euros including post costs.

    So for the moment i cant afford buying a new Raspi.Maybe ill be lucky enough to win one and continue with some projects i have in mind.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dtsartsanis

    why don't just buy one... since it's so cheap image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dtsartsanis
    dtsartsanis over 11 years ago

    Great project. If i win a Raspberry Pi 2 from the "Plug in and win a Pi 2" competition i will definetely try this out.image