Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Building a Thermal Imaging System with the Raspberry Pi 3, Sense HAT and Panasonic Grid-EYE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 9 Nov 2016 12:09 PM Date Created
  • Views 12803 views
  • Likes 19 likes
  • Comments 63 comments
Related
Recommended
  • thermopile sensor
  • pi 3
  • rpiintermediate
  • panasonic grid eye
  • amg8832ek
  • amg8834ek
  • rpibeginner
  • amg8834
  • thermopile
  • amg8832
  • infrared_sensor
  • panasonic grid-eye
  • grid eye
  • thermopile array
  • grid-eye sensor
  • rasberry pi 3
  • javascript
  • panasonic_industrial_europe
  • infrared array
  • node.js
  • pi3-ibm-iot-learnkit
  • grid-eye

Building a Thermal Imaging System with the Raspberry Pi 3, Sense HAT and Panasonic Grid-EYE

shabaz
shabaz
9 Nov 2016

Introduction

Sometimes it is great to be able to see if things are hot or cold with a thermometer or other device. Multiply it by 64 and it is possible to get a graphical image of hot spots or detect humans for instance.

A thermopile array can be used to measure temperature from a distance and a special part from Panasonic called Grid-EYE happens to have 64 of them : )

Since the Sense HAT has 64 LEDs, I wanted to try them together : )

image

 

This is what is implemented:

image

 

For more experiments with the Grid-EYE and a review, see here: Panasonic Grid-EYE RoadTest - Review

 

What can you do with it?

The Grid-EYE is designed for detecting humans or objects that come into its field of view. It could be used for automatically turning on the heating when a human is detected, or automatically opening doors for instance. It differs greatly from the usual passive infrared (PIR) sensors used in alarm systems; they require movement whereas thermopile sensors will continuously detect objects while they remain in the field of view. By processing the images over time it is possible to see which direction humans or objects are moving. This could be useful for more intelligent automated doors or barriers, or for innovative electronic advertising that is triggered by human presence and actions.

 

In the brief time that I explored, it was possible to see people from a distance of five metres, and a 10 ohm resistor connected to an AA battery from about an inch away. By experimenting with the software it is possible to choose the spectrum of color that is desired for the particular temperature range of interest.

image

 

Grid-EYE usefulness for people detection (occupancy sensor) was explored in the Grid-EYE Review blog post.

 

Build Steps

The project is straightforward and simple, so in the interests of efficiency this report won’t have a lot of text!

To build this project, a Pi 3 and a Sense HAT is needed, and the Grid-Eye evaluation kit. I already had the Pi 3 and Sense HAT (and the associated memory card and power supply) as part of the Pi 3 IBM IoT Learner KitPi 3 IBM IoT Learner Kit reviewed here. The Grid-EYE evaluation board is available separately. The one I had (model AMG8832) is not available any more but there is a better performance AMG8834 Grid-EYE Evaluation ModuleAMG8834 Grid-EYE Evaluation Module that can detect humans up to 7 metres away.

 

The evaluation board contains the Grid-EYE, a pre-programmed microcontroller and Bluetooth Smart capability. Basically nothing needs to be done with the eval board except plug it into a power supply! The supply can be a 5V mobile phone charger or a PC USB port. The photo here shows the Grid-EYE evaluation board. It is about the footprint of a playing card. The Grid-EYE module itself is very small, about 12mm on its longest dimension.

image

 

Since the Pi 3 also has Bluetooth Smart capability, the Grid-EYE board connects to the Pi using this. This is great because it means that the imaging can be performed remotely.

The Pi 3 is responsible for translating the 8x8 array of values into colours and sending them to the Sense HAT’s display. The Pi 3 also runs a little web server so any web browser (e.g. PC or mobile phone) can be used to connect to the Pi and view the images live.

Check out the short video (1.5 mins) for some example capture.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Here are the instructions to build it. First, as root user (or prepend sudo to these commands):

 

apt-get install libbluetooth-dev
update-nodejs-and-nodered

 

Then, as normal user (e.g. pi or your username):

 

git clone https://github.com/shabaz123/grid-eye
cd grid-eye
npm install noble
npm install sense-hat-led
npm install rotate-matrix
npm install ioctl
npm install socket.io
npm install imagejs

 

Change the index.js file at grid-eye/node_modules/sense-hat-led using the index.js_mine file (which has been through the babel transpiler) using this command:

 

 

cp index.js_mine node_modules/sense-hat-led/index.js

 

 

The grid-eye/index.js file will need a modification, search for the line with the text progpath and set it to point to the grid-eye folder. The slash at the end is important. For example for me it says:

 

var progpath='/home/shabaz/grid-eye/';

 

That’s it! To run it, as root user (or prepend with sudo) type:

 

node index.js

 

Use a browser to navigate to http://xx.xx.xx.xx:8081/index.html

The code works but is just prototype quality and there is lots of room for improvement. It seems to work reasonably well but would benefit from some configuration options (things like temperature range are hard-coded).

Attachments:
index_pc.zip
  • Sign in to reply

Top Comments

  • ajens23
    ajens23 over 9 years ago +5
    Now that is pretty cool! (errr....hot,,,, or something like that) I'm going to have to try that.
  • DAB
    DAB over 9 years ago +5
    Excellent post. I knew that the Grideye sensor had great capability, so it was great to see that it could be as useful as I thought. Now all I need to do is find some time to play with one. DAB
  • beacon_dave
    beacon_dave over 9 years ago +5
    I have been pondering over how well these Grid-EYE sensors might work for room occupancy monitoring purposes. For example if they were mounted on a ceiling over a seating bank, then could they identify…
  • shabaz
    shabaz over 8 years ago in reply to zcsaki

    Hi csiko,

     

    The eval board sends all the information as a type of stream where the length may not match, i.e. it can be fragmented. Information is just shoved in Bluetooth LE packets and the length is not 135 bytes. So, the receiving code needs to look out for the beginning of a frame, and keep reading packets until there is enough to reassemble the entire frame. You can see the beginning is marked '2a 2a 2a' in your packet capture. The index.js source code also does the same thing if you look at line 103:

     

    if((data[0]==0x2a) && (data[1]==0x2a) && data[2]==(0x2a)){

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to david.aguilar

    Hi David,

     

    This indicates an issue with the Sense HAT, maybe it is not plugged in?

    If you wish to use the code without Sense HAT, there is a file called index_pc.zip that is attached to the blog post.

    For your scenario, do you have the Sense HAT plugged in?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • david.aguilar
    david.aguilar over 8 years ago

    hi, good tutorial congratulations, i have a problem, when i run the program, appears the next error, can you help me please?

     

    /home/pi/grid-eye/node_modules/sense-hat-led/index.js:27

        throw Error('Cannot detect RPi-Sense FB device');

        ^

     

     

    Error: Cannot detect RPi-Sense FB device

        at Error (native)

        at findFB (/home/pi/grid-eye/node_modules/sense-hat-led/index.js:27:11)

        at Object.<anonymous> (/home/pi/grid-eye/node_modules/sense-hat-led/index.js:17:10)

        at Module._compile (module.js:409:26)

        at Object.Module._extensions..js (module.js:416:10)

        at Module.load (module.js:343:32)

        at Function.Module._load (module.js:300:12)

        at Module.require (module.js:353:17)

        at require (internal/module.js:12:17)

        at Object.<anonymous> (/home/pi/grid-eye/index.js:9:12)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zcsaki
    zcsaki over 8 years ago

    Hi,

    it's very cool prjoect i've tested the pc version and is working fine!

    Maybe someone here had the same effect that i've had:
    I would like to have direct access to the datastream, but the datastream size is always different and it's never reach the 135 bytes.
    When I connect to the grid-eye with gatttool i did not get the correct datasize (135 bytes https://eu.industrial.panasonic.com/sites/default/pidseu/files/grid-eye_communication-protocol-v1.0.pdf )
    gatttool -b 00:13:43:3E:E2:66 -I

    [00:13:43:3E:E2:66][LE]> connect

    Attempting to connect to 00:13:43:3E:E2:66

    Connection successful

    Notification handle = 0x0012 value: 2a 2a 2a ff 01 76 00 72 00 74 00 73 00 72 00 71 00 72 00 74

    Notification handle = 0x0012 value: 71 00 73 00 74 00 74 00 74 00 74 00 75 00 74 00 72 00 73 00

    Notification handle = 0x0012 value: 77 00 74 00 73 00 72 00 74 00 71 00 0d 0a

    Notification handle = 0x0012 value: 2a 2a 2a ff 01 77 00 73 00 72 00 73 00 71 00 73 00 73 00 76

    Notification handle = 0x0012 value: 71 00 72 00 72 00 74 00 76 00 75 00 75 00 73 00 74 00 72 00

    Notification handle = 0x0012 value: 00 75 00 72 00 73 00 74 00 74 00 75 00 72 00 71 00 73 00 72

    Notification handle = 0x0012 value: 00 77 00 78 00 76 00 77 00 71 00 73 00 73 00 74 00 74 00 0d

    Notification handle = 0x0012 value: 0a 2a 2a 2a ff 01 75 00 75 00 73 00 71 00 73 00 74 00 72 00

    Notification handle = 0x0012 value: 76 00 75 00 75 00 76 00 71 00 71 00 70 00 74 00 72 00 74 00

    Notification handle = 0x0012 value: 73 00 74 00 73 00 75 00 75 00 75 00 73 00 72 00 71 00 76 00

    Notification handle = 0x0012 value: 71 00 76 00 79 00 75 00 75 00 72 00 75 00 71 00 71 00 6f 00

    Notification handle = 0x0012 value: 0d 0a

     

    Have someone tried to connect with gatttool?

    Cheers,


    csiko



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to maanas.adi

    Hi Maanas,

     

    The code would need to be developed for that, this capability does not exist in the code currently. In index.js, and you'll see that the 64x64 pixel colors are sent, not the temperature. So, you could extend that so that 64 additional values are sent (with temperature information) perhaps, or maybe just send the temperature of the center pixel, or average of five most center pixels, etc. You'd also need to make some changes in the browser-side code (script.js).

    If you do make the changes and they work, please do share the code to help others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>