Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Essential Raspberry Pi Peripherals #1: GPIO and Other Connectors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 26 Aug 2015 1:13 PM Date Created
  • Views 6411 views
  • Likes 3 likes
  • Comments 39 comments
Related
Recommended
  • connectors
  • real_world
  • peripherals
  • pifacecad
  • gpio
  • ethernet
  • hdmi
  • composite_display
  • usb
  • raspberry_pi
  • raspberry-pi
  • digital_io
  • networking
  • display
  • stereo
  • piface

Essential Raspberry Pi Peripherals #1: GPIO and Other Connectors

balearicdynamics
balearicdynamics
26 Aug 2015

With this first post we start off on something of an adventure, experimenting and experiencing one of the most fascinating aspects of this SBC (Single Board Computer): connecting the device with the real world.

(note: here we consider working with a Raspberry PI 2 but almost all the mentioned features and possibilities will apply to the previous models).

 

Connecting the Raspberry PI to Something Else

One of the most interesting features of the Raspberry Pi is that it includes most of the features we need to interact with the real world. Firstly we have the GPIO, which is the array of pins giving the option to interact with the world through many sensors, communication protocols, motors, LEDs and so on.

 

But that's not all. There is more, and the possibilities go beyond what we can imagine.

 

Just as a reminder, take a look to the following image:

image

Seems incredible, the connector we find in this credit-card sized device:

 

  • 40 Pin GPIO (General I/O ports): can be used for powering low consumption devices, connect I2C protocol external components, Input/Output digital signals, SPI (CLK, MISO, MOSI) protocol, TTL Serial TX/RX pins.
  • 4 USB2 ports: that means, on a Linux-based system, the possibility to connect a very wide range of USB devices.
  • 1 HDMI video and audio output: the HDMI video and audio output supporting full 1080P HD format gives the possibility to manage any display ratio (software configurable) with high quality audio. This feature makes the Raspberry PI a good base machine to make a good quality media center, game device and more.
  • 1 combined 4-pole 3.5 mm Jack connector for stereo output and composite video output: ideal when an HDMI monitor is not available.
  • 1 10/100 Ethernet RJ45 connector: for LAN connection as an alternative to the wireless WiFi when using a USB WiFi dongle
  • 1 camera connector: this connector is ready to work for the Raspberry PI camera that opens the door to an entire world of possibilities, from image shooting up to video capture, streaming, image processing and more.
  • 1 display connector: for small projects the use of a full sized external monitor may not be necessary, so a small screen (better if it's a touchscreeb) directly connected to the Raspberry Pi can be a better solution.

 

When the device is in your hands you have got the keys that open the door to an incredible new world.

 

All that glitters is not gold

In fact, this board can't do all that much on its own, solve ANY problems, or replace all your computers. But it can do a lot for sure. Looking in-depth at the Raspberry Pi connectors and functions it seems that some "advanced" features are missing. For example, it'd be better if the Ethernet was 1Gb instead 10/100 only, better if the boot was from something different than an SD card, better if there was also an audio input, great if the GPIO also included some manner of analog input, and so forth.

 

It's true, but the Pi does have the great advantage of stability: many of the apparently missing features are compensated by its extreme versatility and - why not? - our ability to create great projects, including those parts expected but not present. In my personal opinion this SBC remains one of the most complete, versatile and well equipped low-cost devices supporting Linux.

 

An overview on the next posts

To close this introductory first post on the Raspberry Pi peripherals the following is a list of what you can expect in the forthcoming series.

 

#2 Setting up the HDMI monitor

Despite the HDMI connector, not all the monitors support the same resolution. And the Raspberry Pi shares its video memory with the rest of the available RAM, so it's useful if you can totally control the display parameters (frequency, resolution, aspect ratio, video memory) simply by changing the operating system display configuration file.

 

#3 An introductory approach to wired and wireless networking

There are more options than simply plugging the LAN cable in the Ethernet port of the Raspberry PI. In this post we'll see how the Raspberry Pi can be a flexible networking device, acting as bridge, access point, wireless device and more.

 

#4 The Raspberry Pi camera beyond the webcam limits

Thanks to the power of Python and the specific characteristics of the Pi Camera it's possible to specialise the Raspberry Pi as a video/photo station: shooting, filming, image processing for a lot of possible applications; from photography to security, from stop-motion to the time-lapse filming.

 

#5 Lirc and IR controller: extending the limits of keyboard and mouse

With a very simple hardware approach we introduce the first non-conventional peripheral connection. Thanks to the Linux lirc library we can use a simplified HID (Human Interface Device) - a TV infrared control - to manage programs, device behaviour, and more.

 

#6 Enhancing our Pi projects with the Pi touchscreen

We will see how we can setup and integrate in our projects the Raspberry Pi 2.4" touch screen device.

 

#7 Enhancing our Pi projects with the PiFaceCAD LCD display

When a simple message is sufficient to control the Raspberry Pi behaviour but some control buttons would be useful, the PiFaceCAD (Control and Display) is the ideal device, which can be stacked on our Raspberry Pi for mobile, battery-powered applications.

 

Bookmark this page and the Ultimate Guide to Getting Started with a Raspberry Pi page to stay tuned to this essential guide to Raspberry Pi peripherals, folks!

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    The PI does great with multiple devices connected, infact I would find it hard to find a PC that will connect to I2C, SPI and GPIO devices without the help from an external uController these days, my preference…
  • balearicdynamics
    balearicdynamics over 10 years ago +2
    My macyoda, mcb1 You make comments on Grove but clearly don't know anything about Grove, you also don't seem to know much about BRICK, if did you would have never pointed out that it is being DISCONTINUED…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1 +2
    mcb1 Totally agree with you
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    A word of warning

     

    The 30A relay and the latching one are the only two I would consider for any mains related control, if you look at the back of them, they have clear and deliberate seperation of mains and control logic, the one you initially sited is built with a mains capapably relay but in my opinion the fact the power connector is right next to the control connector maks this a dangerious module for mains use. especially for the home / hobby user

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1

    Hi mark,

    thank you for pointing this aspect. This is what is stopping me in the choice of this kind of devices. As we have many other valuable and valid for all. Not only but also the fact that there is not an opening of this hardware it seems to me too much out of the most generalised visione I am trying to give to this tutorials series.

     

    I'll be happy to know also the point of view of other users, including Spanner image

     

    Anyway, IMHO I think we should be as much as possible oriented to give support to DIY than sponsoring one device or another just because we - hopefully - like it. Price influences my vision less than 50% in the choice.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to balearicdynamics

    this board is ONLY compatible with its own sensors

    I found that too.

     

    While the brick type may or may not be compatible with a non published 'standard', price was a deciding factor in my decision.

    These also had the cable that fitted Arduino with the three pins (V, G, Signal), which meant you didn't need a shield.

     

    I did like that most buttons pulled the pin down, but it would have been nice to have other coloured LED's ...image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Thank you for your sponsoring ! image

     

    I have only one doubt; this board is ONLY compatible with its own sensors. But by the other side, I see that these sensors are nice and cheap and probably it is not difficult to interface with there 3-pins system other sensors. The other aspect I am considering - and this is a bare personal opinion - is that the board is a bit expensive for what it supports on it. But I should think about. Anyway this is not the first next priority (every post also mentions the next few peripherals I plan to write on).

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Here are some links that should help:

     

    These guys make the R Pi to Grove shield ...

    http://www.dexterindustries.com/GrovePi/get-started-with-the-grovepi/

     

    They have a quick start and tutorial that I will be using, the more the better!.

     

    Here is a list of Grove sensors that they have tested with the shield ...

    http://www.dexterindustries.com/GrovePi/supported-sensors/

     

    Grove was invented by Seeedstudios, I believe, and here is their Grove section ...

    http://www.seeedstudio.com/depot/category_products?themes_id=1417

     

    When I can, I buy all my Grove parts from EpicTinker.com , and they carry almost EVERYTHING but not the newest stuff, they are usually a little cheaper price and with cheaper shipping and it gets to me very quickly, rather than in 3 weeks that Seeedstudios takes.

     

    As far as I know Brick is an older system that did not hold to their standard very well so problems arose. Grove was created to replace and modernize it, Seeedstudios carries all this stuff and anything that is open source and they have converter cables so that the Brick sensors can be used with Grove. Here is a link for Seeedstudios Bricks ...

    http://www.seeedstudio.com/depot/s/brick.html?search_in_description=0

     

    The same guys that make the GrovePi shield also have a BrickPi kit but it is much more expensive, here ...

    http://www.dexterindustries.com/shop/brickpi-advanced-for-raspberry-pi/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>