Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Essential Raspberry Pi Peripherals #1: GPIO and Other Connectors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 26 Aug 2015 1:13 PM Date Created
  • Views 6412 views
  • Likes 3 likes
  • Comments 39 comments
Related
Recommended
  • connectors
  • real_world
  • peripherals
  • pifacecad
  • gpio
  • ethernet
  • hdmi
  • composite_display
  • usb
  • raspberry_pi
  • raspberry-pi
  • digital_io
  • networking
  • display
  • stereo
  • piface

Essential Raspberry Pi Peripherals #1: GPIO and Other Connectors

balearicdynamics
balearicdynamics
26 Aug 2015

With this first post we start off on something of an adventure, experimenting and experiencing one of the most fascinating aspects of this SBC (Single Board Computer): connecting the device with the real world.

(note: here we consider working with a Raspberry PI 2 but almost all the mentioned features and possibilities will apply to the previous models).

 

Connecting the Raspberry PI to Something Else

One of the most interesting features of the Raspberry Pi is that it includes most of the features we need to interact with the real world. Firstly we have the GPIO, which is the array of pins giving the option to interact with the world through many sensors, communication protocols, motors, LEDs and so on.

 

But that's not all. There is more, and the possibilities go beyond what we can imagine.

 

Just as a reminder, take a look to the following image:

image

Seems incredible, the connector we find in this credit-card sized device:

 

  • 40 Pin GPIO (General I/O ports): can be used for powering low consumption devices, connect I2C protocol external components, Input/Output digital signals, SPI (CLK, MISO, MOSI) protocol, TTL Serial TX/RX pins.
  • 4 USB2 ports: that means, on a Linux-based system, the possibility to connect a very wide range of USB devices.
  • 1 HDMI video and audio output: the HDMI video and audio output supporting full 1080P HD format gives the possibility to manage any display ratio (software configurable) with high quality audio. This feature makes the Raspberry PI a good base machine to make a good quality media center, game device and more.
  • 1 combined 4-pole 3.5 mm Jack connector for stereo output and composite video output: ideal when an HDMI monitor is not available.
  • 1 10/100 Ethernet RJ45 connector: for LAN connection as an alternative to the wireless WiFi when using a USB WiFi dongle
  • 1 camera connector: this connector is ready to work for the Raspberry PI camera that opens the door to an entire world of possibilities, from image shooting up to video capture, streaming, image processing and more.
  • 1 display connector: for small projects the use of a full sized external monitor may not be necessary, so a small screen (better if it's a touchscreeb) directly connected to the Raspberry Pi can be a better solution.

 

When the device is in your hands you have got the keys that open the door to an incredible new world.

 

All that glitters is not gold

In fact, this board can't do all that much on its own, solve ANY problems, or replace all your computers. But it can do a lot for sure. Looking in-depth at the Raspberry Pi connectors and functions it seems that some "advanced" features are missing. For example, it'd be better if the Ethernet was 1Gb instead 10/100 only, better if the boot was from something different than an SD card, better if there was also an audio input, great if the GPIO also included some manner of analog input, and so forth.

 

It's true, but the Pi does have the great advantage of stability: many of the apparently missing features are compensated by its extreme versatility and - why not? - our ability to create great projects, including those parts expected but not present. In my personal opinion this SBC remains one of the most complete, versatile and well equipped low-cost devices supporting Linux.

 

An overview on the next posts

To close this introductory first post on the Raspberry Pi peripherals the following is a list of what you can expect in the forthcoming series.

 

#2 Setting up the HDMI monitor

Despite the HDMI connector, not all the monitors support the same resolution. And the Raspberry Pi shares its video memory with the rest of the available RAM, so it's useful if you can totally control the display parameters (frequency, resolution, aspect ratio, video memory) simply by changing the operating system display configuration file.

 

#3 An introductory approach to wired and wireless networking

There are more options than simply plugging the LAN cable in the Ethernet port of the Raspberry PI. In this post we'll see how the Raspberry Pi can be a flexible networking device, acting as bridge, access point, wireless device and more.

 

#4 The Raspberry Pi camera beyond the webcam limits

Thanks to the power of Python and the specific characteristics of the Pi Camera it's possible to specialise the Raspberry Pi as a video/photo station: shooting, filming, image processing for a lot of possible applications; from photography to security, from stop-motion to the time-lapse filming.

 

#5 Lirc and IR controller: extending the limits of keyboard and mouse

With a very simple hardware approach we introduce the first non-conventional peripheral connection. Thanks to the Linux lirc library we can use a simplified HID (Human Interface Device) - a TV infrared control - to manage programs, device behaviour, and more.

 

#6 Enhancing our Pi projects with the Pi touchscreen

We will see how we can setup and integrate in our projects the Raspberry Pi 2.4" touch screen device.

 

#7 Enhancing our Pi projects with the PiFaceCAD LCD display

When a simple message is sufficient to control the Raspberry Pi behaviour but some control buttons would be useful, the PiFaceCAD (Control and Display) is the ideal device, which can be stacked on our Raspberry Pi for mobile, battery-powered applications.

 

Bookmark this page and the Ultimate Guide to Getting Started with a Raspberry Pi page to stay tuned to this essential guide to Raspberry Pi peripherals, folks!

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    The PI does great with multiple devices connected, infact I would find it hard to find a PC that will connect to I2C, SPI and GPIO devices without the help from an external uController these days, my preference…
  • balearicdynamics
    balearicdynamics over 10 years ago +2
    My macyoda, mcb1 You make comments on Grove but clearly don't know anything about Grove, you also don't seem to know much about BRICK, if did you would have never pointed out that it is being DISCONTINUED…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1 +2
    mcb1 Totally agree with you
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to mcb1

    Something like this but more "kiddy" is what I have in mind for the BBC

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to spannerspencer

    I've been using these for our Arduino in Schools.

    It saves trying to teach electronics, and lets the pupils focus on the code.

    http://www.itead.cc/prototyping/electronic-brick.html

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to spannerspencer

    Hi spannerspencer !

     

    Maybe yes, I think. It is also interesting for me. I should take a look also to the price, as this should be fine for the users. My first impression is that if this really work as promised, most of the problems related to multi-devices connected to the Raspberry PI via the I2C protocol can be solved. But I should take a deep look to this tools and when I answered I was going out. I'll deserve to write down few words as I have a more clear idea of what does this stuff do.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago in reply to balearicdynamics

    Hmm, the Grove stuff is new to me -- looks very interesting, though. I like the modularity of the system. Maybe we should look into this more closely, balearicdynamics?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to balearicdynamics

    Thanks, I plan to use this with many sensors I am hoping the R Pi will be able to access many sensors in complex code without having a lot of overhead like dumping and re-initializing serial buses, basically avoid incompatibilities between Grove sensors, hoping I can easily use many all together.

     

    I am a computer professional but a beginner with R Pi.

     

    I2C is just the place to use a LOT of Grove sensors together, so tutorials on this would be greatly appreciated.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>