• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Getting Started With Raspberry Pi - Part 1
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: patkelly
  • Date Created: 24 May 2013 9:30 AM Date Created
  • Views 745 views
  • Likes 0 likes
  • Comments 3 comments
Related
Recommended

Getting Started With Raspberry Pi - Part 1

patkelly
patkelly
24 May 2013

The $35 Raspberry Pi is a credit-card-size computer developed with the intention of promoting computer science. it is a pleasant exodus from the monotonous computing world.

image

 

Most computer science students get to learn high-level programming languages and application development but they don’t really understand computers. The fun of controlling the real world with a real computer is never exposed to them. A normal computer lacks the capability to communicate with the real world through real interfaces.

 

With a normal computer that has a monitor, keyboard, mouse, printer and modem connected, hardly anything can be done, except the intended use. Of course, the printer port on a PC can be used to interface with the real world but that will be very clumsy and cumbersome not to talk of the non-availability of an easy programming environment for that.

The Raspberry Pi is a pleasant exodus from that monotonous computing world. You can hold this palm-size computer in your hand and at the same time interface with the real world with its 26 input/output (I/O) pins. With a  Raspberry Pi in hand, robotics is no more a fancy imaginary world of big and serious people but a real and authentic one.

 

You can get this computer for a small amount of money. In the UK the Raspberry Pi Model-A costs $25, while the price of Model-B is $35, plus local taxes and shipping/han- dling fees. In India, at many hobby outlets,  it  is  available  for  only  Rs2600. In fact, the latest B Model with 512MB RAM is no less than a Celeron computer of yesteryear, yet with a whole lot of imagination and possi- bilities to tap.

 

Model-A and Model-B

 

The first model of Raspberry Pi that appeared was Model-B, with two USB ports, an Ethernet socket.and 256MB RAM.  Later,  the Model B was upgraded to 512MB, and Model-A  came  to market with one USB port,no Ethernet socket and 256MB RAM. It is built around a BCM2835 Broadcom processor. It consumes 5V electricity at 1A current. As power consumption is less, there is no heat dissipation and no clumsy heat-sink is required. The operating system is based on the light- weight ARMv6 instruction set that a typical Broadcom processor under- stands—all open source and based on Linux variety.

 

 

 

 


Raspberry Pi Model ARaspberry Pi Model B

image
                                            
Buy Now Buy Now
image
Buy NowBuy Now
PriceFrom US$25From US$35
Ethernet/InternetNoYes
Dual USB ConnectorNoYes
512MB MemoryNoYes

Technical Features

ChipBroadcom BCM2835 SoC full HD multimedia applications processorBroadcom BCM2835 SoC full HD multimedia applications processor
CPU700 MHz Low Power ARM1176JZ-F Applications Processor700 MHz Low Power ARM1176JZ-F Applications Processor
GPUDual Core VideoCore IVRegistered Multimedia Co-ProcessorDual Core VideoCore IVRegistered Multimedia Co-Processor
Memory256MB SDRAM512MB SDRAM
EthernetNoneonboard 10/100 Ethernet RJ45 jack
USB 2.0Single USB ConnectorDual USB Connector
Video OutputHDMI (rev 1.3 & 1.4) Composite RCA (PAL and NTSC)HDMI (rev 1.3 & 1.4) Composite RCA (PAL and NTSC)
Audio Output3.5mm jack, HDMI3.5mm jack, HDMI
Onboard StorageSD, MMC, SDIO card slotSD, MMC, SDIO card slot
Operating SystemLinuxLinux
Dimensions8.6cm x 5.4cm x 1.5cm8.6cm x 5.4cm x 1.7cm
Visit the Raspberry Pi Group and Accessories Group for more activites and related products.

 

 

Original copy written by Somnath Bera for electronics for you April edition

  • Sign in to reply
  • morgaine
    morgaine over 13 years ago

    This blog post is incorrectly titled.  It is not a "Getting Started With Raspberry Pi" post at all, but a short newspaper-type overview of the concept and board specs.  It tells you nothing about getting started.  I think it could appropriately be renamed to something like "Overview of Raspberry Pi boards".

     

    That said, I'm not sure why such an article would be posted here almost a year and a half after Pi launch, and long after many highly detailed blog and forum posts have been written here about the Pi boards.  It's like a step back in time.

     

    The post is also wildly inaccurate in making senseless comments like "there is no heat dissipation".  This is an engineering site.  Blog articles don't have to be professional, but they should attempt to stay clear of being just plain wrong.  It does no credit to the site, and worse, it mis-educates any youngsters who may be reading it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • patkelly
    patkelly over 13 years ago in reply to mgt6910

    Thank you for pointing this out Malcolm, I've made the change to the post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mgt6910
    mgt6910 over 13 years ago

    To be historically accurate, I suggest that the following sentence:

     

    The first model of Raspberry Pi that appeared was Model-A, which had only one USB port and no Ethernet socket.  Later,  Model-B  came  into market with two USB ports,Ethernet socket  and 256MB RAM

     

    should be changed to :

     

    The first model of Raspberry Pi that appeared was Model-B, with two USB ports, an Ethernet socket.and 256MB ram.  Later,  the Model B was upgraded to 512MB, and Model-A  came  to market with one USB port,no Ethernet socket and 256 MB ram.