Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Google's Alexa-like Pi AIY Kit, mini teardown
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 4 May 2017 6:30 PM Date Created
  • Views 13368 views
  • Likes 20 likes
  • Comments 66 comments
Related
Recommended
  • aiy google
  • google aiy
  • google sdk
  • google_aiy
  • aiy
  • raspberry_pi
  • raspberry pi
  • amazon alexa
  • aiyproject
  • raspberry pi 3
  • aiy project
  • google embedded sdk
  • raspberry_pi_3

Google's Alexa-like Pi AIY Kit, mini teardown

shabaz
shabaz
4 May 2017

Google has been busy getting stuff attached to MagPi magazines.. I spotted a box containing an 'AIY' kit at the local magazine retailer. Basically it is a card box with some electrical parts and the MagPi magazine.

It is like a cut-down DIY version of Amazon Alexa from what I can tell.

 

They had plenty at closing time, so I suspect there will be lots for people to buy tomorrow too, but from examination it is an audio card and a few peripherals. USB sound cards are cheap these days so that is another option for those who don't/can't purchase the magazine.

Below are photos of the contents of the box (just the electronic bits are shown, there is also a cardboard self-assembly enclosure and the MagPi magazine itself; I might take photos of that later), like a mini-teardown where the teardown is already done.

 

I think it's fair to say the kit component-wise is a little boring, but at least it's cheap. The stereo mic is good to see though. And maybe more projects will be available in future.

Also there are other ways to achieve Alexa-like capability (from both a hardware and PaaS vendor perspective).

For higher quality there are multi-microphone options for Pi, although of course they are more expensive.

 

Where the fun will come in is with the software - it will be a lot of fun to create voice-enabled projects.

Although it is intended to use Google PaaS, not everyone likes sending audio to a cloud, but it is usable for standalone non-Internet-connected audio projects too, e.g. music player. No need to plug in the microphone wires.

 

In summary, it is nice to see traction with voice-enabled natural language assistant projects for hobbyists, and the hardware here is very basic, but at least it keeps interest up and lots of opportunities for those learning programming to have fun and create some cool projects.

 

Some photos and notes follow, as well as any reverse-engineered schematics. Also see the comments section.

 

image

 

Connections Overview

According to google's page, these are the connections (see diagram below). Handily the Pi's I2C, SPI and UART connections are broken out to pads all ready for soldering to the supplied SIL header pins.

There are also some output pins, probably MOSFET driven (can see what looks like SOT-23 sized MOSFETs marked G31 D5 (they are most likely N-channel MOSFETS part code Diodes Inc DMG3420U) on the right of the image along with SMD fuse and diode per output).

See further below for reverse-engineered schematic for that.

 

On the left of the board, there is space for soldering SIL pins for attaching hobby servo motors.

image

Output Drivers

The four drivers (shown on the right side of the diagram above) have most likely the following circuit - I think it is accurate but please let me know in the comments if it isn't:

image

The four MOSFETs are used in an open drain configuration, so the pins marked 'DRIVER' will be switched to ground (0V) whenever the corresponding GPIO pin goes high. If the desired load is 5V powered then the 5V pin can be used to provide power (there is a 500mA resettable fuse). The open drain configuration also allows a lower voltage source to be used to supply the load, and the MOSFET will switch the other end of the load to ground.

The diagram below shows how to connect a relay with a 5V coil. It is inadvisable to use the Driver outputs with a higher voltage despite it being an open drain configuration because current can flow through the diode in the schematic above and the fuse, causing damage.

Also, it is strongly advised not to use this for connecting mains operated equipment, because there are regulations governing what enclosure is used and how the cable is secured and so on. To control mains equipment it is good to use home automation methods such as wireless (there are radio transmitters available for the Pi).

image

 

A suitable relay could be Finder 5V coil SPDT 6A contacts changeover relayFinder 5V coil SPDT 6A contacts changeover relay or Finder SPST 6A relaySPST 6A relay . Both of these relays are very compact (20x10x10mm) and have pins that will fit a breadboard or stripboard so are easy to prototype with. The comments section further below has a photo of how to wire it up and some example Python code to test it by turning the relay on and off. Although these relays can be used with mains, it would be extremely inadvisable to do so without a decent PCB layout (not stripboard!) and other precautions (see here for some reasons). So, the relay control is best used for lower-voltage tasks.

 

Mains Control

One solution is to use wireless control. This can be country or region specific.

UK

I've used an Energenie wireless module before, it is a very small transmitter board that connects to the Pi and wirelessly controls mains sockets. The Energenie kitEnergenie kit comes with the wireless transmitter board and two sockets. It's good value, and meets the relevant electrical standards for the UK. It could be wired to the connections on the left side of the google voice HAT board allocated for Servos for example (by default it needs six GPIO although that number can optionally be reduced if needed).

 

Audio Output

The centre of the board contains the integrated circuit (IC) with the audio digital-to-analog converter and mono audio amplifier inside it, it is Maxim MAX98357A - thanks Inderpreet! (the 16-pin QFN sized IC says AKK BDK on it) and an EEPROM marked 24C32F.

 

image

Power Connections

There is also space for a DC power jack but none is fitted. A DC power jack with thin pins would fit. There is a SOT23-6 part near it, marked K4S DD and a SOT-23 part marked 23X D1 is close too. These two parts have a Q identifier, so are likely some type of transistors.

 

Microphone Board

The microphones are marked 432 QDF21G and are Knowles SPH0645LM4H (thanks again Inderpreet) MEMS digital microphones. They directly output an I2S bitstream.

image

 

The microphone input ports are on the underside:

image

 

This is the schematic of the microphone board, using the information from Inderpreet in the comments below. There may be some minor mistakes (please let me know in the comments section and I'll correct it). In theory the microphone board could be used standalone with the Pi, no need for the main Voice HAT board. It is a convenient breakout board for the surface-mount mics.

 

It could be suitable for small projects, e.g. with the 'Zero or with other boards with an I2S interface. It would be advisable to have a small resistance (e.g. 51 ohms) in series with the LRCLK and BCLK pins if it is connected directly.

There is nothing to stop a voice assistant from working without a speaker (you just won't hear the result, unless the on-board headphone socket on the Pi 3 is used perhaps).

Not all projects would require an audio response. Also, for some projects one may prefer a discreet response in an earphone (e.g. check your calendar by requesting it, but not announcing your plans to everyone).

image

 

Safety Leaflet

This is enclosed in the box:

image

  • Sign in to reply

Top Comments

  • nicklansley
    nicklansley over 9 years ago +5
    I managed to get hold of a copy of MagPi magazine and get it working with a Raspberry Pi 3: www.youtube.com/watch
  • ipv1
    ipv1 over 9 years ago +4
    I have a suspicion that that is not a code but rather an I2S amplifier - MAX98357A I just googled it and sure enough... I have one of those in stock from an unfinished project and just recalled it as I…
  • ipv1
    ipv1 over 9 years ago in reply to shabaz +4
    If I remember correctly, shabaz sir, you did a stereo i2s sound card circuit for the BBB some time back. Theoretically, that can be used here as well. I think I need to read more about that
  • shabaz
    shabaz over 9 years ago in reply to jhewitt123

    Hi John,

     

    I've added a diagram to show the relay connection. The relay will need to have a 5V coil. Note that even though the output from the voice HAT board is 'open collector', a voltage higher than 5V should not be used due to a diode in the circuit. Therefore (say) a 12V coil relay will not function, and trying to supply 12V to it could damage the board or the attached Pi.

    So, it is best to restrict to 5V relays only, and attach as shown.

     

    Also, this shouldn't be used to operate mains powered equipment, regardless of the relay ratings, because of the extreme likelihood of violating electrical regulations (there are regulations that govern what material the enclosure is made of, flame retardency, method used to attach the mains cable, fusing, earthing, gaps, etc. To control mains equipment it is best to use something intended for home automation, like wireless operated devices. For these a wireless transmitter can be connected to the Pi.

     

     

    image

     

    You can check if your fuses are ok by taking the unpowered and disconnected Voice HAT, and connecting one end (either end) of a multimeter (set to Ohms) to the pin marked '5V' on J13, and the other end to the centre pin on the Drivers section, as shown in the photo here. The resistance should be less than 1 ohm (first just short the multimeter wires together to see what the multimeter wire resistance is):

    image

     

    Regarding sound localization, I doubt this would be effective (I could be wrong), because there are only two microphones whereas Amazon Echo has around seven. There is a Pi board available soon called 'MATRIX Creator' which has eight mics but I don't know much more detail about it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jhewitt123
    jhewitt123 over 9 years ago

    Thanks for posting the output drive. I already fried 2 channels on 2 boards trying to guess. How does one reset or speed up resettling of the fuse????

    What is preferred way to drive a regular relay on this output, or for that matter, an opto-isolated relay?

     

    thanks all.

     

    also, does the stero mic permit sound localization and/or distance discrimination via timing differences so that external noise can be discriminated by phase/timing and triaged out? how does one access  this I wonder??

     

     

    Note added: fuse may take a while to reset:

    via  https://en.wikipedia.org/wiki/Resettable_fuse

     

    This cooling usually takes a few seconds, though a tripped device will retain a slightly higher resistance for hours, slowly approaching the initial resistance value. The resetting will often not take place even if the fault alone has been removed with the power still flowing as the operating current may be above the holding current of the PPTC. The device may not return to its original resistance value; it will most likely stabilize at a significantly higher resistance (up to 4 times initial value). It could take hours, days, weeks or even years for the device to return to a resistance value similar to its original value, if at al

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago

    Hi Inderpreet,

     

    Cute kid!! He's growing up fast.

    That circuit would work, I think a lot of the third party audio boards for the Pi ended up using a near-identical chip as that BBB audio project (they used a slightly more recent but pin-compatible part to that TI chip).

    The TI chip was great to work with, and good quality (the same chip is used in a high-end $200 Meridian USB-to-headphone adapter).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago in reply to shabaz

    If I remember correctly, shabaz sir, you did a stereo i2s sound card circuit for the BBB some time back. Theoretically, that can be used here as well. I think I need to read more about that image

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to writerbenjamin

    Hi Benjamin,

     

    The connector on its own won't provide a second channel, because the on-board DAC/Audio amp is mono.

    There is the possibility of adding a second circuit board on top, but I don't know if anyone has tried it.

    It could work out easier to buy a stereo sound card, if you're looking for stereo sound for music.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>