Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Google's Alexa-like Pi AIY Kit, mini teardown
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 4 May 2017 6:30 PM Date Created
  • Views 13371 views
  • Likes 20 likes
  • Comments 66 comments
Related
Recommended
  • aiy google
  • google aiy
  • google sdk
  • google_aiy
  • aiy
  • raspberry_pi
  • raspberry pi
  • amazon alexa
  • aiyproject
  • raspberry pi 3
  • aiy project
  • google embedded sdk
  • raspberry_pi_3

Google's Alexa-like Pi AIY Kit, mini teardown

shabaz
shabaz
4 May 2017

Google has been busy getting stuff attached to MagPi magazines.. I spotted a box containing an 'AIY' kit at the local magazine retailer. Basically it is a card box with some electrical parts and the MagPi magazine.

It is like a cut-down DIY version of Amazon Alexa from what I can tell.

 

They had plenty at closing time, so I suspect there will be lots for people to buy tomorrow too, but from examination it is an audio card and a few peripherals. USB sound cards are cheap these days so that is another option for those who don't/can't purchase the magazine.

Below are photos of the contents of the box (just the electronic bits are shown, there is also a cardboard self-assembly enclosure and the MagPi magazine itself; I might take photos of that later), like a mini-teardown where the teardown is already done.

 

I think it's fair to say the kit component-wise is a little boring, but at least it's cheap. The stereo mic is good to see though. And maybe more projects will be available in future.

Also there are other ways to achieve Alexa-like capability (from both a hardware and PaaS vendor perspective).

For higher quality there are multi-microphone options for Pi, although of course they are more expensive.

 

Where the fun will come in is with the software - it will be a lot of fun to create voice-enabled projects.

Although it is intended to use Google PaaS, not everyone likes sending audio to a cloud, but it is usable for standalone non-Internet-connected audio projects too, e.g. music player. No need to plug in the microphone wires.

 

In summary, it is nice to see traction with voice-enabled natural language assistant projects for hobbyists, and the hardware here is very basic, but at least it keeps interest up and lots of opportunities for those learning programming to have fun and create some cool projects.

 

Some photos and notes follow, as well as any reverse-engineered schematics. Also see the comments section.

 

image

 

Connections Overview

According to google's page, these are the connections (see diagram below). Handily the Pi's I2C, SPI and UART connections are broken out to pads all ready for soldering to the supplied SIL header pins.

There are also some output pins, probably MOSFET driven (can see what looks like SOT-23 sized MOSFETs marked G31 D5 (they are most likely N-channel MOSFETS part code Diodes Inc DMG3420U) on the right of the image along with SMD fuse and diode per output).

See further below for reverse-engineered schematic for that.

 

On the left of the board, there is space for soldering SIL pins for attaching hobby servo motors.

image

Output Drivers

The four drivers (shown on the right side of the diagram above) have most likely the following circuit - I think it is accurate but please let me know in the comments if it isn't:

image

The four MOSFETs are used in an open drain configuration, so the pins marked 'DRIVER' will be switched to ground (0V) whenever the corresponding GPIO pin goes high. If the desired load is 5V powered then the 5V pin can be used to provide power (there is a 500mA resettable fuse). The open drain configuration also allows a lower voltage source to be used to supply the load, and the MOSFET will switch the other end of the load to ground.

The diagram below shows how to connect a relay with a 5V coil. It is inadvisable to use the Driver outputs with a higher voltage despite it being an open drain configuration because current can flow through the diode in the schematic above and the fuse, causing damage.

Also, it is strongly advised not to use this for connecting mains operated equipment, because there are regulations governing what enclosure is used and how the cable is secured and so on. To control mains equipment it is good to use home automation methods such as wireless (there are radio transmitters available for the Pi).

image

 

A suitable relay could be Finder 5V coil SPDT 6A contacts changeover relayFinder 5V coil SPDT 6A contacts changeover relay or Finder SPST 6A relaySPST 6A relay . Both of these relays are very compact (20x10x10mm) and have pins that will fit a breadboard or stripboard so are easy to prototype with. The comments section further below has a photo of how to wire it up and some example Python code to test it by turning the relay on and off. Although these relays can be used with mains, it would be extremely inadvisable to do so without a decent PCB layout (not stripboard!) and other precautions (see here for some reasons). So, the relay control is best used for lower-voltage tasks.

 

Mains Control

One solution is to use wireless control. This can be country or region specific.

UK

I've used an Energenie wireless module before, it is a very small transmitter board that connects to the Pi and wirelessly controls mains sockets. The Energenie kitEnergenie kit comes with the wireless transmitter board and two sockets. It's good value, and meets the relevant electrical standards for the UK. It could be wired to the connections on the left side of the google voice HAT board allocated for Servos for example (by default it needs six GPIO although that number can optionally be reduced if needed).

 

Audio Output

The centre of the board contains the integrated circuit (IC) with the audio digital-to-analog converter and mono audio amplifier inside it, it is Maxim MAX98357A - thanks Inderpreet! (the 16-pin QFN sized IC says AKK BDK on it) and an EEPROM marked 24C32F.

 

image

Power Connections

There is also space for a DC power jack but none is fitted. A DC power jack with thin pins would fit. There is a SOT23-6 part near it, marked K4S DD and a SOT-23 part marked 23X D1 is close too. These two parts have a Q identifier, so are likely some type of transistors.

 

Microphone Board

The microphones are marked 432 QDF21G and are Knowles SPH0645LM4H (thanks again Inderpreet) MEMS digital microphones. They directly output an I2S bitstream.

image

 

The microphone input ports are on the underside:

image

 

This is the schematic of the microphone board, using the information from Inderpreet in the comments below. There may be some minor mistakes (please let me know in the comments section and I'll correct it). In theory the microphone board could be used standalone with the Pi, no need for the main Voice HAT board. It is a convenient breakout board for the surface-mount mics.

 

It could be suitable for small projects, e.g. with the 'Zero or with other boards with an I2S interface. It would be advisable to have a small resistance (e.g. 51 ohms) in series with the LRCLK and BCLK pins if it is connected directly.

There is nothing to stop a voice assistant from working without a speaker (you just won't hear the result, unless the on-board headphone socket on the Pi 3 is used perhaps).

Not all projects would require an audio response. Also, for some projects one may prefer a discreet response in an earphone (e.g. check your calendar by requesting it, but not announcing your plans to everyone).

image

 

Safety Leaflet

This is enclosed in the box:

image

  • Sign in to reply

Top Comments

  • nicklansley
    nicklansley over 9 years ago +5
    I managed to get hold of a copy of MagPi magazine and get it working with a Raspberry Pi 3: www.youtube.com/watch
  • ipv1
    ipv1 over 9 years ago +4
    I have a suspicion that that is not a code but rather an I2S amplifier - MAX98357A I just googled it and sure enough... I have one of those in stock from an unfinished project and just recalled it as I…
  • ipv1
    ipv1 over 9 years ago in reply to shabaz +4
    If I remember correctly, shabaz sir, you did a stereo i2s sound card circuit for the BBB some time back. Theoretically, that can be used here as well. I think I need to read more about that
  • DAB
    DAB over 9 years ago

    Great post.

     

    I just finished reading the MAGPI article on the Kit and it is indeed intriguing.

     

    I would say you get your money's worth of parts with the kit and if the software is as capable as advertised, you could have a lot of fun with it.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago

    Hi sir,

    I forgot to include the part number for the mic It should be SPH0645LM4H since the audio in is on the underside of the device.

     

    Adafruit has the part at https://www.adafruit.com/product/3421

     

    I will be making a small addon on the same lines but while that gets completed, I expect to have a different method working. Fingers crossed.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to ipv1

    Hi Inderpreet,

    Awesome, so now we know what that part number is : )  Excellent detective work!

    Since that is just a DAC/amp and has no ADC, this must mean the mics are digital MEMS ones, i.e. google must have implemented some driver for this (EDIT - I see you've already mentioned these are likely to be I2S, in which case no new driver needed - great).

    I'll probe with a scope over the weekend to prove they are digital, but I'm fairly sure this must be the case since there are no other ICs on the boards other than those mentioned.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago

    I have a suspicion that that is not a code but rather an I2S amplifier - MAX98357A

    I just googled it and sure enough...

    image

    I have one of those in stock from an unfinished project and just recalled it as I was typing this reply - (The human brain is a complex machine)

     

    The microphones are the same ones used in the Cirrus Logic Card and are also I2S Peripherals. I imagine an intern sitting at Google buying these from Adafruit and designing the rest of the PCB around it. MOSFETs seem right though to drive the servos. There should be some PWM generation mechanism in there but I can't see it in the images. Will have a better understanding once the circuit is all traced out. image

     

    Thanks for the brain fodder.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to uscdadnyc

    Hi Edward,

     

    You're right, this would be a cheap way to do that switch for person with disability. I'm in the UK but since we're in a global environment  : ) I sometimes vary between US and UK spellings. Some English spellings feel overly archaic, whereas other spellings are disappearing too fast, e.g. I still like spelling 'encyclopaedia' like that for instance.

    Regarding PaaS  (Platform-as-a-Service), it is the model that google and some other providers use to allow people to create and deliver applications (e.g. google hosts the servers, OS and any other core software that makes up a 'platform' on top of which you can put the higher-level application. The platform often features generic things that apps can make use of like databases, and in this case, voice APIs, for processing any audio sent to it. So, the application doesn't need to implement that, it can just make a call into the platform, using the API.

    So, for an Alexa-style app, really all the coder needs to do is write an app that takes audio from the microphone and pass it to the cloud platform using a voice API. Google's platform will do the rest, and then send back the result which then the app can pass to the loudspeaker. So, the coder is responsible for the app that handles the mic/loudspeaker and sending/receiving data to google, and the google platform does the rest in this case, because the voice and natural language capabilities are part of google's platform service offering.

    Before PaaS, the coder would have been responsible to install or develop a voice library on the system themselves, and maintain it themselves.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>