Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Google's Alexa-like Pi AIY Kit, mini teardown
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 4 May 2017 6:30 PM Date Created
  • Views 13364 views
  • Likes 20 likes
  • Comments 66 comments
Related
Recommended
  • aiy google
  • google aiy
  • google sdk
  • google_aiy
  • aiy
  • raspberry_pi
  • raspberry pi
  • amazon alexa
  • aiyproject
  • raspberry pi 3
  • aiy project
  • google embedded sdk
  • raspberry_pi_3

Google's Alexa-like Pi AIY Kit, mini teardown

shabaz
shabaz
4 May 2017

Google has been busy getting stuff attached to MagPi magazines.. I spotted a box containing an 'AIY' kit at the local magazine retailer. Basically it is a card box with some electrical parts and the MagPi magazine.

It is like a cut-down DIY version of Amazon Alexa from what I can tell.

 

They had plenty at closing time, so I suspect there will be lots for people to buy tomorrow too, but from examination it is an audio card and a few peripherals. USB sound cards are cheap these days so that is another option for those who don't/can't purchase the magazine.

Below are photos of the contents of the box (just the electronic bits are shown, there is also a cardboard self-assembly enclosure and the MagPi magazine itself; I might take photos of that later), like a mini-teardown where the teardown is already done.

 

I think it's fair to say the kit component-wise is a little boring, but at least it's cheap. The stereo mic is good to see though. And maybe more projects will be available in future.

Also there are other ways to achieve Alexa-like capability (from both a hardware and PaaS vendor perspective).

For higher quality there are multi-microphone options for Pi, although of course they are more expensive.

 

Where the fun will come in is with the software - it will be a lot of fun to create voice-enabled projects.

Although it is intended to use Google PaaS, not everyone likes sending audio to a cloud, but it is usable for standalone non-Internet-connected audio projects too, e.g. music player. No need to plug in the microphone wires.

 

In summary, it is nice to see traction with voice-enabled natural language assistant projects for hobbyists, and the hardware here is very basic, but at least it keeps interest up and lots of opportunities for those learning programming to have fun and create some cool projects.

 

Some photos and notes follow, as well as any reverse-engineered schematics. Also see the comments section.

 

image

 

Connections Overview

According to google's page, these are the connections (see diagram below). Handily the Pi's I2C, SPI and UART connections are broken out to pads all ready for soldering to the supplied SIL header pins.

There are also some output pins, probably MOSFET driven (can see what looks like SOT-23 sized MOSFETs marked G31 D5 (they are most likely N-channel MOSFETS part code Diodes Inc DMG3420U) on the right of the image along with SMD fuse and diode per output).

See further below for reverse-engineered schematic for that.

 

On the left of the board, there is space for soldering SIL pins for attaching hobby servo motors.

image

Output Drivers

The four drivers (shown on the right side of the diagram above) have most likely the following circuit - I think it is accurate but please let me know in the comments if it isn't:

image

The four MOSFETs are used in an open drain configuration, so the pins marked 'DRIVER' will be switched to ground (0V) whenever the corresponding GPIO pin goes high. If the desired load is 5V powered then the 5V pin can be used to provide power (there is a 500mA resettable fuse). The open drain configuration also allows a lower voltage source to be used to supply the load, and the MOSFET will switch the other end of the load to ground.

The diagram below shows how to connect a relay with a 5V coil. It is inadvisable to use the Driver outputs with a higher voltage despite it being an open drain configuration because current can flow through the diode in the schematic above and the fuse, causing damage.

Also, it is strongly advised not to use this for connecting mains operated equipment, because there are regulations governing what enclosure is used and how the cable is secured and so on. To control mains equipment it is good to use home automation methods such as wireless (there are radio transmitters available for the Pi).

image

 

A suitable relay could be Finder 5V coil SPDT 6A contacts changeover relayFinder 5V coil SPDT 6A contacts changeover relay or Finder SPST 6A relaySPST 6A relay . Both of these relays are very compact (20x10x10mm) and have pins that will fit a breadboard or stripboard so are easy to prototype with. The comments section further below has a photo of how to wire it up and some example Python code to test it by turning the relay on and off. Although these relays can be used with mains, it would be extremely inadvisable to do so without a decent PCB layout (not stripboard!) and other precautions (see here for some reasons). So, the relay control is best used for lower-voltage tasks.

 

Mains Control

One solution is to use wireless control. This can be country or region specific.

UK

I've used an Energenie wireless module before, it is a very small transmitter board that connects to the Pi and wirelessly controls mains sockets. The Energenie kitEnergenie kit comes with the wireless transmitter board and two sockets. It's good value, and meets the relevant electrical standards for the UK. It could be wired to the connections on the left side of the google voice HAT board allocated for Servos for example (by default it needs six GPIO although that number can optionally be reduced if needed).

 

Audio Output

The centre of the board contains the integrated circuit (IC) with the audio digital-to-analog converter and mono audio amplifier inside it, it is Maxim MAX98357A - thanks Inderpreet! (the 16-pin QFN sized IC says AKK BDK on it) and an EEPROM marked 24C32F.

 

image

Power Connections

There is also space for a DC power jack but none is fitted. A DC power jack with thin pins would fit. There is a SOT23-6 part near it, marked K4S DD and a SOT-23 part marked 23X D1 is close too. These two parts have a Q identifier, so are likely some type of transistors.

 

Microphone Board

The microphones are marked 432 QDF21G and are Knowles SPH0645LM4H (thanks again Inderpreet) MEMS digital microphones. They directly output an I2S bitstream.

image

 

The microphone input ports are on the underside:

image

 

This is the schematic of the microphone board, using the information from Inderpreet in the comments below. There may be some minor mistakes (please let me know in the comments section and I'll correct it). In theory the microphone board could be used standalone with the Pi, no need for the main Voice HAT board. It is a convenient breakout board for the surface-mount mics.

 

It could be suitable for small projects, e.g. with the 'Zero or with other boards with an I2S interface. It would be advisable to have a small resistance (e.g. 51 ohms) in series with the LRCLK and BCLK pins if it is connected directly.

There is nothing to stop a voice assistant from working without a speaker (you just won't hear the result, unless the on-board headphone socket on the Pi 3 is used perhaps).

Not all projects would require an audio response. Also, for some projects one may prefer a discreet response in an earphone (e.g. check your calendar by requesting it, but not announcing your plans to everyone).

image

 

Safety Leaflet

This is enclosed in the box:

image

  • Sign in to reply

Top Comments

  • nicklansley
    nicklansley over 9 years ago +5
    I managed to get hold of a copy of MagPi magazine and get it working with a Raspberry Pi 3: www.youtube.com/watch
  • ipv1
    ipv1 over 9 years ago +4
    I have a suspicion that that is not a code but rather an I2S amplifier - MAX98357A I just googled it and sure enough... I have one of those in stock from an unfinished project and just recalled it as I…
  • ipv1
    ipv1 over 9 years ago in reply to shabaz +4
    If I remember correctly, shabaz sir, you did a stereo i2s sound card circuit for the BBB some time back. Theoretically, that can be used here as well. I think I need to read more about that
  • peakon28
    peakon28 over 9 years ago

    I wonder why do Google need to use an EPROM on the audio output section of the Voice Hat?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jhewitt123
    jhewitt123 over 9 years ago in reply to shabaz

    Yes, I am trying to investigate more on their community to compare the platforms and further the technology in general.

    The developers, originally from google open assistant at least seem to think the modular nature of their code is amenable to unattached mode, ie. no WiFI, but they said it is or would be 'tricky' on the Pi. Trying their image with no sound board, just usb mike and a speaker.

     

    Also the voiceHAT seems like it has alarms, and says one is set after I say 'set alarm for 5 minutes,' but then when I say'cancel alarm' it says 'there are no alarms'. This is no way to run a tight ship I think.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 4ntoine
    4ntoine over 9 years ago

    Excellent work, that's what i've been looking for! I will try to solder it myself

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to jhewitt123

    Hi John,

     

    According to the Mycroft kickstarter page under the section 'How Mycroft Works' it says it does use the cloud, so it will need WiFi or Ethernet to function. In theory it could be possible to have a script that periodically kills the application and restarts it if there is a bug that makes it fail after a while. Not as ideal as resolving the actual bug of course. Or as you say some alternate solution if you need this functioning without WiFi/Ethernet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to marc@raspberrypi.org

    Hi Marc,

    No problem at all, feel free to use the schematic for the educational resource. As you say, I drew the schematic, (i.e. it was not copied from anywhere) so you have permission. Good luck with the resource effort, it's great that kids will benefit from your work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>