Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Home Automation using smart radio devices
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mistertee
  • Date Created: 8 Oct 2015 1:33 PM Date Created
  • Views 2855 views
  • Likes 3 likes
  • Comments 11 comments
Related
Recommended
  • raspberry
  • pi
  • fm
  • radio
  • arduino
  • modules

Home Automation using smart radio devices

mistertee
mistertee
8 Oct 2015

When putting together a Home Automation System together it is often necessary to gather analogue data. This could be from temperature / humidity sensors or to measure battery voltage. Often these are remote to the computing module which could be a Raspberry Pi, and Arduino or a PC - for example when gathering data from a weather station on the roof of a building.

 

This example below shows how the DART and the URR could be used to gather useful information from around the home.

 

image

 

The Dual Analogue Radio Transmitter (DART) is a battery powered device using FM transmission at 433 MHz. This gives it superior performance to AM modules. The low power design enables the user to get nearly 18 months life out of 3 x AAA cells.

 

The Universal Radio Receiver interface to a number of DART devices and outputs the received data out on a serial port, where it can be acted upon by a Raspberry Pi, a PC or an Arduino.

 

In the above example, the DART in the garage is used to monitor the freezer temperature using a TMP36 measurement device which connects simply to the DART. The other (analogue) input of the DART is used to measure the voltage out of a charger. When there is power to the garage the DART sends out 255 and when there is no power it sends out 0.

 

The drawing above shows other DART devices connected to monitor fridge temeprature, a PIR in the bedroom and humidity and door status in the shed.

 

Click here for more information on the DART and the URR.

 

Summary

 

These Radio devices using FM modules gives superior range and allows the user to monitor the status of various appliances around the home.

  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 10 years ago +1
    I have been using Ti boards with ZigBee radios. It works better than WiFi. {main CPU TI CC3200 or others, do not need WiFi, RJ45 will do nicely.} + Thermostat, & house interface(1/4 VGA touch panel)[ZigBee…
  • mistertee
    mistertee over 10 years ago in reply to phoenixcomm +1
    Hi Cristina, thats awesome and where I would like to be. Any chance of a blog post on the challenges you faced when you were doing this? I guess this is a hobby and not a commercial system. Had you used…
  • DAB
    DAB over 10 years ago

    I wonder, could you use these radios to build a link of stations?

     

    I am thinking about primitive sites where you need to establish your own radio links for remote communication support.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<