Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Insight into lan78xx driver support for Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 20 Jun 2021 5:59 PM Date Created
  • Views 8591 views
  • Likes 2 likes
  • Comments 13 comments
Related
Recommended

Insight into lan78xx driver support for Pi

colporteur
colporteur
20 Jun 2021

Does anyone have any insight into lan78xx usb driver support for the Raspberry Pi?

 

I am attempting to use a Microchip PoE USB-C device to enabling networking to a Raspberry Pi4B. The work is part of a RoadTest for Microchip PoE to USB-CRegistered Power and Data Adapter .

 

A quick check with a command line lsmod shows no lan78xx driver. There is no /lib/modules/5.10.17-v7l+/kernel/net/usb to support the lan78xx as suggested in some posts I have found.

 

I did find this post https://wiki.seeedstudio.com/Dual-Gigabit-Ethernet-Carrier-Board-for-Raspberry-Pi-CM4/   and successfully completed the procedure for an Ethernet Port configuration.

image

 

A lan7800 module reference does appear for a command line lsmod after the install. The Microchip PoE USB-C lan7800 port is not detected when connected to the Pi. Still no reference to a lan78xx module appears in the directory structure.

 

The vendors site https://www.microchip.com/wwwproducts/en/LAN7800  indicates there has been support in the Linux kernel. My searches for Pi driver support has been limited. My understanding is lan78xx is a modules in the usb subdirectory when installed. I'm not seeing that for this kludge.

 

I'm thinking maybe I need a a dtsoverlay in the config.txt directory. Really not sure. I have gone as far as to load Ubuntu for the Pi to see if it is O/S related. That didn't prove fruitful.

 

I welcome any insight community members may have regarding network driver installs for the Pi. I will continue to hunt and peck to see if there is anything I have missed.

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 5 years ago in reply to colporteur +3
    I actually got inspired to put it in based on this post: https://www.raspberrypi.org/forums/viewtopic.php?t=246348#p1504603 - Gough
  • Gough Lui
    Gough Lui over 5 years ago +2
    I have the unit working on my Raspberry Pi 4 (but needing a USB-C to A OTG adapter + USB-A to USB-C cable because mine is the version with the CC pin issue , so using the included captive USB-C to USB…
  • colporteur
    colporteur over 5 years ago in reply to skruglewicz +2
    Yes.
  • Gough Lui
    Gough Lui over 5 years ago

    I have the unit working on my Raspberry Pi 4 (but needing a USB-C to A OTG adapter + USB-A to USB-C cable because mine is the version with the CC pin issue, so using the included captive USB-C to USB-C results in no LED/no power).

     

    In config.txt, I added otg_mode=1

    This is mandatory to enable the USB 2.0 OTG controller that services the USB-C port's data pins. If you don't add this line, you will only get power and no USB-Ethernet detection.

     

    On startup, it is automatically picked up on my installation of Raspberry Pi OS (Raspbian):

    [
    0.000000] Linux version 5.10.17-v7l+ (dom@buildbot) (arm-linux-gnueabihf-gcc-8 (Ubuntu/Linaro 8.4.0-3ubuntu1) 8.4.0, GNU ld (GNU Binutils for Ubuntu) 2.34) #1414 SMP Fri Apr 30 13:20:47 BST 2021
    [
    1.394777] usbcore: registered new interface driver lan78xx
    [
    1.984215] usb 3-1: New USB device found, idVendor=0424, idProduct=7800, bcdDevice= 3.00
    [
    1.984263] usb 3-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
    [
    1.984296] usb 3-1: Product: LAN7800
    [
    1.984324] usb 3-1: Manufacturer: Microchip
    [
    1.984353] usb 3-1: SerialNumber: 210460000404
    [
    2.271146] libphy: lan78xx-mdiobus: probed
    [
    2.271192] lan78xx 3-1:1.0 (unnamed net_device) (uninitialized): int urb period 64

     

    I did not need to install any drivers at all to get it working. I wasn't going to write about this until I delivered my RoadTest ... but seeing that you're rushing ahead into blogging, I thought I'd mention it.

     

    Why does your kernel command line have initcall_blacklist=lan78xx_driver_init? That's perhaps not a good thing ... could stop a driver from loading. Perhaps start from a fresh Raspberry Pi OS (Raspbian) and add otg_mode=1 and it should just work.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    (On that page, under the Document tab, there is a driver section.

    If you click the one for the kernel version of your OS, you get a link to the driver tarball.)

     

    Edit: seems from your comments that you are on kernel 5.10. I didn't find a driver for it . But when I check linux git (and raspberry git), it seems to be part of the base code now. Odd.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 5 years ago

    Doesn't the PI 4 have a type c power connector?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<