Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Mains power control
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 13 Jul 2014 2:30 PM Date Created
  • Views 4687 views
  • Likes 4 likes
  • Comments 17 comments
Related
Recommended
  • mains
  • compliance
  • regulations
  • safety

Mains power control

shabaz
shabaz
13 Jul 2014

(This post was prompted by seeing a recent kickstarter project that some people may wish to use for direct mains control.).

 

It may be obvious, but using prototyping strip-board is not advisable for mains control.

It may not injure you, but may kill others who use the project, leaving you morally and legally liable.

Some less obvious things to non-engineers are things like strain relief, flame retardant materials, poor crimps, insulating barrier requirements and use of badly rated/designed cheap components that will never be compliant.

Here are some examples of designs not compliant in at least Europe (these images are reduced in resolution/cropped for fair use):

image

 

image

If you want to directly switch mains power, then avoid this type of design too, it is from a recent kickstarter claimed suitable for reflow oven use with a Raspberry Pi:

image

image

 

Here is another example of a UK product called the Mains Switch Widget - this extract is from the user documentation (extract is legal under fair use):

image

The above rings alarm bells for several reasons. The text in the user documentation snippet above states "this will help to anchor the connections in place" - is this valid according to standards in Europe? According to my understanding the method of clamping has to be well defined, so suggesting that hot glue is not essential but _may_ be used to help is confusing and not well defined, because either the method of clamping is sufficient to comply, or it is not. Also, how does a user know if it is secure? A cable tie can be tied by some people weakly, and by others more securely. Users will not know the test to apply to ensure it is compliant.

Also, the cable tie is wrongly applied to the cable in the photo above, since it should be further back from the unsheathed end. Note that this is not my photo, it is the photo from the product documentation!

 

Furthermore, for safety, since this is a permanently attached mains cable, the earth connection in the opinion of several engineers, should be the last to be stressed if there is any issue with the clamping of the cable.

 

When these points were raised with the creator of the Mains Switch Widget on this forum, the text silently changed in the user documentation - see here:

image

However, it is difficult to see how a documentation change can improve the situation much. The photo still shows the same length wires and cable tie too close to the unsheathed end.

 

Do check out the comments to the post below, for useful information.

A safe solution that requires no wiring is the Energenie modules - at £16.95+VAT for two of them, it appears well priced and safe. It is also cheaper than the Mains Switch Widget. I tried the Energenie modules out, and it was easy to get them working and controlled by the Raspberry Pi and with other microcontroller boards (they can be controlled via a remote control or via the Raspberry Pi etc.).

image

  • Sign in to reply

Top Comments

  • gadget.iom
    gadget.iom over 11 years ago +2
    In terms of physical design this approach seems to be safer:
  • gadget.iom
    gadget.iom over 11 years ago in reply to shabaz +2
    Indeed. From an electrical safety perspective they seem far superior. A non-electrically minded person can use them without resorting to any mains wiring, and if the relay and wiring/traces are rated over…
  • mcb1
    mcb1 over 12 years ago +1
    Shabaz Looking at them ...(and cringing) they aren't compliant in New Zealand (or Australia) either. The middle one doesn't even have strain relief, and the least they could have done is made the earth…
  • gadget.iom
    gadget.iom over 11 years ago

    Not specifically Pi related, but this always sends shivers down my spine!

    http://www.anthony-dacko.net/PSTN-DTMF-Unit.htm

     

    ...of particular interest is the fact that despite lots of (annoying) flashing warning images he continues to wire the circuit in a switched-neutral configuration.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to shabaz

    yup, in fact as you say, the only securing is the strength of the GPIO connector, as these ovens get moved around abit from time to time, there is a chance of a heavy or moderate bounce on a table dislodging the board from the PI and then BANG. No more PI in the oven image, well a crispy one anyway (Over done either way). This is in addition to all the other stuff we have already mentioned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to Robert Peter Oakes

    Hi Peter,

     

    I agree, #1 is least likely to cause an issue by being tugged. The middle one violates a few more rules (at least in Europe) I think - not entirely sure - that soldered to board wires are not acceptable for the mains input (I could be wrong on that), and also some barrier is needed to prevent strands of wire making their way across the gap. The bottom one would fail all tug tests, because it is secured only by the 26-way connector, and huge risk to touch the Ethernet connector on the underside. It's bad in general, I think they had little regard for usability and for the safety of the user, since if the user wants to place it in an enclosure there are no mounting points as you say.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    Looking at the pictures, aside from the fact it is on Vero board, the first one is probably the safest out of all of these. And is not bound by the codes as it is obviously built for personal use (Or I would hope so image )

     

    It is well mounted, strong strain relief on the mains cable, outlet is screwed down and no exposed connectors, we can not see the underside of the relay so we don't know the protective measures taken there but based on the rest, probably some Vero traces ripped out to provide additional clearance, even a slight indication of insulating tape on the bottom of the board, even though it is well glued down to the wood. Does it meet code, of course not but it looks like the creator has taken the time to make it reasonably safe considering the type of construction.

     

    The PI Plate temp controller is lightly to be the one to shock people because who is not used to simply pulling the USB cable out, and then grabbing the board to take it apart. It would be far better to be at the end of a length of ribbon cable, with mounting holes to allow secure mounting . Oh and a BIG warning label about high and lethal voltages being present... It has none of that.

     

    The middle board simple needs some strain relief (Even a cable tie or two on the inside side of the grommets would have worked there and added significant safety for so little cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    He did make some semi-permanent attempts at strain relief.

     

    Some people though have no idea when it comes to Mains voltages.

    We even saw it here with the Piface Digital, until I complained loudly.

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>