• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Minecraft on the Raspberry Pi Model B+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: biglesp
  • Date Created: 2 Dec 2014 8:31 AM Date Created
  • Views 3029 views
  • Likes 9 likes
  • Comments 13 comments
Related
Recommended
  • tutorial
  • minecraft
  • b+
  • rpibeginner
  • raspberry_pi
  • raspberry-pi
  • tutorials

Minecraft on the Raspberry Pi Model B+

biglesp
biglesp
2 Dec 2014

Can you learn with Minecraft?

 

The Raspberry Pi is the ideal platform for learning and there are two great ways to learn coding, and they are physical computing and Minecraft.

  • Physical computing merges the code with electronics to produce all manner of cool projects. We can use all manner of electronic components, such as ultrasonic sensors as inputs and LEDs or buzzers as outputs.
  • Minecraft is also an exciting way to introduce coding and by mixing these two ideas together we can create an exciting introduction to the world of coding and hardware hacking.

image

 

 

The B+ has been designed for embedded projects and can be easily integrated in to many physical projects such as robotics, scientific data collection and flight capable projects.

 

Attaching an add on board to the B+ is managed in exactly the same manner as previous models thanks to a standardised 40 pin GPIO. The first 26 pins of the GPIO are fully compatible with the A and B series of Raspberry Pi, enabling you access to a wealth of great add on boards. The B+ comes with a 40 pin GPIO just like the B+ and this enables future add on board to use the new HAT specification from the Raspberry Pi Foundation. The HAT specification uses pins 27 and 28 of the new GPIO to communicate between the add on board and the Raspberry Pi, enabling the board to instruct the Pi as to how it should be configured.

 

image

 

What better introduction to your new Raspberry Pi B+ than to delve in to the world of Minecraft and learn a little Python and electronics along the way.

 

Getting Started with Minecraft

 

Minecraft is a game created by Swedish programmer Markus "Notch" Persson and later developed and published by the Swedish company Mohjang since 2009. In recent news Minecraft is now owned by Microsoft, who purchased Mohjang in November 2014 for $2.5 billion.

 

Minecraft is available on most platforms, from cell phones to Playstation 4. But where it is most interesting is on the Raspberry Pi.

 

Why is it interesting on the Raspberry Pi?

The Raspberry Pi version of Minecraft comes with a Python API
(Application Programming Interface) that enables us to interact and alter the Minecraft world using Python and as we are using Python we can also like our Minecraft projects to the real world thanks to the GPIO and the Rpi.GPIO Python library.

 

As of September 2014 the latest version of Raspbian comes with Minecraft pre-installed and ready for hacking and this is the easiest way to start this project. You can download the latest Raspbian and find full instructions on how to copy it to your micro SD card via the Raspberry Pi website http://www.raspberrypi.org/downloads/.

 

Getting started

With Raspbian installed on your micro SD card, connect all of the peripherals required to your Raspberry Pi, remember to attach the power last. Switch on your Raspberry Pi B+ and wait for it to boot.

If this is your first boot then the raspi-config application will automatically load and ask you to configure your Raspberry Pi. At this stage we do not need to enable any special configurations, so you can move the cursor to Finish and press Enter to exit the application.


Your Raspberry Pi will now ask you to login, and the default login details are

 

Username: pi
Password: raspberry
                                                            

 

When typing in your password the screen will not print the password to the screen, this is a normal security feature for Linux and prevents anyone from snooping your password from afar.

You will now see a prompt waiting for input, type in the following and then press enter.

 

startx
                                                            


After a few seconds the familiar Raspbian desktop will be loaded ready for use.

Firstly open a terminal using LXTerminal and type in the following and then press enter.

 

sudo idle &
                                                            


This load the idle Python editor with root priveleges, something that is needed in order for us to use the GPIO in our projects. You may be wondering what the “&” does? Well this is a Linux trick to inform the operating system that the command being run, in this case “sudo idle”, should be run and then put in to the background. This frees up the terminal for any other commands that we wish to run. With idle ready to hack, change to the Raspberry Pi second desktop via the desktop switcher in the bottom left of the screen. You can easily change back later. We do this as Minecraft has a habit of running it's window over all the other windows on the screen.

 

On the second desktop double left click on the Minecraft icon to load the application. Start a new game and create a new world. If you already have a world, you can load up that world instead. Once loaded you will be dropped inside of the Minecraft world. Take some time to look around and get a feel for the controls.

 

  • Mouse – Controls where Steve looks
  • Left Mouse Button – Destroys blocks
  • Right Mouse Button – Places blocks
  • W – Moves Steve forward
  • A – Moves Steve left
  • S – Moves Steve backwards
  • D – Moves Steve right
  • E – Opens the inventory of all block types available
  • Esc – Back to menu

 

Now that you are familiar with the Minecraft world, press the Tab key to release your mouse and return to the first desktop via the desktop switcher in the bottom left of the screen.

 

To build this project you will need

 

  • Raspberry Pi B+
  • Raspbian installed on a micro SD card
  • Mouse
  • Keyboard
  • Power Supply
  • HDMI lead
  • TV with HDMI
  • Solderless breadboard
  • Push button
  • Male to female jumper leads
  • 220 Ohm resistors
  • 1.8V LED

 

In this blog post we will discover more about the B+ and Minecraft via three simple to learn projects.

These three mini projects are

 

Project 1: Writing to the chat - Our “Hello World” test to make sure that everything is set up accordingly.

Project 2: Push button teleport - Linking the physical world with the digital, using a push button to teleport Steve around the Minecraft world.

Project 3: Control an LED – It would be great to use an LED to indicate that our teleporter is working.

 

Project 1 – Writing to the chat window

Minecraft has a built in chat window, which enables players in multi-player games to talk amongst one another. In this tutorial we will use this chat system as an output for messages from Python.

 

During our setup we have already loaded Minecraft and it is waiting for us on the second desktop. But before we go back to Minecraft, let us create a new file in idle, click on File >> New Window to launch a new blank document for our project.

 

image

 

We start our project by enabling the Minecraft API for Python, and to do this we import the Minecraft module into our project.

 

 

You'll see that we import the module “mcpi.minecraft” and change it's name to just “minecraft” we do this as it makes it easier to work with.

With the import complete we move on to the next line of code.

 

 

In this line of code we create a variable, a container, called “mc” and in the variable we store the string “minecraft.Minecraft.create()” which will create a connection between our Python project and Minecraft.

 

Our final line of code simply calls the postToChat function and we pass if the string “Hello World”, not very original but a great test to make sure that everything is working.

 

 

To run your code, firstly you will need to save it, and to do this click on File >> Save. Save it to your home directory and give the file a name, but please do not save it as minecraft.py or Minecraft.py as this may cause issues in future.

With your project saved click on Run >> Run Module and then quickly switch back to the desktop with Minecraft using the desktop switcher icon.

 

You should see this on the screen.

 

image

 

Extension Activity – Countdown

 

Now that we have a method to post to the chat window, let's use it to create a countdown.

 

Using the code that we just created as a base let's alter it to meet our needs.

 

 

As you can see in the code we import the sleep function from the time module, this enables us to control the speed of our project. Next we create a new variable called “n” in which we store the integer 5 this will be the start of our countdown. We next use a conditional statement that states.

 

While the value of “n” is greater than 0
Post it's value to the Minecraft chat window
Sleep for 1 second
Change the value of “n” by subtracting 1 from it's current value.
                 

 

Try this code in your project and quickly switch back to Minecraft. You should see the chat window appear and a countdown happen.

 

image

 

Project 2 – Push button teleport

During our setup we have already loaded Minecraft and it is waiting for us on the second desktop. But before we go back to Minecraft, let us create a new file in idle, click on File >> New Window to launch a new blank document for our project.

 

image

 

We start our project by enabling the Minecraft API for Python, and to do this we import the Minecraft module into our project.

 

 

This is followed by three further imports, the first RPi.GPIO enables access to the GPIO. We again import sleep from the time module, and finally we import the random integer function from the random library, we will use this to select random numbers later in the project.

 

 

Our next two lines of code handle the GPIO. The first instructs the module that we will be using the Broadcom pin mapping for our GPIO pins (refer to the GPIO layout image for reference) The second line instructs the GPIO library that pin 17 is an input and that we will set it to be high by default.

 

 

In our next section of code we create an infinite loop using while True: Inside of this loop we create a condition that says.

 

If the button attached to pin 17 is pressed
Choose a random number between 0 and 100
Choose a random number between 0 and 100
Choose a random number between 0 and 100
Wait for the button press to finish
Get the players current position in the game world
Change the players position using the values stored in a,b,c (these correspond to x,y,z)
Post to chat “Energize” because I am a Star Trek geek.
Wait for 5 seconds and then the process repeats.
                                                  

 

Type this code into IDLE and save the file. Now we will build a simple circuit using the hardware components. Connect up the components as per the diagram.

image

 

When your wiring is complete, run the project in idle via Run >> Run Module and then quickly swap back to Minecraft using the desktop switcher. When ready press the button on your breadboard.

 

imageimage

 

Steve will be teleported to a new location on the map, if he gets stuck press the button again.

 

Project 3 – Adding an LED to our teleporter

For our last project we expand upon Project 2 by adding a physical output to our teleporter. So let's take a look at the code.

 

We will reuse the code from project 2.

 

 

Our first addition is setting up pin 27 as an output, we will attach an LED to this pin later in the project.


 

When the button is triggered the LED will light up.

 


The LED will now turn off.




Now we will build a simple circuit using the rest of the hardware components. Connect up the components as per the diagram.

 

image

 

When your wiring is complete, run the project in idle via Run >> Run Module and then quickly swap back to Minecraft using the desktop switcher. When ready press the button on your breadboard.

Steve will be teleported around the Minecraft world and the LED on your breadboard will light up.


Congratulations, you have taken your first steps with Minecraft on your Raspberry Pi B+.

 

All of the code for these projects can be found on my Github page.

  • Sign in to reply

Top Comments

  • biglesp
    biglesp over 11 years ago in reply to gadget.iom +2
    Thank-you very much for your kind comment. The scope of the project was to encourage anyone to try something new and learn more about their new Raspberry Pi. I'll produce a further tutorial to expand upon…
  • biglesp
    biglesp over 11 years ago in reply to markvenn +2
    Sure A simple tactile switch can be wired up as per project 2. Create a house with doorway, make a note of the x,yz co-ordinates of the door. When the button is pressed, instruct Minecraft to remove the…
  • gadget.iom
    gadget.iom over 11 years ago +1
    This is an excellent tutorial. A great way to get younger people interested in interfacing with their pi.
  • brianchadorourke
    brianchadorourke over 11 years ago

    Great tutorial.  I have a couple of pi's and I have lots of fun with them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • williamhyland88
    williamhyland88 over 11 years ago

    I cant wait to do this it looks so fun

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago

    Thanks for sharing!

    Great work!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Just got my first Raspberry PI (model b+) and I came across this great write up.  I am new to programming (some linux) and I have never used minecraft.  So what a GREAT way to get started with my new Raspberry PI.  The write up is excellent and the diagrams are really easy to read too.

     

    Here is hoping you expand on this project in the near future.

     

    Thanks for the great work.

     

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    Have you explored the official Raspberry Pi site: Raspberry Pi

    There are some fairly active forums on there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>