• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog New Raspbian version "Pixel"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 4 Jan 2017 5:48 PM Date Created
  • Views 3988 views
  • Likes 4 likes
  • Comments 19 comments
Related
Recommended
  • operating system
  • jessie pixel
  • keyboard
  • ssh disabled
  • hdmi
  • ssh access
  • remote access
  • jessie
  • warning
  • sudo_open
  • configuration
  • mouse
  • raspberry pi 3

New Raspbian version "Pixel"

balearicdynamics
balearicdynamics
4 Jan 2017

I decided to write this post due a silly trap that to be honest I think should be avoided in next updated of the raspbian pixel version. The last official downloadable version at the date is the 2016-11-25-raspbian-jessie.img

 

Here and there there are tons of posts of users that are not able to connect via SSH to a fresh raspbain installation on a PI3 of this version; I had the same problem too and tried to solve the problem thinking to the most common issues like removing the .ssh/known_hosts, check and double check the device IP address etc.

My fault is that I have not read the pixel version release notes, but IMHO the bigger fault is what they wrote in the release notes of this version. Don't forget that the Raspberry PI 3B like the previous models as well is primarily an embedded Linux device headless, it borns headless and any further element to be added to the original system - I mean keyboard, mouse, screen at least - should be considered something extra, not provided with the original hardware.

 

The consideration is: if I am a newbie and I buy a Raspberry Pi 3B then I install the last, modern and updated native operating system on the device, I must be able to run and access to it without to be obliged to buy or have in-house a keyboard, a mouse and a HDMI device. Absolutely not! Instead the problem is just this as you can read in the few lines above, the release notes referred to the mentioned release.

2016-11-25: 
* SSH disabled by default; can be enabled by creating a file with name "ssh" in boot partition
* Prompt for password change at boot when SSH enabled with default password unchanged
* Adobe Flash Player included * Updates to hardware video acceleration in Chromium browser
* Greeter now uses background image from last set in Appearance Settings rather than pi user
* Updated version of Scratch
* Rastrack option removed from raspi-config and Raspberry Pi Configuration
* Ability to disable graphical boot splash screen added to raspi-config and Raspberry Pi Configuration
* Appearance Settings dialog made tabbed to work better on small screens
* Raspberry Pi Configuration now requires current password to change password
* Various small bug fixes
* Updated firmware and kernel

The only possible workaround is to install a previous version (I suggest the 2016-05-27-raspbian-jessie.img image) then update/upgrade the system to the pixel version that - hopefully - should not change the previous installation settings, including the ssh accessibility from the LAN.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to beacon_dave +3
    Yes, that's how to do it. Works perfectly (meanwhile, @self keeps the rant for himself that he wants to post in each discussion about the Pi guys deciding to shut down SSH instead of enforcing a default…
  • clem57
    clem57 over 9 years ago +2
    I have blogged elsewhere that a file called "ssh" with nothing in it gives 1 time access to SSH. When the boot up occurs, the file is deleted to prevent another attempt( That does not stop another try…
  • beacon_dave
    beacon_dave over 9 years ago in reply to balearicdynamics +2
    How about taking an Arduino Micro and turning it into a USB HID macro playback device so as to replay the necessary mouse and keyboard input into one of the R-Pi USB ports so as to turn on the SSH / VNC…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to beacon_dave

    Yes, that's how to do it. Works perfectly (meanwhile, @self keeps the rant for himself that he wants to post in each discussion about the Pi guys deciding to shut down SSH instead of enforcing a default password change)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to clem57

    Nice, worth than expected.

     

    In the meantime I have done also a test. A HDMI TV connected to the the pi with bluetooth keyboard and a Logitech touch. Apparently it's perfect but obviously the Bluetooth is not set until you don't access to the PI from somewhere so the result is a couple of useless devices. If the - poor - newbie decide to buy a wireless keyboard and mouse (finally it is possible with the PI3 !!! image ) he should anyway use a USB device to connect to the system and setup the minimal settings for the device management. It sounds like a blocking update.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago

    Hi Enrico,

     

    I'm just about to encounter this scenario myself as a R-Pi 3 'newb'.

     

    Can't you just add the 'ssh' file to the SD card after flashing the Raspbian image as described ?

     

    "For headless setup, SSH can be enabled by placing a file named 'ssh', without any extension, onto the boot partition of the SD card."

    https://www.raspberrypi.org/documentation/remote-access/ssh/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago

    I have blogged elsewhere that a file called "ssh" with nothing in it gives 1 time access to SSH. When the boot up occurs, the file is deleted to prevent another attempt(imageThat does not stop another try with "ssh" in boot partition).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<