• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog New Raspbian version "Pixel"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 4 Jan 2017 5:48 PM Date Created
  • Views 3987 views
  • Likes 4 likes
  • Comments 19 comments
Related
Recommended
  • operating system
  • jessie pixel
  • keyboard
  • ssh disabled
  • hdmi
  • ssh access
  • remote access
  • jessie
  • warning
  • sudo_open
  • configuration
  • mouse
  • raspberry pi 3

New Raspbian version "Pixel"

balearicdynamics
balearicdynamics
4 Jan 2017

I decided to write this post due a silly trap that to be honest I think should be avoided in next updated of the raspbian pixel version. The last official downloadable version at the date is the 2016-11-25-raspbian-jessie.img

 

Here and there there are tons of posts of users that are not able to connect via SSH to a fresh raspbain installation on a PI3 of this version; I had the same problem too and tried to solve the problem thinking to the most common issues like removing the .ssh/known_hosts, check and double check the device IP address etc.

My fault is that I have not read the pixel version release notes, but IMHO the bigger fault is what they wrote in the release notes of this version. Don't forget that the Raspberry PI 3B like the previous models as well is primarily an embedded Linux device headless, it borns headless and any further element to be added to the original system - I mean keyboard, mouse, screen at least - should be considered something extra, not provided with the original hardware.

 

The consideration is: if I am a newbie and I buy a Raspberry Pi 3B then I install the last, modern and updated native operating system on the device, I must be able to run and access to it without to be obliged to buy or have in-house a keyboard, a mouse and a HDMI device. Absolutely not! Instead the problem is just this as you can read in the few lines above, the release notes referred to the mentioned release.

2016-11-25: 
* SSH disabled by default; can be enabled by creating a file with name "ssh" in boot partition
* Prompt for password change at boot when SSH enabled with default password unchanged
* Adobe Flash Player included * Updates to hardware video acceleration in Chromium browser
* Greeter now uses background image from last set in Appearance Settings rather than pi user
* Updated version of Scratch
* Rastrack option removed from raspi-config and Raspberry Pi Configuration
* Ability to disable graphical boot splash screen added to raspi-config and Raspberry Pi Configuration
* Appearance Settings dialog made tabbed to work better on small screens
* Raspberry Pi Configuration now requires current password to change password
* Various small bug fixes
* Updated firmware and kernel

The only possible workaround is to install a previous version (I suggest the 2016-05-27-raspbian-jessie.img image) then update/upgrade the system to the pixel version that - hopefully - should not change the previous installation settings, including the ssh accessibility from the LAN.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to beacon_dave +3
    Yes, that's how to do it. Works perfectly (meanwhile, @self keeps the rant for himself that he wants to post in each discussion about the Pi guys deciding to shut down SSH instead of enforcing a default…
  • clem57
    clem57 over 9 years ago +2
    I have blogged elsewhere that a file called "ssh" with nothing in it gives 1 time access to SSH. When the boot up occurs, the file is deleted to prevent another attempt( That does not stop another try…
  • beacon_dave
    beacon_dave over 9 years ago in reply to balearicdynamics +2
    How about taking an Arduino Micro and turning it into a USB HID macro playback device so as to replay the necessary mouse and keyboard input into one of the R-Pi USB ports so as to turn on the SSH / VNC…
  • beacon_dave
    beacon_dave over 9 years ago in reply to balearicdynamics

    How about taking an Arduino Micro and turning it into a USB HID macro playback device so as to replay the necessary mouse and keyboard input into one of the R-Pi USB ports so as to turn on the SSH / VNC settings via the Pixel GUI... image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Jan Cumps

    Jan, I was not aware of this, But this is not the way we should think for a valid distro IMHO.

     

    Good to know anyway.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to clem57

    I understand the trigger and the problem. The applied solution [keyboard refuses to type what I'm thinking of it]

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to Jan Cumps

    I think news like this http://www.networkworld.com/article/3141579/security/akamai-look-for-iot-devices-to-attack-during-thanksgiving-christmas… has shaken the RPI foundation to change. But they seem to want to lessen roadblocks to new people using the Pi at the same time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to beacon_dave

    Hello Dave,

     

    I am almost sure that you can't. Ate least you can't do it in a 100% secure way because as far as I know when the system boot a ram disk is loaded in memory with something and the boot partition is something that may result corrupted it managed externally. But should be verified as I am not a super expert on how the boot mechanism works in this specific Linux environment.

     

    Ufnortunately I should also add another wrong thing; always in the release notes thay says that now the Raspberry Pi has the real VNC so - it seems they declare considering obvious - "you now did not have the ssh access (stupid also for a Linux newbie as he never will learn what really Linux is and one of its most powerful features. Instead it is not true. I have tested installing the VNC Viewer on my laptop and tried to connect to the PI IP Address. The response is always connecton refused. The reason? Because the VNC server really exists but NOT active by default.

     

    I have the personal sensation that someone got this new distro in the hands of a Windows developer image image image

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>