Raspberry Pi
  • Products
  • More
Raspberry Pi
Blog Raspberry Pi 2 ADS-B Receiver
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 4 May 2015 3:59 PM Date Created
  • Views 5870 views
  • Likes 20 likes
  • Comments 22 comments
Related
Recommended
  • raspberry
  • pi
  • defined
  • software_defined_radio
  • raspberry_pi
  • radio
  • radar
  • raspberry_pi_2
  • raspberry_pi_space
  • sdr
  • rtl2832u
  • model_b
  • adsb
  • rtl-sdr
  • rtl2832
  • software

Raspberry Pi 2 ADS-B Receiver

e14 Contributor
e14 Contributor
4 May 2015

Why build a radar?

If you have an interest in aircraft then a cheap and easy way to receive details of aircraft near to you is using a cheap USB TV tuner as a software defined radio to decode aircraft radar transponder transmissions. Modern transponders can transmit more than just a squawk code and altitude allowing you to see their identity, position, speed and direction, and a Raspberry Pi is cheap enough to dedicate to the task. Tuners can be had from eBay for less than £10. Here's the hardware I'm using to test:

image

Software setup

Starting with the latest raspbian image apply the latest updates, then we can install a few extra packages and compile the software we need:

sudo apt-get install libusb-1.0.0-dev libmysqlclient-dev cmake

git clone git://git.osmocom.org/rtl-sdr.git

cd rtl-sdr

cmake .

make -j4 (because we have lots of cores to play with on a Pi2)

sudo make install

cd

wget http://lee.smallbone.com/blog/wp-content/uploads/2014/03/dump1090-1.08.1003.14-mysql.tar.gz

tar xvfz dump1090-1.08.1003.14-mysql.tar.gz

cd dump1090-mysql

PREFIX=/usr/local make -j4

cat <<EOF > /etc/modprobe.d/rtl-sdr-blacklist.conf

# This system has librtlsdr0 installed in order to

# use digital video broadcast receivers as generic

# software defined radios.

blacklist dvb_usb_rtl28xxu

blacklist e4000

blacklist rtl2832

EOF

cp dump1090 view1090 /usr/local/bin/

cp -av public_html /usr/local/share/dump1090

  

At this point you have the software built, but linux will have loaded the tv drivers not the sdr drivers. The simplest solution to this is a reboot.

 

Actually receiving data

 

Once things are up and running again you can fire up dump1090:

dump1090 --interactive --net --modeac --phase-enhance --aggressive --net-http-port 8080

You should see something like this in your terminal:

image

This shows you any aircraft being received. For a more interesting view point your browser to port 8080 on your Pi and you should see something like this:

image

So now you have a list of the local aircraft, and a map showing their position. Selecting an aircraft will cause its track to be recorded and displayed. The centre of the map and the range rings can be configured for your location - you need to edit the config.js file in /usr/local/share/dump1090

 

Pi or Pi 2?

I've been running this setup on an original Pi Model B for a number of months logging to a database and also supplying data to Flightradar24. The load average on an original Pi is around 1.05 and this causes it to slowly grind to a halt and eventually become completely unresponsive. A reboot solves this but is annoying if you're trying to collect long term data. Running the same software on a Pi 2 results in a loadaverage of 0.43 - so you could probably get away with running multiple receivers on a single system.

 

So is it worth an upgrade?

If you're just running dump1090 to see whats around you then an original Pi will just about cope. Once you want to actually do something with the data then a Pi 2 will really make a difference to the performance and stability of the system.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Very cool. I love rtl-sdr stuff. Another good platform is the odroid . Powerful enough to add a 2nd stick and maybe AIS or some voice.
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    Starting it with this commandline will remove networking: dump1090 --interactive --modeac --phase-enhance --aggressive If you're really worried about performance you can remove the phase-enhance and aggressive…
  • mcb1
    mcb1 over 7 years ago in reply to mcb1

    https://planefinder.net/

    https://www.flightradar24.com/60,15/6

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to Fred27

    There is aircraft data fed from some ATC's as well.

    Our data sent out from the system has a delay so that the information cannot be used for other purposes, but ADS-B broadcasts are in real time.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to Fred27

    "It's not quite radar though"

     

    I suspect it is referring to 'secondary surveillance radar' ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    Very interesting. I had no idea that there was so much aircraft info publicly exposed. It's not quite radar though. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 11 years ago in reply to e14 Contributor

    You'll find steps to fix this here: rtl-sdr – OsmoSDR

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>