Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog Raspberry Pi Lapdock HDMI cable work-around
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 27 Sep 2012 1:14 AM Date Created
  • Views 13714 views
  • Likes 5 likes
  • Comments 75 comments
Related
Recommended
  • rpiexpert
  • rpi

Raspberry Pi Lapdock HDMI cable work-around

johnbeetem
johnbeetem
27 Sep 2012
imageWant to build this project?
View Parts

 

Abstract:  I recently acquired a Motorola Atrix Lapdock and tried to get it working with my RasPi.  Unfortunately, something was wrong with the micro HDMI cable, specifically some cheap HDMI cables do not implement the individual ground lines.  I came up with a temporary work-around.  I thought people might be interested in the combination of detective work and exploration that got me to the solution.  Also, some of the Lapdock analysis I did may be useful to others.

 

 

I first read about the Motorola Atrix Lapdock quite a few months ago.  It's a really neat idea, to use a smart phone as a motherboard to make a laptop computer with "good enough" performance.  I suspect it failed to catch on for two reasons: (1) the list price of US$500 was way too much for the capabilities and (2) the smart phone software was unsuitable for a laptop.  I suspect it's primarily the software problem -- so many promising technologies have been sunk because the software isn't there in time.  So Motorola remaindered them, and grateful tinkerers have benefited from Motorola's optimism.

 

I had thought of using Lapdock for RasPi, but I couldn't find enough technical information to tell if it was possible and I wasn't willing to fork over US$100 for something that might have been impossible to interface.  So I was very glad to see Drew Fustini's element14 'blog Raspberry Pi laptop.  I was especially glad that he listed sources for the unusual Micro HDMI and USB adapters and cables.

 

So I ordered a Lapdock along with the cables and adapters that Drew recommended, including a short USB A male to A male adapter as in Update #2.  I ordered a Micro HDMI D male to HDMI A male cable that was different from Drew's.  They're all the same, right?

 

I was very impressed by Lapdock when it arrived.  It's a very beautiful piece of equipment.  Internally it's quite complex with lots of cable assemblies, tiny circuit boards, and specialized mechanical hardware.  I can see why Motorola orginally charged US$500 for it.

 

When the cables arrived from China, I eagerly charged up my Lapdock and attached the cables.  Well, it didn't work.  I didn't want to send the Lapdock back, since I didn't know if the problem was the Lapdock or one of the HDMI cables or adapters.  I was easily able to test the USB cables and adapters -- they were fine.

 

There's a lot of useful information about how Lapdock works in Drew's 'blog and its links.  There's also a long thread on the subject at raspberrypi.org called "I made a Raspberry PI Laptop".  From veryevil [5 June 2012] and Lob0425 [20 July 2012] I learned that you must connect an HDMI source to Lapdock for it to power on and provide +5V on the micro USB connector.  Nick S [30 June 2012] posted some very nice photos of Lapdock internals, including this one of the high-density 30-pin JHDMI receptacle that has the Micro HDMI and USB signals.  In that same photo you can see the 30-pin mating plug that's at the end of a small (and probably expensive) cable assembly.  Those are tiny connectors -- I think they're 1 mm pitch.  [Update: wrong by a factor of two: they're 0.5 mm image]

 

ARMed with this information, I took a look inside my Lapdock -- with power supply / battery charger disconnected, of course.  I figured I had already voided any warranty by hooking up non-Motorola cables, so what did I have to lose?  (Speaking of warranties, if you want to try this at home my comments here come with no warranty.  Proceed at your own risk!)  Lapdock is actually pretty easy to disassemble -- you only need to take off the small strip in the back of the Lapdock and it's held on by three small screws (two under pry-off rubber feet) and some plastic tabs that I managed to unhook without breaking anything off.  You get good quality for US$500.

 

There is a plastic shield over part of the circuit board.  It is there for a good reason.  Under it are direct connections to the 12V battery and it's really easy to short those points to ground "mit Spitzensparken".  So leave the shield in place.  Also, power is on unless you disconnect the cable that goes to the battery.  I was afraid to disconnect this cable, so I worked with 12V power on and stayed away from the shielded areas.

 

So where to begin?  Well, the 30-pin JHDMI receptacle is a good starting point since that's where the HDMI cable attaches.  The 30-pin plug comes off easily it you gently pry the edge with a small screwdriver.  Next it's time to start probing with a multimeter.  Always start with volts.  A voltmeter is high impendance so you're less likely to damage something than if you use an ohmmeter or ammeter setting.  The two USB A ports have nicely grounded shells, so that's a good place for the black lead on the voltmeter.

 

Here's a close-up of the first JHDMI pins.  The magnifier is trade show swag from Coilcraft.  Pin 1 is marked with a triangle and there are tick marks every 5 pins.  (Thank you very much, whoever did the excellent Lapdock PCB layout.)

image

As expected, most of the 30 pins were 0V.  After all, Lapdock is powered off.  But JHDMI pin 3 was around 10 volts!  WTF?  Who in their right mind would have 10V on a pin that connects to 5V or 3.3V equipment?  OK, must be a defective Lapdock.

 

At this point serendipity occurred.  I happened to have a USB tester dongle plugged into one of the Lapdock USB A ports.  This was so I could easily get at the USB Vbus and Gnd without shorting to the shell.  This USB dongle (shown below) was another bit of trade show swag, this time from Softeq Development.  When you plug it into a live USB port, the LEDs light up bright blue.  Really bright.

image

When I was testing JHDMI pin 3, at one point my probe accidentally touched JHDMI's shield and guess what?  The USB dongle LEDs flashed -- just for a moment.  I tried it again and they did the same thing -- just a momentary flash.  This was the first evidence that I was making real progress, because it meant that Lapdock was energizing 5V at least momentarily.  Using a sillyscope, I discovered that Lapdock was turning on sometimes for 18 msec, sometimes 47 msec.

 

If I'm going to have 10V running around, I sure hope it's current-limited.  I tried grounding pin 3 through an ammeter.  Sure enough, I got the same flashes and the current was around 64 uA.  This means that there's a 160K pull-up resistance to 10V.  I'm still leery about 10V running around, but at least it's such low current that as long as your HDMI device has proper diode clamps you won't damage it.

 

So where is JHDMI pin 3 connected to the Micro HDMI and USB connectors?  Well I decided to go through the long process of analyzing the cable assembly that connects JHDMI to the Micro HDMI and USB connectors.  In hindsight, this was not needed to solve my problem of getting Lapdock running, but I didn't know what the solution was going to be and I wanted to rule out other possibilities.  So using an ohmmeter setting and a safety pin so I could probe tiny micro HDMI contacts, here is what I came up with.  The first number on each line is the JHDMI pin.  HDMI pins are designated Ax for full-size type A and Dx for Micro type D.  Wikipedia lists the HDMI signals -- they're also in a white paper from HDMI Licensing.  The cable assembly shorts the HDMI connector shell to all the individual HDMI grounds pins except for DDC/CEC ground.

 

1  HDMI A19/D1 = hot plug

2  HDMI ground

3  HDMI A17/D16 = DDC/CEC ground

4  HDMI ground

5  HDMI A16/D18 = SDA

6  HDMI A15/D17 = SCL

7  HDMI ground

8  HDMI A12/D14 = Clock-

9  HDMI A10/D12 = Clock+

10 HDMI ground

11 HDMI A1/D3 = Data 2+

12 HDMI A3/D5 = Data 2-

13 HDMI ground

14 HDMI A4/D6 = Data 1+

15 HDMI A6/D8 = Data 1-

16 HDMI ground

17 HDMI A7/D9  = Data 0+

18 HDMI A9/D11 = Data 0-

19 unknown

20 HDMI A18/D19 = +5V

21 unknown

22 USB 2 = D-

23 USB 3 = D+

24 USB shield (shorted to HDMI ground)

25 USB 4 = ID

26 USB 5 = GND (not shorted to HDMI ground)

27 unknown

28 unknown

29 USB 1 = Vbus

30 USB 1 = Vbus

 

I hope this is right.  Please leave a comment if you find something different.

 

So here's the deal: all HDMI grounds are shorted to the HDMI shell except the DDC/CEC ground which is connected to JHDMI pin 3.  If nothing is plugged into the Lapdock Micro HDMI port, Lapdock pulls DDC/CEC ground to +10V.  Then when you plug an Atrix into Lapdock, Atrix shorts DDC/CEC ground to the other grounds, and Lapdock detects that Atrix is present and brings up the +5V charging voltage on the Micro USB connector.  If Lapdock is open, it also turns on the two USB A ports and turns on the display, keyboard, and trackpad.

 

The same things happen if you hook up a Raspberry Pi through HDMI and USB cables -- provided that the HDMI cable implements the DDC/CEC ground wire.  However, not all HDMI cables are the same.  A lot of cheap HDMI cables do not implement the individual ground signals.  Instead, they just have a common foil shield that's connected to the connector shells at both ends.  This works in most HDMI applications, but if your application requires individual ground lines -- like Lapdock -- it won't work.

 

(I found out about this early this year when I was trying to hook up my rev B4 BeagleBoard through a cheap HDMI cable.  After trying everything short of surgery, I finally opened up one of the cheap HDMI cables and verified that they hadn't bothered to include the individual grounds.  It turns out that rev B4 BeagleBoard did not ground the shell for reasons nobody remembers.  I attached a ground line to BeagleBoard's HDMI shell and it works fine with cheap cables.)

 

OK, so now I understand why my Lapdock didn't work with my RasPi.  The problem is that getting a replacement cable takes time and there's no guarantee that the next one won't have the same problem.  Since I wanted to bring my new Lapdock to RasPi's USA Hackspace Tour in San Francisco this coming Saturday, I decided to fix it the Hacker Way.  Since JHDMI pin 3 is right next to ground pin 4, I added a tiny solder bridge between the two pins.  So my Lapdock now thinks there's always an HDMI cable attached and works great with RasPi.  I added a switch to USB +5V to prevent power from getting to RasPi when Lapdock is closed.

 

Now, there's a little problem with doing it this way: battery discharge.  By grounding pin 3, I have a constant 64 uA draining from the battery.  It's not a lot, but it will discharge the battery faster than it would without it.  Also, Micro USB +5V is now constantly active.  With RasPi switched off, the +5V switcher isn't producing any output current, but the switcher's quiescent current is not zero and adds to the battery drain.

 

At some point, I want to install a tiny switch near Lapdock's Micro HDMI and USB connectors and use it to ground JHDMI pin 3.  When I do that, it will power off Lapdock completely and I won't need the +5V power switch on RasPi any more.  The problem is that I need to access a PCB trace that connects to JHDMI pin 3.  As far as I know, it's not accessible on the top surface but I bet I can find it on the bottom surface.  There has to be a 160K pull-up resistor there somewhere, and I should be able to attach to it.  But I'll watch the Engadget tear-down carefully first.

 

One thing I'm puzzled by is why the Lapdock USB A ports are energized when you connect HDMI with the lapdock closed.  Is Lapdock taking a long time to detect that it's closed and assumes it's open when first powered up?

 

Update 3 October 2012: I've installed a tiny toggle switch to ground JHDMI pin 3, so now when Lapdock is off it's no longer draining 64 uA from the battery along with whatever it uses to generate +5V for the Micro USB connector.  As a bonus, with the new switch in place, I no longer need a switch for RasPi USB +5V.

image

I had originally thought of attaching a wire to JHDMI pin 3 by finding a suitable spot on the bottom of the Lapdock PCB, but I soon realized that it would be better to attach to the Lapdock cable that goes between JHMDI and the Lapdock micro HDMI and micro USB connectors.  This way I avoid Lapdock PCB modifications.

 

It's fairly easy to peel back the shielding tape from the JHDMI end of the cable, exposing the wires that connect to the micro HDMI connector.  I only exposed wires at the pin 1 end.  Here's the best photo I could manage:

image

The wires are very thin, so be very careful not to break any.  I found some good photos of the other (Micro HDMI) end of the cable at "Raspberry Pi (modding Atrix Lapdock)", which helped confirm wire colors.  I believe these are the wires for JHDMI pins 1-7:

 

1  HDMI A19/D1 = hot plug (black)

2  HDMI ground (white)

3  HDMI A17/D16 = DDC/CEC ground (brown)

4  HDMI ground (white)

5  HDMI A16/D18 = SDA (red)

6  HDMI A15/D17 = SCL (green)

7  HDMI ground (white, IIRC)

 

I scraped insulation off the brown wire and verified that it did indeed connect to JHDMI pin 3.  Then I carefully cut it and soldered it to a longer (red) wire going to one side of the switch.  I connected a (black) ground wire from the other side of the switch to the micro HDMI shielding tape by inserting it under the plate that holds the micro HMDI and micro USB connectors in place.

image

I used a C&K GT02 sealed ultraminiature SPST toggle switch I had in my spare parts collection.  This is was designed for PCB mounting, but I was able to bend the mounting pins 90 degrees so I could hold the switch in place with #2-56 screws.  There's actually quite a bit of room in there, as you can see.

 

I didn't need to label the toggle switch.  It's left off when you're done using RasPi, and right on when it's time to create.

 

 

[This blog entry is copyright 2012 John F. Beetem and is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License (CC BY-SA 3.0). To view a copy of this license, visit http://creativecommons.org/licenses/by-sa/3.0/.  No warranty is expressed or implied.]

 

 

 

Product Name*DescriptionSupplier
Raspberry Pi Model BRaspberry Pi Model BRaspberry Pi model BRaspberry Pi
Buy NowBuy Now
Optical MouseOptical MouseBasic USB optical mouseIONE / Pro Signal
Buy NowBuy Now
Raspberry Pi Power SupplyRaspberry Pi Power Supply120-240v to 5V power supply with micro USB connectorRaspberry Pi
Buy NowBuy Now
KeyboardKeyboardBasic USB keyboardGear Head / A4 Tech
Buy NowBuy Now
Pre-Programmed 4GB SD CardPre-Programmed 4GB SD Card4GB Class 4 SD card preloaded with Debian 6 LinuxSamsung
Buy NowBuy Now
Adafruit Pi CobblerAdafruit Pi CobblerGPIO breakout kit for Raspberry PiAdafruit Industries
Buy NowBuy Now
BreadboardBreadboardBasic breadboard with 830 connection pointsTwin Industries
Buy NowBuy Now
Jumper wire bundleJumper wire bundleJumper wires for use on breadboardBud Industries
Buy NowBuy Now
FTDI USB-Serial CableFTDI USB-Serial Cable3.3v USB to serial interface cableFTDI
Buy NowBuy Now

 

*Products and resources listed are listed to help members build their own Pi Projects. They are suggestions and listed for educational purposes. For substitutions of any parts, please post a question asking the original author.

  • Sign in to reply

Top Comments

  • alexose
    alexose over 6 years ago +2
    If you don't want to tear open your Lapdock, I can personnaly vouch for the DIY HDMI cables from Adafruit. They actually include all 19 wires and work properly with the Pi. You'll need the following parts…
  • johnbeetem
    johnbeetem over 14 years ago in reply to mobilewill +1
    William Garrido wrote: I think I kinda of got it working, its more of a timing thing of when the lapdock detects the RPi. I have the Rpi to force HDMI on. If the Lapdock is on battery and not supplying…
  • mobilewill
    mobilewill over 14 years ago in reply to johnbeetem +1
    Thanks for the info. It seems like the lapdock 100 is the same behavior. I like the capacitor idea since if I can get another RPi I want to make it semi attached to the lapdock. This one has a rubber slot…
  • alexose
    alexose over 6 years ago

    If you don't want to tear open your Lapdock, I can personnaly vouch for the DIY HDMI cables from Adafruit.  They actually include all 19 wires and work properly with the Pi. You'll need the following parts:

     

    https://www.adafruit.com/product/3561

    https://www.adafruit.com/product/3559

    https://www.adafruit.com/product/3556 (or Mini or Standard depending on your Raspberry Pi model).

     

    These parts are also available via eBay for cheaper, but they ship from China.

     

    Unfortunately the PCB is somewhat wide, so you'll need a very slim micro USB cable to go with it.  I used a dremel to shave down my cable so it would fit.  You could also probably make your own cable from one of these connectors: https://www.adafruit.com/product/4023 .

     

    (I'm cross-posting this response several places because getting to the bottom of this issue took me several days and at least $60 worth of cables and converters. Hoping that I save someone else the headache!)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to jemenake

    Joseph Emenaker wrote:

     

    Does anybody know if the LapDock behaves this way? Is the data from the USB port deactivated if there is no load on the power wires?

    You didn't say which Lapdock you have.  My experience is with the Atrix Lapdock, and I've read that the Droid Bionic Lapdock works the same though the connectors are rotated.  I've also read that it's hard to get a Lapdock 100 or 500 to work.

     

    I don't think the Atrix Lapdock cares if you're drawing power on the 5V line.  A lot of early Atrix Lapdock users clipped the 5V line to prevent problems back-powering RasPi Model B 1.0 PCBs which had 140 mA fuses on the USB lines.  I've also read of them being used successfully with ordinary PCs: http://weblog.mrbill.net/archives/2012/05/11/using-a-motorola-atrix-lapdock-as-a-hdmi-monitor-and-usb-keyboard-mouse/  This hacker cut the 5V USB line.

     

    I think the most likely culprit is that the Micro USB connector isn't connecting reliably to the Lapdock.  I've been using an Atrix Lapdock with my RasPi for a couple years now, and lately I've been losing the keyboard and mouse.  When I wiggle the Micro USB connector a bit they come back.  I expect complete failure at some point, which will require either a new Micro USB female to USB A cable or if the Lapdock's Micro USB plug fails I'll have to go in and do surgery, connecting a USB A cable directly to the internal wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jemenake
    jemenake over 11 years ago

    So, I'm having a confusing problem with trying to using a LapDock with a RasPi: the keyboard and trackpad don't work. But I don't think it's an issue with the data wires, I think it might be something odd happening in the LapDock, itself.

     

    Almost all of the HOWTO's for LapDock/RasPi interconnect I've seen use the LapDock to power the RasPi, making a Frankenstein laptop, in a way. That is not my application. I've got some RasPi's embedded in the field. What I'm trying to make is a portable KVM where I can go out to a location, plug in my LapDock and have a console whereby I can work on the RasPi. In other words, it is to save me from having to lug an LCD monitor and USB keyboard out to the location and then find a place to plug in the monitor.

     

    The crucial bit to understand is that the RasPi is already powered via its micro-USB port before I come along with the LapDock. When I connect things up, the HDMI connection works fine, the RasPi just never sees the LapDock's keyboard or trackpad. I know the USB ports on the RasPi work because I can plug any other USB keyboard into it. I also have tried plugging the USB line from the LapDock into a regular PC, and that does not work. So, something about the LapDock's USB data is failing to get to the RasPi. My suspicion, thus far, is that the LapDock doesn't activate it's keyboard/trackpad unless it sees something draining power from the USB port (as this is how it would sense that you've got your phone docked in it). For people powering their RasPi from the LapDock, there is power being taken from the USB port, so this could explain why nobody else is having the issue.

     

    Does anybody know if the LapDock behaves this way? Is the data from the USB port deactivated if there is no load on the power wires?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baskybas
    baskybas over 12 years ago in reply to e14 Contributor

    Hi,

    Any idea what is the approx cost for your direct cable with No adaptors. Please explain what do you mean by No adaptors. I am frusturated trying my raspberry pi with Lapdock100. I could not make it up by hacking the adapters and wasted around $20 for cables and adapters. I am interseted and very curious to get the cable you dessigned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi.  How is the direct connection cable coming along?  Any idea what the approx. cost might be for one of these?  I am so frustrated trying to get my RPi-dock to start reliably.  Currently I have to cable it in just the right order whilst patting my head and rubbing my tummy and even them sometimes I am disappointed!

    Barry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>