• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Raspberry Pi OS on old PCs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 4 Jan 2017 11:04 PM Date Created
  • Views 6091 views
  • Likes 3 likes
  • Comments 2 comments
Related
Recommended
  • operating system
  • raspberry pi
  • cabeatwell
  • neat
  • os
  • x86
  • raspbian
  • innovation

Raspberry Pi OS on old PCs

Catwell
Catwell
4 Jan 2017

imageimage

(LEFT) Boot Screen of Rasbian for PC operating sytems. (RIGHT) This is Raspbian running on a PC. (via Raspberrypi.org)

 

The Raspberry Pi Foundation has created a version of the Raspbian OS for MAC and x86(Windows) personal computers. Raspbian is the Debian based Linux distro that until now, was intended specifically for the Raspberry Pi series of SBCs. This OS is purported to need a minimum of 512MB of RAM but you can see in the comments that at least one user got it running on a machine with just 256MB of RAM. The OS is meant to be run from a DVD or a USB drive. Just boot from the medium of your choice and then you will be taken right to the new PIXEL desktop.

 

I am sure that most maker/engineer types out there (like myself) have an alarmingly large pile of ancient computer equipment. I know that, at any time, I could have downloaded Knoppix or Ubuntu or really any other Linux distro and revived my sad and smudgy collection of laptops and desktops but I don’t need just another computer. However, a pi-top made from an actual old laptop would be awesome. I use Raspbian and Raspberry Pi’s extensively and it is really cool to be able to reuse that old hardware for RasPi development. Maybe you could set up a dual boot so that you can run the OS on your desktop for those days when you need to do some RasPi work but you don’t want to actually hook up a Raspberry Pi. But really, seamlessly (hypothetically) moving work across platforms but not operating systems is really conducive to familiarly with the OS.

 

That is one of the reason given by raspberrypi.org for why this whole endeavor is worth doing. Being able to work in the same environment regardless of platform reduces the learning curve and removes the need to adjust for different operating systems. Now their example refers to student users but it applies to users of all types.

 

Also, I am willing to bet that for a lot of people the only version of Linux that they have ever experienced is Raspbian. The release of the Raspberry Pi has almost certainly exposed a legion of people to Linux who otherwise might never have had need to use it.

 

Users of the new distro may notice the absence of Wolfram Mathematica and Minecraft. The RasPi foundation reports that they are only licensed to include that software on versions of the OS meant to run on an actual Raspberry Pi computer. Also, the RasPi foundation does caution that this release is a prototype, and while updates will be forthcoming, users can expect to see some issues with the OS recognizing some hardware configurations.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 9 years ago +2
    Too many other Linux distros for PC's especially DSL etc. Check out DistroWatch.com: Put the fun back into computing. Use Linux, BSD. for others that are small footprints. People who have run Raspbian…
  • clem57
    clem57 over 9 years ago

    Too many other Linux distros for PC's especially DSL etc. Check out DistroWatch.com: Put the fun back into computing. Use Linux, BSD.  for others that are small footprints.

     

    People who have run Raspbian, a build of Debian for Raspberry Pi computers, are probably familiar with the distribution's PIXEL desktop environment. PIXEL grew out of a customization of the LXDE desktop and provides Raspbian users with a snappy desktop environment that can run on the Pi's minimal ARM-based hardware. Fans of the PIXEL desktop will be happy to know the environment is now available to people running desktop and laptop computers with x86 processors. "Back in the summer, we asked ourselves one simple question: if we like PIXEL so much, why ask people to buy Raspberry Pi hardware in order to run it? There is a massive installed base of PC and Mac hardware out there, which can run x86 Debian just fine. Could we do something for the owners of those machines? So, after three months of hard work from Simon and Serge, we have a Christmas treat for you: an experimental version of Debian+PIXEL for x86 platforms. Simply download the image, burn it onto a DVD or flash it onto a USB stick, and boot straight into the familiar PIXEL desktop environment on your PC or Mac." The Debian+PIXEL image runs on 32-bit x86 machines and gives Pi users the option of having a consistent desktop experience across multiple devices. Additional information and screen shots can be found in the announcement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago

    The very interesting option is try to rung this version of the OS on different SBC, maybe more or differently performing than the PI. I will try as I have time on the Gizmo Intel based SBC where I have already run Windows 8 industrial and the standard Debian distro