Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog System on a Chip for the Raspberry Pi (RPPSOC)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: land-boards
  • Date Created: 28 May 2016 10:22 PM Date Created
  • Views 1112 views
  • Likes 0 likes
  • Comments 3 comments
Related
Recommended
  • system on chip
  • diy
  • raspberry pi

System on a Chip for the Raspberry Pi (RPPSOC)

land-boards
land-boards
28 May 2016

We've got a new project up on Kickstarter. It's a Programmable System on a Chip (PSOC) hat for the Raspberry Pi.

 

image

Features

  • Cypress Semiconductor PSOC 5LP part  CY8C5267AXI-LP051
  • Core: ARM Cortex M3
  • Data Bus Width: 32 bit
  • Maximum Clock Frequency: 67 MHz
  • Program Memory Size: 128 kB
  • Data RAM Size: 32 kB
  • ADC Resolution: 12 bit
  • Data RAM Type: SRAM
  • Interface Type: I2C
  • Number of ADC Channels: 1
  • Number of I/Os: 72
  • I/O Number of Timers/Counters: 4
  • Timer Program Memory Type: Flash
  • Works on all Raspberry Pi cards with 40 pin GPIO (A+/B+/Pi2/Pi3/Zero)
  • All 29 Raspberry Pi I/O lines are connected to the PSOC
  • Configuration EEPROM
  • LED (see below for details)
  • Fuses on 3.3V and 5V power
  • Two I/O connectors 14 + 16 = 30 I/O pins
  • Each of the two I/O connectors can be 3.3V or 5V
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 10 years ago +1
    There is a thread about the kickstarter here at e14: https://www.element14.com/community/message/198148/l/psoc-5lp-hat-for-a-raspberry-pi#198148
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Afsha Shaikh,

         This has nothing to do with the topic at hand. Furthermore, this is a product blog with no important information unless you are locking for a problem to solve.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Great blog on SoC. It was very informative and thanks for sharing this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago

    There is a thread about the kickstarter here at e14:

    https://www.element14.com/community/message/198148/l/psoc-5lp-hat-for-a-raspberry-pi#198148