• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Watchdog Timer for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mistertee
  • Date Created: 19 Jul 2016 10:15 AM Date Created
  • Views 7987 views
  • Likes 1 like
  • Comments 19 comments
Related
Recommended
  • autostart
  • watchdog timer

Watchdog Timer for the Raspberry Pi

mistertee
mistertee
19 Jul 2016

Like all PCs the Raspberry Pi is likley to hang up during operation due to unexpected events not being catered for in the code. In an unattended application where the program automatically starts this can be a problem as there is no one around to restart the RPi. If there is no keyboard or HDMI monitor this is by power cycling. The Raspberry Pis internal watchdog timer has a poor reputaion - there are many comments about it being unreliable. This post presents a simple external watchdog timer.

 

Although there are dedicated power supply monitoring chips this solution uses components that are likley to be in most electronic hobbyists kit - based around the popular 555 timer.

 

image

 

The programme has to supply a Hi going pulse every few seconds. If there is no pulse for more than about 60 seconds the 555 output on Pin 3 will go low. This is coupled through to the on-board reset pin of the Raspberry Pi through a capacitor to issue a low going pulse which resets the Pi.

 

A capcitor is used here so that only a pulse going from Hi to Low will reset the raspberry Pi. A constant Lo voltage which is present while the raspberry Pi is starting up will have no effect.

 

If a shorter time is required then either reduce the value of R1 (1Mohm) or reduce the value of C1 (100 uF).

 

The LED pulses every time a Hi Pulse is issued to provide a visual indication to the user that everything is fine. The 555 timer does not easily provide a retriggerable monostable function that is required for a watchdog timer. Diode D1 is used to discharge the capacitor every time a pulse is received.

 

The reason the delay before a reset is set at more than 60 seconds is that the Raspberry Pi takes more than 30 seconds to start up.

 

Click here for a guide to setting the Raspberry Pi to autostart.

 

image

 

The image above shows the connection to the Reset pin of the Raspberry Pi.

 

Summary

 

Althogh the Raspberry Pi has an in-built watchdog timer, this has a poor reputaion. This watchdog timer is a reliable way of resetting the Raspberry Pi in remote applications where there is a risk of it hanging up due to the code not handling unexpected events correctly.

  • Sign in to reply

Top Comments

  • mistertee
    mistertee over 10 years ago in reply to mcb1 +1
    True - I am sure there is a much better chip out there. 555 timers are like Marmite - you either love it or hate it. I had some in stock (doesn't one always) and couldnt be bothered to order a new IC and…
  • mistertee
    mistertee over 10 years ago in reply to shabaz

    Sounds good. Any guidance on how to do this? All my experience is with hardware - hence the use of Python and gut instincts leading me to a watchdog.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mistertee

    I've not used one for the Pi, so this will only be a general comment - manufacturers like On Semi have these devices, programmed to different threshold voltages.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mistertee

    Hi Seggy,

     

    The possibility of Python code crashing is a good example of a situation that does not require a hardware watchdog. You can have the application be killed and restarted. In other words, a process monitor i.e. a software watchdog.

    A hardware restart due to a hardware watchdog kicking off because of a Python app not responding could make the situation worse (for example file system corruption).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mistertee
    mistertee over 10 years ago in reply to shabaz

    Would you guys be able to recommend one that you've used before?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mcb1

    Hi Mark,

     

    That's a good point, power-related issues that require a reset could be handled with brown-out detection driving the reset.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>