• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Blog Watchdog Timer for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mistertee
  • Date Created: 19 Jul 2016 10:15 AM Date Created
  • Views 7988 views
  • Likes 1 like
  • Comments 19 comments
Related
Recommended
  • autostart
  • watchdog timer

Watchdog Timer for the Raspberry Pi

mistertee
mistertee
19 Jul 2016

Like all PCs the Raspberry Pi is likley to hang up during operation due to unexpected events not being catered for in the code. In an unattended application where the program automatically starts this can be a problem as there is no one around to restart the RPi. If there is no keyboard or HDMI monitor this is by power cycling. The Raspberry Pis internal watchdog timer has a poor reputaion - there are many comments about it being unreliable. This post presents a simple external watchdog timer.

 

Although there are dedicated power supply monitoring chips this solution uses components that are likley to be in most electronic hobbyists kit - based around the popular 555 timer.

 

image

 

The programme has to supply a Hi going pulse every few seconds. If there is no pulse for more than about 60 seconds the 555 output on Pin 3 will go low. This is coupled through to the on-board reset pin of the Raspberry Pi through a capacitor to issue a low going pulse which resets the Pi.

 

A capcitor is used here so that only a pulse going from Hi to Low will reset the raspberry Pi. A constant Lo voltage which is present while the raspberry Pi is starting up will have no effect.

 

If a shorter time is required then either reduce the value of R1 (1Mohm) or reduce the value of C1 (100 uF).

 

The LED pulses every time a Hi Pulse is issued to provide a visual indication to the user that everything is fine. The 555 timer does not easily provide a retriggerable monostable function that is required for a watchdog timer. Diode D1 is used to discharge the capacitor every time a pulse is received.

 

The reason the delay before a reset is set at more than 60 seconds is that the Raspberry Pi takes more than 30 seconds to start up.

 

Click here for a guide to setting the Raspberry Pi to autostart.

 

image

 

The image above shows the connection to the Reset pin of the Raspberry Pi.

 

Summary

 

Althogh the Raspberry Pi has an in-built watchdog timer, this has a poor reputaion. This watchdog timer is a reliable way of resetting the Raspberry Pi in remote applications where there is a risk of it hanging up due to the code not handling unexpected events correctly.

  • Sign in to reply

Top Comments

  • mistertee
    mistertee over 10 years ago in reply to mcb1 +1
    True - I am sure there is a much better chip out there. 555 timers are like Marmite - you either love it or hate it. I had some in stock (doesn't one always) and couldnt be bothered to order a new IC and…
  • mistertee
    mistertee over 10 years ago in reply to mcb1

    True - I am sure there is a much better chip out there. 555 timers are like Marmite - you either love it or hate it. I had some in stock (doesn't one always) and couldnt be bothered to order a new IC and pay postage and wait 2 days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mistertee
    mistertee over 10 years ago in reply to shabaz

    The need for this watchdog circuit came out of a recent application the bare bones of which are rpesented below.

    Remote RF linked temperature monitors (upto 8 possible)

    RF receiver with serial link to RPi

    Ethernet connection to upload data to cloud and e-mail alerts

    Remote set-up with autostart (no keypad or monitor)

     

    Even after plenty of testing the possibility of software (written in Python) crash is there. eg data collision resulting in corrupted data, e-mail failure due to server issues ........

     

    I know the theoretical response is going to be "Test the system and iron out all bugs". However in practice this is a "safety net" while we do this and allows us to trial the system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to shabaz

    Would using a proper brown-out IC (with the similar pulse before time-out) be preferable than this approach.

     

    I do agree that simply resetting it could mask another issue that requires resolving.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago
    Like all PCs the Raspberry Pi is likley to hang up during operation.

    Hi Seggy,

     

    Just to flesh out things a bit, perhaps an application could be likely to hang, generally the Linux kernel is not likely to hang unless there is a very severe issue like a build issue, hardware fault or power related issue.

    It is worth mentioning that if the board ever does lock up, this should be investigated; because for the hardware watchdog to have to ever take action on a Linux platform is "severe".

    Possible reasons could be a poor power supply perhaps, or bad cooling strategy, and for these the hardware watchdog action is like a sticking plaster and does not fix the underlying issue(s).

    The underlying issues should therefore be resolved if the watchdog timer actually has to ever take action.

    Finally, if users are experiencing application hangs then these do not require a hardware watchdog timer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<