Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum So I ordered this camera with the hopes of using it on the pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 704 subscribers
  • Views 1852 views
  • Users 0 members are here
  • pi
  • BeagleBone
  • camera
Related

So I ordered this camera with the hopes of using it on the pi

easyejl
easyejl over 6 years ago

And I'm stumped. I haven't tried connecting it to a pi yet, just a windows pc. It shows up via USB as an audio device, and also as a USB drive. On the drive is an .apk file for android, to install their in car DVR software (and driver I guess?) to allow the android device to access it as a camera.

 

https://smile.amazon.com/gp/product/B07VM85H2P/ref=ppx_yo_dt_b_asin_title_o05_s00?ie=UTF8&psc=1

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 6 years ago

    I think what Clem says is right, it could just be a USB cable to pull off files.

    To do live video capture may need a different camera, there's some info on webcams here:

    https://www.raspberrypi.org/documentation/usage/webcams/

    However it used to be that very few webcams worked with Linux, so I don't know if that has changed.

    The Pi camera module in Sean's link (that plugs into the flat-flex slot) could be easier to use, since the Raspbian image supports it by default.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to shabaz

    "However it used to be that very few webcams worked with Linux, so I don't know if that has changed."

    There used to be a list of supported USB webcams which worked with the USB Video Class Linux driver listed here:

    Linux UVC driver & tools

    I stumbled across it when using webcams with the Intel Galileo SBC.

     

    Another approach is to use USB audio/video class compliant devices like the AJA U-TAP

    https://www.aja.com/products/u-tap-hdmi

    https://www.aja.com/products/u-tap-sdi

    or Epiphan AVIO and bring your video in that way without the need for yet another driver. I use them for getting broadcast video into devices that expect to use USB webcams. Not a cheap option unfortunately, but allows you to use whatever HDMI/HD-SDI device you want to.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • easyejl
    easyejl over 6 years ago in reply to beacon_dave

    that is a cool device (the U-Tap) but dang that price. I'll have to remember that it exists if I ever find a deep need for it

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to easyejl

    Epiphan do a similar one.

    https://www.epiphan.com/products/avio-hd/

    If I recall correctly you need to install a driver if you want to configure it, but once configured it is USB AV class compliant.

     

    May be possible to do something on a budget with a FPGA dev board, as a number of them have HDMI capture and USB connectivity.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to beacon_dave

    Interesting product!

    It looks great for microscopes - noticed it mentions latency is extremely low.

    I have a similar type thing for analog uncompressed video from The Imaging Source, but it is not HD : (

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to beacon_dave

    Interesting product!

    It looks great for microscopes - noticed it mentions latency is extremely low.

    I have a similar type thing for analog uncompressed video from The Imaging Source, but it is not HD : (