Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My success with the Cirrus Logic Audio Card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 706 subscribers
  • Views 3353 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

My success with the Cirrus Logic Audio Card

jcjc
jcjc over 10 years ago

Hello,

 

I've had a successful year building and using devices using the CLAC (cirrus logic audio card) since my last visit (http://www.element14.com/community/message/151149/l/re-cirrus-logic-audio-card-working-on-the-raspberry-pi-2#151149).  Returning to this discussion area a year later, I still see lots of good work by individuals, and still some frustration.  I thought I'd quickly recount my experience to those who helped me - I used Ragnar Jensen's .deb's and got help from him that was invaluable.  It is remarkable what is achieved here - on the back of volunteer help - despite people's frustrations and little (no?) input from the manufacturer. 


The device I build is an outdoor audio recorder in a waterproof box with a battery.  In 2014 it was used with a USB microphone, until I found the Cirrus Logic card.  It's been used in 2015 to monitor bird populations by ornithologists.  They have collected several terabytes of audio data used for research.  The performance has been good - the only device that had to be replaced was literally lost-in-the-forest (the deployer forgot where it was located - so it is surrendered to future archaeology).  There have been no hardware failures (20 devices deployed over about 6 months, each recording permanently for as long as the USB battery pack allowed - about 5 days then cycled every week).


The device stores audio in 10-minute long audio files on the SD card, timestamped, and divided into folders one-per-day.  I use the really basic "arecord" to do the recording, sending a signal (USR1 via a cronjob) to it every 10 minutes to split the audio file.  There is no break in the recording at file-boundaries so you can subsequently concatenate the wav files seamlessly (no clicks, no gaps, no overlaps) - this is necessary for the stats which the ornithologists want.  The time-of-day is read at boot-time from the "piface shim" RTC, which works in conjunction with the CLAC without doing anything clever.  I found a good source of microphones for outdoor use recently (micbooster.com in the UK) which use the Primo EM172.Z1 capsule, which I hope to use widely in the coming season (2016).


The "user experience" is to flash a SD card with my customised ".img", plug it into the unit, turn on the power bank, close the waterproof lid and walk away.  Data recovery involves visiting the recorder, collecting (or swapping) the SD card (and battery), and then copying to your PC back in the lab.  This is easy on Mac and Linux, but windows is a nuisance as it won't read my bespoke third FAT partition containing the audio.  (This partition is created and formatted at first-boot and uses up all the remainder of the SD card space thereby fully utilising any size of SD card - I recommend 32 or 64Gb cards).  Users can pre-customize their images by replacing a special /boot/recorder.conf file (which is read/write-able from Windows - nice). Config options include mic-gain, sample-rate (16/32/44.1KHz).  It will have to support stereo/mono for this year (see below).


Plans for the coming year:


(*top priority*) leaarn how to emulate!!!. Developing by ferrying SD cards between my PC and the Raspberry Pi hardware is unmanageably tedious. (looking at pilfs.  XEC design has vanished, I find this whole topic hard to get into). I just want to run a few commands on a stock raspbian to install my code, and upgrade to the CLAC-enabled kernel - to produce a ship-able "img" to users, but I currently boot a bare metal Raspberry pi to do this).

1) try the WittyPi (from UUgear)  power manager so we can have a calendar of when to record.  Hopefully shut down the pi when not in use, and reboot when recording should re-start.

2) move to stereo recording with microphones separated by a meter or so - this will allow direction-of-source analysis to be done back in the lab (x-correlation between L+R).  With a pair of such devices pointing at the same outdoor scene, we can triangulate to find the location of the source of the sound (bird, or whatever).  (Ironically I spent a lot of time fussing with .asoundrc files to get mono working last year)

3) Integrate using larger 12v batteries (SLA or vehicle batteries) to get deployments of a month or more.  This needs a low-loss 12v to 5V (or 3.3v?) regulator.

4) losslessly compress (flac) audio files to increase storage capacity on SD card. (tricky with arecord + kill -USR1) - consider move to gstreamer.

5) move to latest raspbian - integrating 4.? kernel, systemd (does rc.local still work?).

6) Power : does the raspberry pi zero give any saving on power usage (crikey! - no header pins, what a hassle).

7) ultrasound for bats.

 

I'm sticking with the arm-V6 raspberry pi's (version A+) as the pi-2 (V7) is too power hungry.  I'll shortly have to catch up with all the posts on this site regarding what has changed since a year ago.  HiassofT's stuff looks interesting and good old Ragnar is hopefully still around.  Systemd, jessie, kernel-4.1, device-tree are on my mind.

 

Note that I don't sell these.  I've built a few for friends, but most are assembled by users (they are pretty easy to assemble with my guidance on the phone and email). I'll upload a public copy of the .img if there is any interest - but it is a year old (based on raspbian from February 2015, I think...)

 

So life is good, and these devices work well.  A huge thanks to those who have made this happen.  There are real consequences of this work (for a few PhD students, and some British birds at least).

 

Happy new year to you all.

 

James.

 

Images for fun: 

First is the bare recorder.

Second is the B+ with piface shim RTC ready for CLAC installation.

Third is the unit in waterproof box, ready to deploy (this is an older version using USB microphone - so no cirrus card on this one).

Fourth is another of the old-fashioned USB mics  - this time the anatomy.  Note: I've given up on the power-off switch - nobody used it.


 

imageimage

imageimage

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    J C,

     

    In your first photo you show the Primo EM172.Z1 connected directly to the Cirrus line in port. Are you running ./Record_from_lineIn_Micbias.sh to power the mic? I took over a research project that uses an RPi with the CLAC and an electret microphone wired to a DAQ (powered by 2xAA batteries) that is in turn plugged into the CLAC's line in. I assume the student who designed this must have wired the microphone to the DAQ at least for the power option, and possibly for the preamp on the DAQ, but it seems like it should be possible to use the bias through the line in port to eliminate the need for batteries. My knowledge of circuits is virtually zero, so my questions may be stupid, but your setup looks promising. Does the EM172.Z1 get enough power through the CLAC's line in to record at a decent volume? I attempted to use my iPhone earbud/mic through the line in, but those recordings are so quiet they are useless. I hope that microphone is simply not compatible. The former student may have opted for his external DAQ with batteries configuration to minimize noise. Is there more noise in recordings when a mic is powered via line in bias vs. an external power source? Maybe I'm going in the wrong direction and should stick with his designs. Unfortunately I'm having to learn a lot of this stuff on my own.

     

    Ultimately, if quality recordings are possible, I'd like to set up something as simple as this electret capsule microphone (or maybe the EM172.Z1) soldered to the wiring of a 3.5 mm plug (this one could be cut in half for a 2-for-1 deal!). The microphone will be fixed to my custom RPi case only a few inches from the line in port, so as nice as this ready-made mic is, it's way too much wire for the small footprint I'm trying to maintain. Plus, eventually I'll set up 20-30 of these RPi recorders, so cost is a factor. I think I can handle a little soldering.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jcjc
    jcjc over 10 years ago in reply to e14 Contributor

    Dear Matt Nalley,

    The Primo EM172 microphone capsule works very well connected directly to the line in of the Cirrus Logic Audio Card, with micbias turned ON, so that the mic is provided with a few volts of power (I measured it once... I think it's 2.75 volts, and it's applied to both left and right channels).  The proper name for this is Plug-in Power (PiP) and is covered halfway down this wikipedia article.  PiP is not to be confused with the commonplace "phantom power" used by studio musicians which is 48 volts. 

     

    So I don't use a pre-amp, or a battery in my microphones.  I just bought 35 Primo EM-172's for deployment this year, and am impressed so far.  I bought them from micbooster in the UK.  The microphone capsules you link to also look plausible.

     

    If you are having volume problems, there are 2 volume controls on the line input:  one appears to be a "preamp" and the other is a digital volume (I'm guessing a bit here, but this is my best educated guess).  Look in the script Record_from_lineIn_Micbias.sh for these volumes.  Or see the last 10 lines of https://github.com/solosystem/amon/blob/master/amon.conf#L53 for my comments about these, their ranges and meanings.  In short: increase the "Volume" first, then the "Digital Volume" until you reach your desired input levels.  (On the solo you can do this by editing amon.conf in /boot.) If you want are changing it on a live system (which sounds probable if you are in a lab, not in a forest) then restart the recorder with "amon stop; amon start".

     

    I'm happy to discuss more - in particular, are you aware that there are _on board_ stereo microphones already on the CLAC selected using the other startup script (the one with DMIC in the name) - they might be better quality and less hassle to use than your capsule idea - your chamber might fit straight over the board?  Also - have you also considered ultrasound?  The CLAC will record up to 96kHz. Fruit flies are small, and possibly emit frequencies higher than 20kHz (which is your capsule's stated cut-off)  - particularly if they really are "singing" and it's not just the noise of their wings flapping.  But I am way out of my league here, and perhaps you were being euphemistic.

     

    Good luck and keep in touch.

    James.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jcjc
    jcjc over 10 years ago in reply to e14 Contributor

    Dear Matt Nalley,

    The Primo EM172 microphone capsule works very well connected directly to the line in of the Cirrus Logic Audio Card, with micbias turned ON, so that the mic is provided with a few volts of power (I measured it once... I think it's 2.75 volts, and it's applied to both left and right channels).  The proper name for this is Plug-in Power (PiP) and is covered halfway down this wikipedia article.  PiP is not to be confused with the commonplace "phantom power" used by studio musicians which is 48 volts. 

     

    So I don't use a pre-amp, or a battery in my microphones.  I just bought 35 Primo EM-172's for deployment this year, and am impressed so far.  I bought them from micbooster in the UK.  The microphone capsules you link to also look plausible.

     

    If you are having volume problems, there are 2 volume controls on the line input:  one appears to be a "preamp" and the other is a digital volume (I'm guessing a bit here, but this is my best educated guess).  Look in the script Record_from_lineIn_Micbias.sh for these volumes.  Or see the last 10 lines of https://github.com/solosystem/amon/blob/master/amon.conf#L53 for my comments about these, their ranges and meanings.  In short: increase the "Volume" first, then the "Digital Volume" until you reach your desired input levels.  (On the solo you can do this by editing amon.conf in /boot.) If you want are changing it on a live system (which sounds probable if you are in a lab, not in a forest) then restart the recorder with "amon stop; amon start".

     

    I'm happy to discuss more - in particular, are you aware that there are _on board_ stereo microphones already on the CLAC selected using the other startup script (the one with DMIC in the name) - they might be better quality and less hassle to use than your capsule idea - your chamber might fit straight over the board?  Also - have you also considered ultrasound?  The CLAC will record up to 96kHz. Fruit flies are small, and possibly emit frequencies higher than 20kHz (which is your capsule's stated cut-off)  - particularly if they really are "singing" and it's not just the noise of their wings flapping.  But I am way out of my league here, and perhaps you were being euphemistic.

     

    Good luck and keep in touch.

    James.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jcjc

    Thanks for the swift reply, James!

     

    I think I'll test one of those ready-made EM172 mics to see if it can capture fly "song" with appropriate sensitivity after adjusting the volume settings.

     

    Yes, fly people use the term singing to refer to wing buzzing. We also call ourselves fly people haha. I do like the ultrasound idea. I'll see if anyone has attempted to record fruit flies at those frequencies. I have no idea if they have other modes of making sound. Our current setup is actually only recording at 6 kHz because that is plenty to capture the "songs" they make with their wings.

     

    I played with DMIC a few times by accident. I mistook that usecase script for the mic-in script before I noticed those MEMS mics on the CLAC. I'm not sure if I could design a case for the RPi to hold our fly courtship chambers close to those mics (right now the whole RPi/CLAC is encased in acrylic so I can't easily test it), but if that is possible and they are sensitive enough, then it could be a viable alternative.

     

    I'm not sure if you do any work in the realm of building electrical circuits, but I never went beyond a couple college physics labs so a lot of this is new to me. If it turns out that the signals from a the micbooster EM172 mic are too weak, I'm wondering if a mic with a preamp like this MX4466 could be wired in essentially the same way, with the line in port supplying 2.7-2.8 V. According to the specs it needs 2.4-5.5 V, and "somewhere in the middle" like 3 V is considered ideal, so maybe that would be a relatively simple alternative if I need to boost gain?

     

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jcjc
    jcjc over 10 years ago in reply to e14 Contributor

    Matt,

     

    I'm not the person to help with pre-amps, I'm afraid, so can't make any recommendations.  Good luck with the EM172, though.

     

    James.