Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it safe to power a raspberry pi from battery's?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 715 subscribers
  • Views 5413 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
Related

Is it safe to power a raspberry pi from battery's?

e14 Contributor
e14 Contributor over 10 years ago

I want to make my raspberry pi portable, is  it safe to run it from battery's?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, I'm currently working on an Instructable and element14 article about making a Raspberry Pi PowerHAT. It will let you power your Raspberry Pi with batteries, safely. I'll share the links here, once I complete them.

     

    First of all, by using the 5V GPIO pin you are bypassing the input fuse that is on the RPi. This means you have no protection in case of a short circuit, or reverse voltage. If you do make an error, a lot of current (depending on how much you power supply can provide) can flow through your Pi and can damage it. You are also bypassing a high-efficiency diode circuit, so you are basically without any protection. I've included a schematic of the power management circuit for a Raspberry Pi Model B+, below.

     

    image

    Despite all these cons, it's still possible to power the Pi through the pins, with a simple circuit. First off, a regulated 5V power source has to be inputted to the 5V and ground GPIO pins. Most power adapters won't output a regulated voltage (unless stated otherwise on them) so you would also need to use some voltage regulator circuit. Lastly, there are a few capacitors used to smooth the voltage, which makes power more stable.

    To power the Pi, you will need to have a regulation circuit, or use a regulated power supply. Then, just add a schottky diode on the input, and maybe a resettable fuse. I hope this helps, and I'll try to provide a schematic of said described circuit.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, I'm currently working on an Instructable and element14 article about making a Raspberry Pi PowerHAT. It will let you power your Raspberry Pi with batteries, safely. I'll share the links here, once I complete them.

     

    First of all, by using the 5V GPIO pin you are bypassing the input fuse that is on the RPi. This means you have no protection in case of a short circuit, or reverse voltage. If you do make an error, a lot of current (depending on how much you power supply can provide) can flow through your Pi and can damage it. You are also bypassing a high-efficiency diode circuit, so you are basically without any protection. I've included a schematic of the power management circuit for a Raspberry Pi Model B+, below.

     

    image

    Despite all these cons, it's still possible to power the Pi through the pins, with a simple circuit. First off, a regulated 5V power source has to be inputted to the 5V and ground GPIO pins. Most power adapters won't output a regulated voltage (unless stated otherwise on them) so you would also need to use some voltage regulator circuit. Lastly, there are a few capacitors used to smooth the voltage, which makes power more stable.

    To power the Pi, you will need to have a regulation circuit, or use a regulated power supply. Then, just add a schottky diode on the input, and maybe a resettable fuse. I hope this helps, and I'll try to provide a schematic of said described circuit.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Dylan, I am also working to a project to power the Pi with a battery. And your suggestion is very good. I was just planning to adopt a solution like this. In your scheme the power is connected to the USB connector, but IMHO with this kind of power control it is the case to use the direct GPIO power connection leaving the USB connector free for the wall mount power supply as an alternative to the battery support.

     

    Enrico