Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum FT5316 touch driver on Raspbian Jessie?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 743 views
  • Users 0 members are here
  • driver
  • touch
  • raspberrypi.
  • ft5604
  • ft5316
  • raspberry_pi
  • jessie
  • raspbian
Related

FT5316 touch driver on Raspbian Jessie?

e14 Contributor
e14 Contributor over 10 years ago

I would like to connect a display with a capacitive touch screen to my Raspberry Pi 2 B running Raspbian Jessie. The touch driver is the FT5316.

I already have the official 7" with FT5604 running, and I would like to know if the two drivers are compatible or not. If no, is there a chance to make the FT5316 work?

Thank you!

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    You should be able to run them both because they are I2C devices and one is on a different I2C bus to the other so they should not collide even if they use the same address

     

    The PI 7" display is using I2C on the DSI Cable, the other comes out on the 40 Pin header

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Perhaps I did not explained well my problem image I'm don't want to work with the two displays together at the same time, I just wonder how can I make the FT5316 based touch screen display work on Raspbian Jessie (only the FT5316 one). Have I to modify or change some modules or drivers? Can I use that display with the current Raspbian Jessei OS?

    Many thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Perhaps I did not explained well my problem image I'm don't want to work with the two displays together at the same time, I just wonder how can I make the FT5316 based touch screen display work on Raspbian Jessie (only the FT5316 one). Have I to modify or change some modules or drivers? Can I use that display with the current Raspbian Jessei OS?

    Many thanks image