Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What's Your Pi Plan??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 248 replies
  • Subscribers 723 subscribers
  • Views 21590 views
  • Users 0 members are here
  • video
  • hdmi
  • single_board_computer
  • single_board_computers
  • media
  • xbmc
Related

What's Your Pi Plan??

e14 Contributor
e14 Contributor over 14 years ago

Hi!

 

Just curious about what people were planning on using their Raspberry Pi's for once they started getting them!??

 

Current plan- SFF Media PC / NAS etc mounted onto the VESA on the back of my TV

 

Later plan- Replace car stereo etc with RPi

 

Probably not the most origional use there but still, godda start somewhere!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I developed a GPS board addon for the RPi

     

    Added some bluetooth, some external SRAM, high power LEDs, temperature sensor and ports for I2C for other sensors

     

    https://lh3.googleusercontent.com/-5ruw070Hu00/T1DUxZhVDHI/AAAAAAAAEeQ/2PQ53dfEVwc/s288/IMG_20120301_205107.jpg

     

    https://lh4.googleusercontent.com/-2mfgZvqS9fM/T1DUtbwKijI/AAAAAAAAEeQ/eX2rQhnZIbk/s288/IMG_20120301_205124.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    I developed a GPS board addon for the RPi

     

    Added some bluetooth, some external SRAM, high power LEDs, temperature sensor and ports for I2C for other sensors

     

    https://lh3.googleusercontent.com/-5ruw070Hu00/T1DUxZhVDHI/AAAAAAAAEeQ/2PQ53dfEVwc/s288/IMG_20120301_205107.jpg

     

    https://lh4.googleusercontent.com/-2mfgZvqS9fM/T1DUtbwKijI/AAAAAAAAEeQ/eX2rQhnZIbk/s288/IMG_20120301_205124.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    My intention is to make a mini driving chess robot. I'm an average programmer and studying ICT in Business, bit of both worlds.

     

    My ultimate goal would be a little robot car running a chess engine or online chess environment (like FICS). With very tiny wheels, board mounted vertical, so it squeezes at the sidelines or on the board.

    A little camera, or for testing my current webcam, will detect the moves. The state of the board is stored in the computer, like any chess engine.

    For moving pieces, it would therefore now which squares are free, and be able to calculate the path before moving really quick.

    For detecting moves, it would know which moves it has to check and will calculate its path for checking using the squares that will be free in any case.

     

    Is this feasible or impossible to do? My idea is that i should start on a large sheet of paper, draw my own chess board, and place little pieces on there. Use my own big webcam, and don't care too much about miniature. It's just a proof of concept.

    I think that it's the computing power on small surface in raspberrypi that could be the brain of a standalone chess player / mover.

     

     

    Greetings,

     

    Wouter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Wow! I love the GPS addon. what are you using? Sirf? I'd only considered using it for weather etc. More info on your solution would be gratefully received. Reckon I could develop a fuel sensor to give data alongside the GPS and feed it through NMEA2000 to a data screen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Very cool! Do you have the project details online somewhere?

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The bluetooth would eventually talk to other devices I'm building such as a CAN enable MCU that talks to the car, maybe some distance sensors, or maybe a bluetooth powered remote ignition. Im also considering a GPRS solution for remote access but that is still being planned

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MattyLad
    MattyLad over 14 years ago in reply to e14 Contributor

    I'm making a Pisatellite with mine, first though I'll have to make a PiRocket to get it up there.

     

    You will need this to work with your planned PiGPS units.

     

    Although eventually it may well become a PiShelfspaceUnit image

     

    Starting out as an XBMC media player thingy I think I'll dig out some of the interface boards I have in the cellar

    and control the world or perhaps just a few LED's.

     

    If I was allowed to put an LED message board in the back of the car to tell people to check their back lights, get off my backside

    or pull over and take the bus then that may be a good project for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Some great input here.

    I liked the GPS board development, Herson will you be making this GPS project open source?

    My background is mechanical engineer in automation who migrated into PC's via the CNC/CAD/CAM route and have been deploying large IT systems for over 15 years. Last year I gave up my job to start a new school here in Ireland as I want to contribute to the overall success of society by investing in creative talent.

    I intend running courses on computer programming (or whatever else I can do with these) and opening them to our own students and also to network with homeschooled students and other similar schools through the country and make the sessions available over the web using ustream TV or similar.

    I had also considered deploying a ThinStation build on the RPi as they would seem to suit being used as a low cost thin client device.

    My intention was to run an entirely open source (ulteo or similar) cloud compute environment with edubuntu at the back end and leverage off my IT knowledge to kick start interest in engineering & computing in general in our young people.

     

    That's also why I was hoping something like Herson's GPS project would be open sourced so we could try our hand at some electronic innovation too.

     

    Keep the ideas coming as it's great imagination fuel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    yeah, it will soon enough. Im currently developing the firmware for the built in microcontroller. The good thing is, it can actually function by itself without the RPi. I still have to create another PCB for CAN operation that interfaces directly to a car system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Check this remote chess robotic system which used the arduino microcontroller. Cool use of under board magnets / sensors to move the peices plus over the net comunication why havent i seen this as a comercial product yet??

     

    http://www.youtube.com/watch?v=dX37LFv8jWY