Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What's Your Pi Plan??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 248 replies
  • Subscribers 723 subscribers
  • Views 21756 views
  • Users 0 members are here
  • video
  • hdmi
  • single_board_computer
  • single_board_computers
  • media
  • xbmc
Related

What's Your Pi Plan??

e14 Contributor
e14 Contributor over 14 years ago

Hi!

 

Just curious about what people were planning on using their Raspberry Pi's for once they started getting them!??

 

Current plan- SFF Media PC / NAS etc mounted onto the VESA on the back of my TV

 

Later plan- Replace car stereo etc with RPi

 

Probably not the most origional use there but still, godda start somewhere!

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 14 years ago

    I have at least sort of two different plans with the Raspberry Pi

     

    1- Use it for research on low cost embedded Linux application development as a remote or central controller for other systems, Internet of Things kind of stuff

        Some of the stuff I'm working on I started to post it here http://www.element14.com/community/thread/18981?tstart=0

     

    2- I was planning to put together sort of a development lab, contributing my time and funding to have a bunch of R-pis on a local High School, but I'm having second thougths about it given that I'm loosing confidence in the Raspberry Pi Foundation to be able to deliver, and some attitudes that have been developing over there, on top of some of the techincal issues related to the board. I'll probably put the money on something more reliable and with more features, it will probably be more expensive but at least it won't blow up TVs or force me to try a collection of power supplies, SD cards, keyboards, etc, etc, to make sure they work

     

    I was really excited about the R-pi, I've other ARM based development boards such as Beagleboard, Beaglebone, Pandaboard, etc., but my level of exciment with the Pi declined considerably, I'm now waiting for shipment of the http://apc.io/.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    jamodio wrote:

     

    I was really excited about the R-pi, I've other ARM based development boards such as Beagleboard, Beaglebone, Pandaboard, etc., but my level of exciment with the Pi declined considerably, I'm now waiting for shipment of the http://apc.io/.

     

    -J

    The apc looked interesting, sensible size, mounting holes in the corners but the 720p & no general purpose i/o is a downer. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    When I got into the microprocessor world I learned to program with six seven segment displays, so 720p for programing in Phyton does not sound that bad.

     

    I really have no clue how good/bad this board is going to turn, information still sketchy, pictures and overall design looks good, it has VGA much better than composite video if you don't want to go HDMI, form factor is sort of standard in the PC world, and comes!! with a power supply.

     

    I placed my preorder last month, they are expected to start shipping during July.

     

    It Android runs decently well, it could become an interesting platform for development and experimentation with Android applications, and I've no doubt that sooner or later some folks (including me) will cut an Linux kernel image, well after all in Android the kernel is Linux :-)

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    jamodio wrote:

     

    When I got into the microprocessor world I learned to program with six seven segment displays, so 720p for programing in Phyton does not sound that bad.

     

    The WonderMedia WM8750 does 1080p, so not really sure why APC has limited it to 720p -- http://www.wondermedia.com.tw/en/products/platform/soc/wm8750/index.jsp

     

    It might just need a small hack to get it working at full SoC spec.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    jamodio wrote:

     

    When I got into the microprocessor world I learned to program with six seven segment displays, so 720p for programing in Phyton does not sound that bad.

     

    --- snipped ---

    -J

    When I wrote my first test program it was for a multiprocessor 16 bit industrial mini programmed in octal and displayed on rows of filament lamps. Used to be able to read the octals but wasn't sorry to move to hex! Paper tape input and output. No end to this theme..........

     

    I will hopefully be using my Pi for a media server  from NAS but also on the side I would like to interface with an existing Arduino weather station. Never got that connected past an LCD display but it will be great to see the data up on the big screen. So some XRF radio to interface to hence the need for external I/O.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    jamodio wrote:

     

    When I got into the microprocessor world I learned to program with six seven segment displays, so 720p for programing in Phyton does not sound that bad.

     

    --- snipped ---

    -J

    When I wrote my first test program it was for a multiprocessor 16 bit industrial mini programmed in octal and displayed on rows of filament lamps. Used to be able to read the octals but wasn't sorry to move to hex! Paper tape input and output. No end to this theme..........

     

    I will hopefully be using my Pi for a media server  from NAS but also on the side I would like to interface with an existing Arduino weather station. Never got that connected past an LCD display but it will be great to see the data up on the big screen. So some XRF radio to interface to hence the need for external I/O.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Nice !!!

     

    I know what type of system you mean, I worked with one that was donated to our school that have that type of display, it was actually a "a direct register" machine, the instruction set was spread on a keyboard, and in fact numeric values were entered in octal.

    The printer was a teletype attached to the monster, RAM was actually magnetic cores, and storage was fortunatelly not perforated tape but magnetic tape.

     

    After a while, the thing became our best source of TTL integrated circuits for other experiments.

     

    I think is possible but I really don't see the Pi as a good media server, but for the weather station and connecting with Arduino that will probably work great, think about trying to use ZigBee, some modules include both the RF transceiver and a little MCU, or an RF-MCU combo that runs the ZigBee protocol and you can use different ways to talk to it, via UART, I2C or SPI.

     

    That sounds like an interesting project with the Pi.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    It's a gathering of old-timers here.  You too probably remember reading code by holding up paper tape to the light. image

     

    The Pi founders talk about the BBC Micro like it were the dawn of computing, but really they were 2nd or 3rd generation, just users of consumer gadgets with all the rough edges smoothed off for public consumption.  The hardcore technical work came before that.

     

    Programming in Python won't really tell youngsters much about their machinery, although hopefully it will get them interested in technology in general, so it could be a stepping stone away from consumerism and towards better understanding.  I hope so.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    http://ccgi.royles.force9.co.uk/gallery2/main.php?g2_view=core.DownloadItem&g2_itemId=39&g2_serialNumber=4

     

    Picture of part of a core plane from a scrapped display system that I kept. Few bits there!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Haha, nice.  I guess I'm a newbie compared to that, but I did possess a 64 KB hard drive (yes, Kilo) ex PDP-7, and I still have a pile of those old DECtape cases which I use for component storage.  Oh and I preserved a 2MB RK07 removeable disk pack for posterity, just because it was reputed to be the base model for Hans Solo's Millennium Falcon. image

     

    From a slightly more modern vintage, one of my main racks here is from a PDP-11/34.  I'm so sad that I didn't grab the old PDP-11/20's binary toggle switches when the machine was thrown away, on which I'd entered the bootstrap code from memory so many hundreds or thousands of times.  I'm not really much into memorabilia that isn't functional, but the switch panel could have been interfaced nicely to an ARM Cortex to make a pretty unique UI for binary-aware techies. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Ohhh my, this is g33k p0rn :-)

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    When I moved from New Jersey (where I had a basement) to Texas, I had to leave behind a lot of equipment. I worked for several years with the company that ran one of the original NSFNet regional networks, JVNCNet that was build around the Princeton University and the John Von Neumann supercomputer center, after the center closed we inhireted a lot of stuff.

     

    Some PDP-11 19" racks ended in my basement to mount part of the equipment I used for R&D in large scale networking and other stuff, in front of the racks shown in the picture I had a running PDP-11 and a Microvax, can't find where I put a picture of that one.

     

    image

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    @jamodio: Yup, same rack system, except that mine has an ornamental head section and I still have the slot-in side covers on mine which you've removed there.  Awesomely strong hardware, built to last forever unlike some modern racks.

     

    I was so sad when DEC were purchased by Compaq, a mere PC company.  I knew it was the beginning of the end for their professional quality hardware. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    You bet Morgaine, I also miss DEC a lot, and the old Hewlett Packard too, I remember anxiously waiting for the latest catalog or HP Journal to arrive on the mail, now not even Circuit Cellar is worth the money.

     

    Some of the things I still have with me, is a collection of HP Series 80 desktop computers, once in a while I still use them to control via HP-IB a bank of instruments.

     

    Here are some pics about how my office/lab looks like:

    https://picasaweb.google.com/110518276636040092961/MyHomeLabAndOffice?authuser=0&feat=directlink

     

    Sorry Folks for the totally OT thread :-), but kind of interesting to exchange some of this stuff.

     

    Cheers

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    It's a gathering of old-timers here.  You too probably remember reading code by holding up paper tape to the light. image

    We mostly had pink paper tape, so you didn't need to hold it up to the light like black paper tape.  Yellow paper tape had an icky color IMO.

     

    For one class, we had limited access to a shared PDP-11/20, so I entered the first draft of my PDP-11 ASM programs using an off-line ASR-38 teletype, punching the program directly onto paper tape.  You had to type carefully because it had limited back-space capability.  If you made a mistake, you pushed the punch's backspace button one or more times and then typed one or more DEL characters, which as you all know from the ASCII chart is all ones.  This told the paper tape reader to ignore the deleted characters.  Then I transferred my program on DECtape and fixed the remainng typos and made other modifications with a text editor.

     

    Everybody else in the class used punched cards.  However, the card reader was flaky, so when it was down I got extra access to the PDP-11 :-)  Using the ASR-38 allowed me write lower case comments.  This was considered heresy and made me an outcast among outcasts :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    From a slightly more modern vintage, one of my main racks here is from a PDP-11/34.  I'm so sad that I didn't grab the old PDP-11/20's binary toggle switches when the machine was thrown away, on which I'd entered the bootstrap code from memory so many hundreds or thousands of times.

    We had a hardware tech who liked to play a little joke after fixing the front panel, e.g., replacing one of the many incandescent light bulbs that displayed address and data.  He would run a program which executed code at clever addresses so it looked like the address lights were counting in binary, but bit reversed.  Then he's say "oops, I must have hooked up the address lights backwards" :-)

     

    I never had to enter PDP-11 bootstrap code -- we must have had the ROM option.  OTOH, I remember toggling in the PDP-8 RIM loader, which then read in the BIN loader, which then read in the actual program.