Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum ports
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 641 views
  • Users 0 members are here
  • raspberry_pi
Related

ports

e14 Contributor
e14 Contributor over 14 years ago

Hello

I think the next about ports:

 

- There is a discussion about hdmi/vga. I think VGA port is interesting, because there are a lot of old monitors (and smalls) where maybe we would like to connect the RPi. In my case, for example, I will use RPi using VNC, but at the beggining I need to connect it to a display. However, I think that RCA out is less useful.

 

- I think that RJ45 port is suppresible, because we can use and usb-wifi deive or a usb-lan card (like this http://www.ebay.es/itm/Ethernet-External-USB-to-Lan-RJ45-Network-Card-Adapter-10-100-Mbps-for-Laptop-PC-/270926546529?pt=LH_DefaultDomain_0&hash=item3f147b0661)

 

I suppose that these ideas can be interesting for future versions of RPi.

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    There are USB VGA adaptors available starting around $30. 

     

    VGA is not a trivial item to add.  It's all analog, and the chips to do it aren't cheap.  It could potentially double the cost of the board.

     

    HDMI/DVI/Composite are all integrated into the system-on-a-chip, so that's basically free - all that was needed to support it was basically the plugs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    There are USB VGA adaptors available starting around $30. 

     

    VGA is not a trivial item to add.  It's all analog, and the chips to do it aren't cheap.  It could potentially double the cost of the board.

     

    HDMI/DVI/Composite are all integrated into the system-on-a-chip, so that's basically free - all that was needed to support it was basically the plugs.