Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Small monitor options for R-Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 715 subscribers
  • Views 9599 views
  • Users 0 members are here
  • raspberry_pi
Related

Small monitor options for R-Pi

e14 Contributor
e14 Contributor over 14 years ago

So, I know many people will want to hook the R-Pi up to a 50-inch HDTV, but some of us will want to keep it small (such as for a CarPC). I am not thinking about touchscreen capability, simply small LCD displays. So, there are $1000 5" to 8" LCDs meant for digital photography, but that is nuts. So, I found that small portable LCD TVs should be the way to go. The cheap Coby and Axion 7" LCD TVs have RCA/composite video input jack, and luckily the R-Pi also has an RCA/composite video output jack!  They are about $50 to $60.

 

Coby

http://www.bing.com/shopping/coby-tf-tv791-7-lcd-tv/specs

 

Axion

http://www.bing.com/shopping/axion-axn-8701-7-lcd-tv/specs

  • Sign in to reply
  • Cancel
Parents
  • recantha
    recantha over 14 years ago

    I invested £21 in a car rear view parking screen. It works through the composite socket on the Pi. I just had to find a 20V power cable (which I had hanging around). It's a 3.5" screen, which means it's small, but you can still just about read text on it, and I've done plenty of bash commands and text editing through it. X windows also works on it and shrinks to fit. I like it, in that it suits the purpose I bought it for. What's particularly nice is that it's roughly the same size as my Pi enclosure so attaching the two together is a definite possibility. It folds down, too, screen side down, so it's nicely protected for transport.

     

    image

     

    http://www.ebay.co.uk/itm/200775489378

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • recantha
    recantha over 14 years ago

    I invested £21 in a car rear view parking screen. It works through the composite socket on the Pi. I just had to find a 20V power cable (which I had hanging around). It's a 3.5" screen, which means it's small, but you can still just about read text on it, and I've done plenty of bash commands and text editing through it. X windows also works on it and shrinks to fit. I like it, in that it suits the purpose I bought it for. What's particularly nice is that it's roughly the same size as my Pi enclosure so attaching the two together is a definite possibility. It folds down, too, screen side down, so it's nicely protected for transport.

     

    image

     

    http://www.ebay.co.uk/itm/200775489378