Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What Arm do you plan on running?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 708 subscribers
  • Views 1013 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • pi
  • raspberry_pi
  • raspberrypi
Related

What Arm do you plan on running?

e14 Contributor
e14 Contributor over 14 years ago

Hello everyone,

 

     I was Wondering what everyones choice for an Arm/OS they are plannig on running and why? I am not the most experienced in Linux just the little I have learned in my IT degree for Linux has caught my attention. I Dont know themain difference between the three, Debian, Arch, or Fedora, I have only used Fedora. Any insight or sugestions would be great and aid in my descision on which one to run when I recieve the RPi.Thank you ahed of time for you sugestions and answers.

 

Bjorn

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 14 years ago

    I won't be getting a RasPi from the first batch, so I'm going to read the comments from RasPi pioneers at raspberrypi.org and here to see what problems there might be with the various distros.  The current information is that Fedora is intended for new GNU/Linux users who want to be sheltered from OS details and Fedora will the be the OS for the education-oriented launch later this year.  Debian is better suited for serious developers.  Arch is smaller and uses less memory, but requires more GNU/Linux knowledge.

     

    Personally, I expect I'll be going with Debian, about which I've always heard good things.  I need gcc from day one, which is not included by default in Fedora.  Supposedly it's easy to download packages for any of the distros, especially the first two.  I don't see any point in downloading anything until I have a firm ship date for my RasPi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to johnbeetem

    I personally have moved from slackware, to suse, to redhat, to debian to ubuntu.

     

    What I like about debian/ubuntu is that with "apt-get install XXX" you get to download/install a package. Easy. I hear this is now also possible with redhat/fedora, except that the program is called "yum".

     

    Other than that, they should be somewhat similar. If you WANT you can dive in and change low-level stuff. If you don't you can stick with using the programs offered.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    As my interest in the Raspberry Pi is purely intended for use as a Mediacentre, I was planning on going for the Raspbmc distribution being developed at the moment.

     

    http://www.raspbmc.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I'll try them all, since none of them are my distro of choice which is Gentoo, and Gentoo is probably inappropriate for Rpi because compiling everything from scratch natively would take so long on the Pi's weak CPU.  Also, the continuous rewriting of storage that source-based distros like Gentoo perform acts against SDcard longevity, as well as taking up a lot of space.  I could cross-build Gentoo for the Rpi, but native use is probably not viable.

     

    One distro that seems very suitable for Rpi is the minimalist Puppy Linux, so I'll keep an eye open on progress there as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    this earlier post may be helpful:

    http://www.element14.com/community/thread/17582?tstart=90

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    You wrote:

     

    > Neither Debian nor Fedora has GPU accelerated X Window drivers,

    > and neither is built specifically for the v6 ARM11 architecture.

     

    Has anything been mentioned on the blog or elsewhere about a distro with X acceleration and also compiled for the Pi's specific architecture?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Apparently, nobody is working on X acceleration, and one guy is working on

    compiling Debian for ARM 11.

     

    http://www.raspberrypi.org/forum/projects-and-collaboration-general/debian-hard-float-armhf-for-rpi

    http://www.raspberrypi.org/forum/general-discussion/so-whos-workingworked-on-an-xorg-server

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Yeah, something like puppy linux or even DSL would be great for the Raspberry pi. I remember running DSL entirelly in RAM on a pentium4 machine with 500MB RAM. It made my Core2Duo with 4GB RAM look slow image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I still have a working P2 with 32MB and a couple of P3's with 64MB running firewalls, and Linux loves them (various distros).  It really doesn't need much RAM to be perfectly happy. image