Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How can I interface the PI to sensors ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 710 subscribers
  • Views 2422 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • raspberry_pi
  • raspberrypi
Related

How can I interface the PI to sensors ?

GreenYamo
GreenYamo over 14 years ago

Sorry if this has been asked before

 

I have experience playing around with the Arduino platform and interfacing sensors such as temperature, pressure etc.

 

I would like to know how this would be possible with the PI. I have seen the 'Gert Board' and also the board produced by Ciseco here: http://shop.ciseco.co.uk/slice-of-pi/. Is it as simple as plugging in sensors (and of course the odd LED or two) to the general I/O pins mentioned in the description for the last item and writing some code to read / write to these (I'm hoping in Python?).

 

Would I do better to learn more about I2C and SPI to get the most of the Pi ( I have seen you can do this on the Arduino, but i'm somewhat a beginner so keeping it simple at the moment). If so, can anyone recommend a good primer on I2C and SPI for the Arduino?

 

Given the power differential of the Pi to the Arduino in terms of processing power I think this would be a great platform to work on for this type of exercise.

 

Thanks for any pointers.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I built my own GPS board but has a separate microcontroller that can talk to sensors. The RPi and the MCU talks via serial connection through the onboard UART on the headers.  So in essence, I can send a command to the MCU to grab sensor data. Something like  root:>$GPS#LAT? root:>$LED1#ON? root:>$SENS#TEMP1? root:>$SERV#145?  of course, the MCU would have to be programmed to grab sensor data continuously and respond to command received from its serial port  that's just example. its better (at least for me with MCU experience) than messing around with Linux SPI/I2C kernel drivers.  also makes it easier to interface with higher level applications like php/java/etc.

     

    https://lh5.googleusercontent.com/-KRuqdpwOfAU/T1xBaaTHZkI/AAAAAAAAEf0/8Y0JGUxLS6g/s640/IMG_20120310_191400.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    I built my own GPS board but has a separate microcontroller that can talk to sensors. The RPi and the MCU talks via serial connection through the onboard UART on the headers.  So in essence, I can send a command to the MCU to grab sensor data. Something like  root:>$GPS#LAT? root:>$LED1#ON? root:>$SENS#TEMP1? root:>$SERV#145?  of course, the MCU would have to be programmed to grab sensor data continuously and respond to command received from its serial port  that's just example. its better (at least for me with MCU experience) than messing around with Linux SPI/I2C kernel drivers.  also makes it easier to interface with higher level applications like php/java/etc.

     

    https://lh5.googleusercontent.com/-KRuqdpwOfAU/T1xBaaTHZkI/AAAAAAAAEf0/8Y0JGUxLS6g/s640/IMG_20120310_191400.jpg