Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum TTY Into Raspberry Pi Via USB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 706 subscribers
  • Views 1665 views
  • Users 0 members are here
  • frontpage
  • raspberry_pi_space
Related

TTY Into Raspberry Pi Via USB

screamingtiger
screamingtiger over 10 years ago

I know that I can take an Arduino programmer and plug it into my computer, then connect the RX/TX to serial of the pi.   I believe that will work.

Im also thinking that if I used two of the programmers, one connect to the pi usb and the other a PC usb, that I could SSH in that way as well and leave the serial port free.

 

What would be nicer, if there is a way using only the USB ports and no serial converters.  I would need an adapter since they are both host usb but just curious.

 

Id like to work on projects at work during lunch but they have blocked SSH at the protocol level so a change in ports wont work.   I could just bring the pi to work but having two programmers connected up makes it kind of a mess...

 

just plugging the USB ports together would make it much easier!

 

Ideas?

  • Sign in to reply
  • Cancel
  • clem57
    clem57 over 10 years ago

    SSH means TCP/IP stack protocols.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 10 years ago

    Good point, telnet, not SSH

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 10 years ago

    I guess telent is tcp/ip too.  I want to open a console using usb ports only, old fashioned serial communciations vie USB port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to screamingtiger

    Console is not TCP/IP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 10 years ago

    Right, so I am using serial (TTY).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 10 years ago

    It appears that unless I have a driver than make a USB port look like a com port on both systems, it wont work.

     

    So the easiest way is to use an ardunio programmer (FDTI) and connect that to my PC, that will in turn make a USB port look like a com port.

     

    Then I can use the serial port built into the Pi and connect up the RX/TX.

     

    Then it is only a matter to ensure a console is opened up on /dev/TTYS0 and I can "serial" in to the pi.

     

    Since I am using a PC, the putty program I normally use to SSH does have a serial option.

    Unfortunately this requires the programmer or a USB<->Serial adapter but they are small.