Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum after a wi fi dongle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 709 subscribers
  • Views 20289 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • pi
  • raspberry_pi
  • raspberrypi
Related

after a wi fi dongle

cullimore
cullimore over 14 years ago

hi there,

 

i am after a wi fi usb dongle for when i get my Raspberry Pi.

 

will any wi fi usb dongle work?? will drivers be available??

 

cheers

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Drew, are you going to test the wifi adapter listed as a R-Pi accessory to check it works?

    http://uk.farnell.com/micronext/mnwd152b/adaptor-wireless-n-usb/dp/2081765

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Hi Paul, a colleague in the UK (user ajtag in fact) had compiled that 8192cu.ko module to get the Micronext MNWD152B working.  I'll ask if he can chime in with some additional details of testing, but to my knowledge, it did work ok.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Arch does not boot with my Edimax EW-7811Un dongle inserted. I have to blacklist the standard module.

     

    I tried:

     

    install -p -m 644 8192cu.ko /lib/modules/3.1.9+/kernel/drivers/net/wireless/

     

    followed by:

     

    depmod -a

     

    and added the file rtl8712u.bin as per http://www.raspberrypi.org/forum/troubleshooting/trying-to-get-an-rtl8188cus-wireless-usb-nic-working to:

     

    /lib/firmware/rtlwifi/rtl8712u.bin

     

    and it still fails.

     

    If anyone has any success with Arch I'd love to hear from you.

     

    Felix

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Is there any related errors in the kernel log?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Quick update. I managed to get the Edimax EW-7811Un working by following the instructions above.

     

    The process worked for me on Debian but not Arch images.

     

    In the process, I discovered that the dongle would *only* work if it was connected directly to the R-Pi usb port and would *not work* through a powered usb hub.

     

    This is surprising since I was attempting to protect the Pi from excessive power drain, but in fact it was actually the cause of the problem.

     

    Perhaps this is an incompatability with this particular hub.

     

    For the record the hub in question is a (lsusb)

     

    05e3:0608 Genesys Logic, Inc. USB-2.0 4-Port HUB

     

    Anyway, thanks for the help. I can confirm Edimax EW-7811Un as working (on Debian)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cullimore
    cullimore over 14 years ago in reply to e14 Contributor

    glad this works as i just brought one for my Pi. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    The WiFi document here: http://www.element14.com/community/docs/DOC-44703 and at least three other people on the raspberrypi forum have made the same observation: a WiFi adaptor works directly on the Pi, but NOT from a powered hub, even with a fully adequate power supply to the hub.

    http://www.raspberrypi.org/forum/troubleshooting/usb-power-hub-wifi/page-3

     

    Based on other reports about USB packet loss http://www.raspberrypi.org/forum/troubleshooting/usb-packet-loss

    and the USB and Network issues reported here: https://github.com/raspberrypi/firmware/issues/9

    I think there is a software problem that is causing many or most WiFi adaptors to fail when connected through a hub.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Thanks for posting those links.  I definitely was baffled at times by the behavior of using USB hub.  Some adapters worked ok from USB hub and others did not (smsc95xx register r/w errors).  The last I tested I realized all the adapters stopped (darn smsc95xx errors) working when I added a mouse, trying both the powered hub and direct.

     

    Interesting to know there might be a kernel issue.  I had been suspicious power was an issue.  The only insight I had was DMM on TP1/TP2 which gave me a solid 5.1V everytime I checked.  I'm hoping to get access to a Pi again next week to do some more testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Just to repeat what I posted on the RasPi forum:

     

    There is hope. Two days ago (April 30) there were several USB subsystem commits marked "added support for TT in the USB driver". See below for what that means. I am not sure, but I think it means in this case, if your hub is running at USB High-Speed for the USB WiFi device, and if you also have a keyboard or mouse (low-speed USB protocol) on the same hub,  then it would not work without TT.

    A USB hub consists of a Hub Repeater section, a Hub Controller section, and a Transaction Translator (TT) section. [...] The Transaction Translator (TT) takes high-speed split transactions and translates them to full-/low-speed transactions when the hub is operating at high-speed and has full-/low-speed devices attached. from http://www.cypress.com/?id=4&#…..;rID=54981

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Thanks for digging that up.  Very interesting about low-speed versus high-speed.  I never even thought of that.  I look forward to testing again soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>