Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 713 subscribers
  • Views 26454 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 14 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    There's a nice new write-up of Valent F(X) FPGA boards for RasPi and BeagleBone at Linux Gizmos: BeagleBone and Raspberry Pi gain FPGA add-ons.  Boards not yet available commercially, but they're considering a Kickstarter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Very interesting.  I had a good chuckle at "LOGI-BONE SLIM" and "LOGI-BONE PHAT". :-)

     

    Care to hazard a guess at pricing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Very well presented and argued, John.  I agree in every respect.

     

    The day that you have a rudimentary open source tool that works with a specific programmable logic device, whichever that may be, I'll be very happy to buy the hardware and experiment with your code, and hopefully help you improve it.  It never hurts to have extra testers, and that's a very low barrier to entry for anyone wishing to support the development of open source EDA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    this is absolute rubbish,

    VHDL is both a simulation and design language the fact that you find it hard to use is not down to the language but down to your lack of understanding over how to use it correctly, if you have difficulty learning a tool the best way to understand it better is to practice using it. there is no demand for an open source FPGA design tool because nobody else has the issues that you state that you have,

    Ive been using Xilinx, altera and actel tool sets for donkeys years and Ive seen many attempts to rewrite VHDL into something simpler but they always fail due to the huge complexity of the task. The complexity of writting a VHDL synthesis tool capable of handling all devices from all vendors and covering all the VHDL functionality and verifying that it works correctly is stupendously large.I know for a fact that the latest synthesis tools from Xilinx for example took something in the region of 575 man years to write and verify,  and you get it for free..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I once had some idiot telling me that he wanted to rewrite XST because it couldnt handle the complexity of his code, puzzled I had a look at his code, the reason XST couldnt handle it was it written as if it was software and was full of aysncronous feedback loops so XST was spitting it out. He was a self proclaimed software genius.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    I'm a long term VHDl user but I'm currently forcing myself to use Verilog on a project in order to widen my horizons. There are a great many Verilog users and I doubt that the only reason that they don't use VHDL is prejudice or stupidity. By the same token it is obviously possible that a better solution than either VHDL or Verilog might be devised.

    It isn't necessary to leap right in and write a complete tool chain to make a contribution. One of the downsides of VHDL (and Verilog) is the number of mindless (but significant) lists of ports required to define and join up different components. There are several relatively simple tools you can use to manage or automate this process but I'm sure that better ones are possible.

    Starting from the other end is possible too - VHDL -> FPGA sysnthesis is very complicated but gate level -> FPGA could be quite simple. It was essential to get any performance out of Xilinx's first FPGAs with an 8 x 8 array of logic cells.

     

    The problem with the current situation, where the tools are almost all closed and locked to some degree to the silicon vendor, is that experimentation is usually directed towards gaining market advantage which is not always alligned that well with the long term. Having more competition and more lateral thinking in FPGA tool development would be a good thing.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to e14 Contributor

    IMHO the "good thing" that would come from an open source FPGA compiler would be that the open source community, together with universities, can work on algorithms and methods to improve the whole process for everybody. i.e. improve the set  of known algorithms and methods for the world as a whole.

     

    Such a compiler would need to be well-thought-out, so that it would be very modular. Then incremental improvements can be made. Someone improves a placer, someone makes a better router. Sometimes such a step takes the form of an improvement of an existing program from the "suite", sometimes it is a new algorithm in a new addition to the suite.

     

    This allows universities to set tasks for students like: implement this improved algorithm in the free-fpga-suite. Or allow researchers to suggest improved algorithms and test them out.

     

    Once things start rolling, it should become relatively easy to extend the suite with smaller projects. New output modules for specific architectures, or just a new chip.

     

    For the users who don't want to mess with the code, the advantage is that they get better uniformity between vendors. Now if you write something for a xilinx, porting it to altera means you probably run into a few snags. Things that don't compile right away. That's called vendor lockin. They like that. It makes it harder for you to go to the competition, yet not hard enough that they can't win over the big professional players.

     

    Software compilers are more "common" than the hardware ones. So if 1% of the users is able to contribute, you have a much larger pool of developers for say "GCC" than the "open source FPGA project". That in turn might mean we're missing a "critical mass" for things to start rolling.

     

    So... Although I think it's likely that "it will never happen", I do see advantages to the open source FPGA project. Maybe if I was a professor at a university I'd be able to get such a project going. But as it is I'm not in a position to invest the required amount of time and effort in such a project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rew

    rewriting the language or rewriting the tools because you dont know how to use them is not the way forward, the 'digital handcuffs' are there to ensure that designs are done to best practices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to e14 Contributor

    You are writing that in response to what?
    YOU are the one making that point with your XST post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to rew

    Roger Wolff wrote:

     

    IMHO the "good thing" that would come from an open source FPGA compiler would be that the open source community, together with universities, can work on algorithms and methods to improve the whole process for everybody. i.e. improve the set  of known algorithms and methods for the world as a whole...

     

    So... Although I think it's likely that "it will never happen", I do see advantages to the open source FPGA project. Maybe if I was a professor at a university I'd be able to get such a project going. But as it is I'm not in a position to invest the required amount of time and effort in such a project.

    I don't think it needs an organized project.  Indeed, my experience at trying to get academics to work together on anything is far worse than "herding cats".

     

    But what it does need is FPGA architectures with open documentation so that interested individual researchers can see something actually working instead of just writing papers.  Then people can work on the bits that interest them, and if they release the results under a FaiF license the community will be able to collect the results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    this is absolute rubbish,

     

    VHDL is both a simulation and design language the fact that you find it hard to use is not down to the language but down to your lack of understanding over how to use it correctly, if you have difficulty learning a tool the best way to understand it better is to practice using it. there is no demand for an open source FPGA design tool because nobody else has the issues that you state that you have,

     

    Ive been using Xilinx, altera and actel tool sets for donkeys years and Ive seen many attempts to rewrite VHDL into something simpler but they always fail due to the huge complexity of the task. The complexity of writting a VHDL synthesis tool capable of handling all devices from all vendors and covering all the VHDL functionality and verifying that it works correctly is stupendously large.I know for a fact that the latest synthesis tools from Xilinx for example took something in the region of 575 man years to write and verify,  and you get it for free..

    I'll speak to Verilog and Xilinx since that is what I use most.  I don't like to type more than necessary and I have limited space for source code listings.

     

    I'm able to get excellent results from Verilog and Xilinx tools, but it's not easy.  If you want to get the right results from Verilog (and I assume VHDL) you have to write your source code so that XST matches the templates to use the correct FPGA resources.  Since I did my Ph.D. and later industrial and academic research on CAD tools, it's easy for me to visualize how XST works and help it get the right results.  I think I'll call this Human-Aided Computer-Aided Design.  It's like a primitive C compiler with poor optimization where the programmer needs to know how to write source code that helps the compiler generate decent machine language.

     

    My point upstream is that this is a lot to dump onto a new FPGA designer.  Sure, an experienced Verilog or VHDL designer has learned how to write code to conform to the eccentricities of the tools, but newbies are going to have a lot of trouble -- something that gets worse as new tool releases add more complexity and steepen the learning curve.  Duane Benson gave an excellent talk called "FPGAs: I know nothing... yet" at the 2013 DesignWest conference.  Duane is an accomplished microcontroller designer and wanted to give his perspective on the challenges of coming up the FPGA learning curve.  The reality from Duane's point of view is that it's really hard to get started.  As I said upstream, the FPGA vendors seem to think that everything is fine and dandy in Toolsville, an opinion you seem to share.

     

    Regarding the complexity of the VHDL tools: yes, I suppose if I were using VHDL as the starting point the problem would be intractable for an individual or a small group.  I also wonder what the late John McCarthy would say if he saw Xilinx's code? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to johnbeetem

    John, one of the differences between VHDL and Verilog is that VHDL is more verbose. Thinking it was more or less an arbitrary choice I went for VHDL first time. The verbosity gets annoying after a while. I had to integrate some Verilog one day and decided to switch.

     

    In C I stick to the rule that I prototype my functions. VHDL requires the prototypes. But whereas a C-prototype will usually be about a line, a VHDL prototype will be about a page.... So that's one of the VHDL things people are complaining about.

     

    Anyway, getting open source FPGA "bootstrapped" means one language -> hardware trajectory implemented. Then adding input modules and output modules should be easy to help things along.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 12 years ago in reply to johnbeetem

    John, one of the differences between VHDL and Verilog is that VHDL is more verbose. Thinking it was more or less an arbitrary choice I went for VHDL first time. The verbosity gets annoying after a while. I had to integrate some Verilog one day and decided to switch.

     

    In C I stick to the rule that I prototype my functions. VHDL requires the prototypes. But whereas a C-prototype will usually be about a line, a VHDL prototype will be about a page.... So that's one of the VHDL things people are complaining about.

     

    Anyway, getting open source FPGA "bootstrapped" means one language -> hardware trajectory implemented. Then adding input modules and output modules should be easy to help things along.