Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Role for FPGA or CPLD with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 713 subscribers
  • Views 26451 views
  • Users 0 members are here
Related

Role for FPGA or CPLD with Raspberry Pi

michaelkellett
michaelkellett over 14 years ago

Interesting - we obviously move in rather different circles despite being in the same business:

 

Take the current project:

 

One master processor (ARM Cortex M4 with ARM serial debugging port and 4 wire trace, Ethernet, USB and serial for debugging)

One supervisor processor (ARM Cortext M0 with ARM serial debugging port)

FPGA with JTAG port

Up to 6 slave processors (ARM Cortex M4s with ARM serial debugging ports)

All in one little box about 25cm x 160cm x 5cm

 

Now to bring up the Ethernet on the master processor I can use its serial port for "printf" error messages (from the Ethernet/TCP/IP library) and the ARM debugging port to load/run/trace the processor. The ARM trace interace box (Keil Ulink Pro) is a USB interface to the development PC.

The superivisor processor is connected via another Ulink to another PC.

The FPGA JTAG interface is USB to yet another PC.

The fourth PC runs Wiresharc and is connected by Ethernet to see what's coming out.

 

It would be nice if the debug tools had Ethernet rather than USB interfaces but they don't.

I could isolate the serial debug port but since I must have three other non-isolated connections it's not worth the effort.

 

This system is all quite low power - so certainly safe to humans and fairly safe to computers. (The really exposed parts are the debug interfaces and there is nothing to be done about that since they need fast conenctions to the hardware.)

In the last 10 years I've lost one debugger and one PC due to my mistakes and in the same time at least 10 PCs have just died (as they do) so it's a cost effective approach.

 

Of course when these things connect to external systems handling real power different rules apply.

 

(AFIK most Ethernet interfaces are not specifically tested for mains safety - either during qualification or as part of normal regular safety checks (and the flash test requirement for Ethernet magnetics is 1500V AC which is OK for some equipment but not for all)).

 

Michael Kellett

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    There's a nice new write-up of Valent F(X) FPGA boards for RasPi and BeagleBone at Linux Gizmos: BeagleBone and Raspberry Pi gain FPGA add-ons.  Boards not yet available commercially, but they're considering a Kickstarter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Very interesting.  I had a good chuckle at "LOGI-BONE SLIM" and "LOGI-BONE PHAT". :-)

     

    Care to hazard a guess at pricing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Packrat? moi? naw. I just can't part with my 1975 RCA COSMOS Digital catalog.

    Who remembers Silicon on Saphire?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    an open source tool chain for FPGA design is frankly a ridiculous idea, all FPGA vendors release and support their own proprietry design software and trying to integrate all the features that they support into a single tool is, well the first question I would ask is why the hell would you even want to think about attempting it?

    The whole idea is typical of the open source software community as a whole, nerds with nothing better to do than bleat about linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    @FF

     

    The economics may be different but in principle the idea of FOSS support for FPGA design is not that different from the GCC concept. At the higher levels of abstraction the tools are (in both cases) hardware agnostic. Actual fitting and routing into an FPGA is very hardware specific (although I'm not sure that FPGA architectures are any more diverse than processors'). The usual way this is dealt with is by a vendor supported software component but completely independent designs are possible.

     

    The question as to why is perhaps less obvious - quite good FPGA tools are available free or very cheap but when you need serious tools it starts to cost a bit more.

    The VHDL/Verilog simulator that I use on a day to day basis costs more than £10k - you can get the same thing for free in a crippled  version (artificially slowed down). If there were an open source version it would run at full speed for everyone so that would fit nicely with the silicon vendors free router/fitter.

     

    The open source community has every right to crow/bleat/be-proud-of Linux - it is hugely successful and has done a lot to stimulate the efforts of others to make better stuff at better prices.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelkellett

    If you have so little to do in your day job that you think rewritting huge amounts of code to no good effect is a good use of your time then maybe you should come and work for me and we'll get you doing real world designs which we have to sell to real customers using the code supplied by the likes of Xilinx and Altera.In my company we spend our time making money by selling designs which people use, rather than dicking about with open source crap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    I'll ignore the somewhat offensive tone and address the substance of your comment.

     

    At no time did I suggest that I would be investing my time in writing FOSS code for FPGA development. The most likely source for such funding would be one of the smaller silicon vendors and the reason that they might do it is that rather than pay Mentor\Aldec etc for the subsidised use of their tools they could fund FOSS and leverage the open source effort that this might attract.

     

    Your perspective of FPGA design is obviously limited by your Altera/Xilinx focus, I already sell designs which people use and I don't use Altera or Xilinx parts. As I explained before I use a paid-for simulation tool.

     

    I'll leave it to others to correct your rather weird generalised open source antipathy - I don't happen to use Linux but I do use some open source tools - and I find the range of quality to be not much different than paid-for but the cost is lower.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    Frippy Frippy wrote:

     

    An open source tool chain for FPGA design is frankly a ridiculous idea, all FPGA vendors release and support their own proprietry design software and trying to integrate all the features that they support into a single tool is, well the first question I would ask is why the hell would you even want to think about attempting it?

     

    The whole idea is typical of the open source software community as a whole, nerds with nothing better to do than bleat about linux.

    I've been advocating for open FPGA documentation for decades, so I'll be happy to address this topic.  Basically, the problem with proprietary tools in general is that if they don't suit your needs, you're stuck.  Here are some of the issues with FPGA tools:

     

    1.  FPGA tools (I'm most familiar with Xilinx and Actel/Microsemi) have a very steep learning curve, which makes them hard for new users to learn.  Since most Xilinx / Altera / Actel / etc. customers are experienced, none of the vendors see that this is a problem.  Indeed, their marketing literature says that the tools are gloriously simple to use, and you can't expect solutions from people who don't recognize that they have problems.  The steep learning curve makes FPGAs hard to teach, so this wonderful technology is out of reach of many who could benefit from it.  It would be like Intel only allowing people to program their processors in PL/M, while refusing to expose the machine language so that others could write compliers.

     

    2.  FPGA design languages -- VHDL and Verilog -- have a lot of problems.  While they aren't too bad for expressing behavior, it's very tricky to use them to create the hardware you actually want.  The choice usually boils down to which one hates the least.  But they're the only way in, so you're stuck with two ugly choices.

     

    3.  FPGAs ought to be a wonderful technology for high-performance reconfigurable compute engines, but the tools aren't up to the task: see this Geek Times article.  I talked about this last April in this element14 discussion:

     

    There was a lot of talk over the decades about FPGAs being used as reconfigurable compute engines.  This use has never really had any traction, and my hypothesis is that this hasn't occurred because FPGAs are too hard to design with using the current tools.  The tools are fine if you're designing a custom chip for a product and your other choice is ASIC.  But if your other choice is to wire up an array of high-performance microprocessors, the FPGA solution is too difficult.

     

    If FPGAs were open like many microprocessors, people who could solve this would work on it.  But given that any results will be "purely academic", the kind of people who want to see something actually working (e.g., all engineers) have no incentive even to start.  It's IMO truly a missed opportunity, but could be rectified at any time by an FPGA vendor if it chose to do so.

    4.  When I buy a chip, I'd like to be able to use it for whatever I want, rather than have "digital handcuffs" limiting what I can do with it.  Otherwise it's like buying a car and being told I can only buy gas from one particular vendor, I can only use the car to drive to certain approved destinations, and I can only get repairs from the dealer.  This a basic argument behind Free-as-in-Freedom (FaiF) or Free (Libre) Open Source Software (FLOSS).  If you think that what you're allowed to do with the products you buy should be left to the seller, that's your prerogative.  FaiF / FLOSS proponents think differently and advocate for this freedom.

     

    As to the question "why would I want to do it?", that's easy: because I think I can write better FPGA tools to address some of my needs than what I can buy or download from the vendors, and solving these kinds of problems is something I find passionately interesting.  As a proponent of open documentation and FaiF/FLOSS software, I'd want to share the result.  Most people wouldn't find this fun, but then not that many people find 16x16 Sudoku puzzles fun either.  I'll let Mr. Knightly from Jane Austen's Emma speak for me: "Very well. If the Westons think it worth while to be at all this trouble for a few hours of noisy entertainment, I have nothing to say against it, but that they shall not choose pleasures for me."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Very well presented and argued, John.  I agree in every respect.

     

    The day that you have a rudimentary open source tool that works with a specific programmable logic device, whichever that may be, I'll be very happy to buy the hardware and experiment with your code, and hopefully help you improve it.  It never hurts to have extra testers, and that's a very low barrier to entry for anyone wishing to support the development of open source EDA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    this is absolute rubbish,

    VHDL is both a simulation and design language the fact that you find it hard to use is not down to the language but down to your lack of understanding over how to use it correctly, if you have difficulty learning a tool the best way to understand it better is to practice using it. there is no demand for an open source FPGA design tool because nobody else has the issues that you state that you have,

    Ive been using Xilinx, altera and actel tool sets for donkeys years and Ive seen many attempts to rewrite VHDL into something simpler but they always fail due to the huge complexity of the task. The complexity of writting a VHDL synthesis tool capable of handling all devices from all vendors and covering all the VHDL functionality and verifying that it works correctly is stupendously large.I know for a fact that the latest synthesis tools from Xilinx for example took something in the region of 575 man years to write and verify,  and you get it for free..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I once had some idiot telling me that he wanted to rewrite XST because it couldnt handle the complexity of his code, puzzled I had a look at his code, the reason XST couldnt handle it was it written as if it was software and was full of aysncronous feedback loops so XST was spitting it out. He was a self proclaimed software genius.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    I'm a long term VHDl user but I'm currently forcing myself to use Verilog on a project in order to widen my horizons. There are a great many Verilog users and I doubt that the only reason that they don't use VHDL is prejudice or stupidity. By the same token it is obviously possible that a better solution than either VHDL or Verilog might be devised.

    It isn't necessary to leap right in and write a complete tool chain to make a contribution. One of the downsides of VHDL (and Verilog) is the number of mindless (but significant) lists of ports required to define and join up different components. There are several relatively simple tools you can use to manage or automate this process but I'm sure that better ones are possible.

    Starting from the other end is possible too - VHDL -> FPGA sysnthesis is very complicated but gate level -> FPGA could be quite simple. It was essential to get any performance out of Xilinx's first FPGAs with an 8 x 8 array of logic cells.

     

    The problem with the current situation, where the tools are almost all closed and locked to some degree to the silicon vendor, is that experimentation is usually directed towards gaining market advantage which is not always alligned that well with the long term. Having more competition and more lateral thinking in FPGA tool development would be a good thing.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    I'm a long term VHDl user but I'm currently forcing myself to use Verilog on a project in order to widen my horizons. There are a great many Verilog users and I doubt that the only reason that they don't use VHDL is prejudice or stupidity. By the same token it is obviously possible that a better solution than either VHDL or Verilog might be devised.

    It isn't necessary to leap right in and write a complete tool chain to make a contribution. One of the downsides of VHDL (and Verilog) is the number of mindless (but significant) lists of ports required to define and join up different components. There are several relatively simple tools you can use to manage or automate this process but I'm sure that better ones are possible.

    Starting from the other end is possible too - VHDL -> FPGA sysnthesis is very complicated but gate level -> FPGA could be quite simple. It was essential to get any performance out of Xilinx's first FPGAs with an 8 x 8 array of logic cells.

     

    The problem with the current situation, where the tools are almost all closed and locked to some degree to the silicon vendor, is that experimentation is usually directed towards gaining market advantage which is not always alligned that well with the long term. Having more competition and more lateral thinking in FPGA tool development would be a good thing.

     

    MK