Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Doing more with less: Raspberry Pi & Software Engineering
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 709 subscribers
  • Views 2916 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
  • raspberrypi
Related

Doing more with less: Raspberry Pi & Software Engineering

morgaine
morgaine over 14 years ago

Minimalism is a concept which hardware engineers embrace almost instinctively, but sadly in the world of software it's rarely even present in the vocabulary.

 

The emphasis in practical computing today is to ride upon the shoulders of giants by reusing the work of others, which is a terrific idea in principle but can be a disaster when applied without checks and balances.  It almost always results in cancerous growth of colossal monolithic applications, which is why so many software systems today are bloated beyond belief and become ever more flaky in proportion to their size, not to mention suffering from dependency hell.

 

We used to call this nightmare "The Software Crisis", the reason why "software bridges" collapse millions of times a day across the world, in contrast to the products of other branches of engineering where reliability is required, expected and achieved as a matter of course every day, not as the exception.  The Software Crisis is rarely mentioned anymore, because we have lost the war, surrendered to complexity, and have no solution in sight.  Software bridges continue to fall, ever faster.

 

How does this relate to Raspberry Pi?  Not very strongly, except in the sense that in software, "smaller is better".  256MB is such a huge amount of memory that if any significant part of it is used to hold the program code of a monolithic application then that application is in crisis, whether it's admitted or not.

 

There isn't really any solution to this problem available at the present time.  It would require a breakthrough in computing science to come up with a way of doing more with less, and then to force it upon a world which doesn't even realize that its pride and joy is actually an engineering disaster.  That's not going to happen any time soon.

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    Excellent post, Morgaine.  The only part I disagree with is your assertion that there isn't a solution at this time.  Sure, it's a hard sell since so many people believe that "more features" means better, and "more apps" means better, and "more complex" means better.  But I do read articles occasionally about "good enough computing" and how most people can easily get by with RasPi-like machine capabilities.

     

    I like to make an analogy with the RISC versus CISC argument of the 1980s.  (One of my favorite article titles of the time is from Electronics (5 May 1986): “RISC: Is it a Good Idea, or just another Hype?”)  In the 1980s transistors became so cheap you could afford to design computers with every instruction you always wanted.  However, those instructions were useless if the compiler couldn't take advantage of them, and their presence slowed down the performance of the instructions you really needed.

     

    I say software is similar: useless features clog the software with complexity, making the features you really need harder to use and learn.  I have a longer essay on the subject at http://code.google.com/p/xxicc/wiki/RSCwiki if you're interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    I liked your linked article a lot, John.  I can't find fault with any of it, and since I started my Unix days on a PDP-11/34, I both agree with your premises and also found your writeup very nostalgic.

     

    With regard to solutions for the Software Crisis, I guess it comes down to where one draws the finish line.  You've pointed out some directions that help reduce the speed of headlong rush towards the precipice, and I agree with them, but in the end the velocity vector is still towards it, just a little less quickly.

     

    And sadly there is no existing solution that could sway the current high priests of the software fraternity, who totally believe that they are on the true path of enlightment already.  To make matters even worse, there is no shortage of programmers who do what they do because it's fun and COOL, rather than for engineering reasons.  You can't argue against COOL, engineering disaster be damned.  It's one of the biggest problems of computing today --- programming is fun and creative, and as a result, serious engineering is almost entirely ignored.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

     

    you wrote:

    "256MB is such a huge amount of memory that if any significant part of it is used to hold the program code of a monolithic application then that application is in crisis, whether it's admitted or not."

     

    this is true, but beside the point.  Most linux applications aren't monolithic, and none that I know of are anywhere near 256MB of code, or even 10% of that.  But a lot of commonly used applications do often consume 256MB of memory as data.  For example, a web browser viewing a large page, or with several tabs open, or a word processor editing a large book, or a compiler compiling a large program.   It doesn't indicate that the application is needlessly monolithic, or bloated with needless features, or in any sort of crisis. 

     

    Modern applications are doing exactly what you want them to do, which is to keep their data in fast memory rather than paging it to slow disk.  With memory prices as low as they are, at only a few dollars per GB, and with just about every PC sold in the last 5 years having a 64-bit address space,  it makes no sense for applications to try to minimize memory usage.

     

    As you say, engineering is about minimalism, but the flip side of the coin is that engineering is about meeting requirements, and with adequate margins.  The minimum memory requirements for Debian, Fedora, Ubuntu, Android, etc., are all around 1GB.  Below that you will bump into the limits, often for reasons beyond your control, such as trying to view a large web page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    @coder27: I wasn't referring to amount of memory used to hold data, as that doesn't impact on program complexity.  After all, a one-line program can be designed to use arbitrary amounts of data, so there is no direct correlation between data memory used and program complexity.

     

    I'm certainly not suggesting that Pi's memory should be restricted --- in fact, in another thread I argued expressly against holding to 256MB as some people were proposing.  Here I'm referring only to program design and the software engineering of applications, so it can't be used as an argument for restricting data memory.

     

    While it's true that applications tend to be less monolithic in *nix than in Windows because of the Unix Tools legacy, that way of compositing larger applications out of many smaller and independent programs is almost completely unused today except in minor scripting.  The malaise of monolithic programming has crept into all operating systems, and it is now the completely standard way of working.

     

    I once tried to gain a programming community's interest in non-monolithic design for a 3D graphics client -- see this wiki page of mine: https://wiki.secondlife.com/wiki/Multi-Process_Client_VAG_--_draft .  It got nowhere, not because anyone argued against it, but because it's just not the standard way of doing things so there was no mental buy-in.  When the entire software industry is designing monolithic horrors and thinking that they're cool, you have to provide a lot more than just a conceptual framework to gain any interest at all.  For some reason that I find difficult to understand, people know that their huge monolithic programs are utterly bug-ridden and almost impossible to maintain, yet are not willing to do anything about the root cause of the problem.

     

    It must have something to do with the almost total lack of engineering mentality in the software community today, because engineers don't create things that way outside of software, no matter how complex they are.  If the space shuttle had been built as a monolithic unit, it would never have got off the ground because of complexity meltdown .

     

    Systems of that complexity are built out of innumerable smaller parts, each of which is completely independent and presents only a very narrow interface to external systems.  It goes far beyond mere object orientation and unit testing at development time:  hardware "units" continue to be independent even when put together into a whole, they don't lose their independence and observability when they are linked together.  Software does not really have the equivalent of that yet, although I know of some systems that come close.  The key difficulty isn't that the problem is hard, but that the problem has no recognition.

     

    You mentioned web browsers.  There could be no worse horror to illustrate what I'm saying. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    @coder27: I wasn't referring to amount of memory used to hold data, as that doesn't impact on program complexity.  After all, a one-line program can be designed to use arbitrary amounts of data, so there is no direct correlation between data memory used and program complexity.

     

    I'm certainly not suggesting that Pi's memory should be restricted --- in fact, in another thread I argued expressly against holding to 256MB as some people were proposing.  Here I'm referring only to program design and the software engineering of applications, so it can't be used as an argument for restricting data memory.

     

    While it's true that applications tend to be less monolithic in *nix than in Windows because of the Unix Tools legacy, that way of compositing larger applications out of many smaller and independent programs is almost completely unused today except in minor scripting.  The malaise of monolithic programming has crept into all operating systems, and it is now the completely standard way of working.

     

    I once tried to gain a programming community's interest in non-monolithic design for a 3D graphics client -- see this wiki page of mine: https://wiki.secondlife.com/wiki/Multi-Process_Client_VAG_--_draft .  It got nowhere, not because anyone argued against it, but because it's just not the standard way of doing things so there was no mental buy-in.  When the entire software industry is designing monolithic horrors and thinking that they're cool, you have to provide a lot more than just a conceptual framework to gain any interest at all.  For some reason that I find difficult to understand, people know that their huge monolithic programs are utterly bug-ridden and almost impossible to maintain, yet are not willing to do anything about the root cause of the problem.

     

    It must have something to do with the almost total lack of engineering mentality in the software community today, because engineers don't create things that way outside of software, no matter how complex they are.  If the space shuttle had been built as a monolithic unit, it would never have got off the ground because of complexity meltdown .

     

    Systems of that complexity are built out of innumerable smaller parts, each of which is completely independent and presents only a very narrow interface to external systems.  It goes far beyond mere object orientation and unit testing at development time:  hardware "units" continue to be independent even when put together into a whole, they don't lose their independence and observability when they are linked together.  Software does not really have the equivalent of that yet, although I know of some systems that come close.  The key difficulty isn't that the problem is hard, but that the problem has no recognition.

     

    You mentioned web browsers.  There could be no worse horror to illustrate what I'm saying. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    @Drew Fustini (admin): I'm conscious that we've accidentally strayed outside of the topic of Pete's thread.  It's probably not too bad yet, but if this discussion about software engineering continues too long, you might want to consider doing another split as you did for the FPGA topic.  Perhaps something like "Raspberry Pi and Software Engineering" might be an appropriate title.

     

    I guess it's Pete's call.  I hope he's not too annoyed with us yet, image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    I can branch if that would be helpful.  What do you think would be the best place as which to do so?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustiniadmin

    Probably starting at my #112 because coder27's preceding post was still very much on topic about expanding Pi memory.  It was me who went off at a tangent about software engineering.  (Sorry Pete. image)

     

    But I think the new topic may have died anyway, so might as well leave it for now unless more replies follow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine - your a mind reader (was travelling today and following the conversation and thought the same thing) - interesting discussion - but as you say we have gone a bit off topic and therefore a shame its buried in something that is titled differently.

     

    I would like to suggest that we try to keep this thread to things that people have found wrong with the Pi rather that the philosophy of programming. What the Pi could have been, rather than what actually would also be better in another thread but these work so well together I would leave them together if that is OK?  So I would cut earlier and title something like "Lack of Memory on the Pi?" and it would hopefully encourage people to read and comment.

     

    Never annoyed - it's a community thread - it is Drew's and the Admin's job to keep us in some sort of order.  image

     

    Off to eat some humble Raspberry Pi whilst I fix up the daft mistakes on the schematics, good job they are not on the board - V1.1 soon.

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    I went ahead and branched after seeing what Pete wrote, too.  I've manually set the language setting again to English to avoid that visibility problem which happened last time I branched a thread.  But the issue with the subject of individual replies not changing hasn't been fixed yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    @Pete: Haha, don't kick yourself, things of this complexity are improved iteratively, they're not born magically perfect.  Well at least mine aren't.  image

     

    @Drew: Many thanks for doing the deed.  Of course, now that it's split, the discussion is guaranteed to dry up. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

       Why aren't your complex products born magically perfect?

     

    In message 12 of thread:

    http://www.raspberrypi.org/forum/features-and-requests/interfaces-case-package-requestsuggestion

     

    Liz wrote:

     

    "I can absolutely assure you that we won't be shipping a product that still requires beta testing! What you'll see at the end of the year will be the finished, polished product. The reasons we"re having a hobbyist release first are basically dull old business reasons – we need some income to get the larger release of boards made, which we mean to raise by selling the first batch to…you lot, because we know the demand is there!"

     

    If the RPi can do it, you should be able too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

     

    You wrote:

    "If the space shuttle had been built as a monolithic unit, it would never have got off the ground because of complexity meltdown."

     

    Interestingly, the shuttle's solid rocket boosters perhaps should have been built as a monolithic unit, but instead were built in segments to facilitate transport.  But the poorly-designed segment joints caused the Challenger tragedy. Sometimes, the overhead involved in splitting up a monolithic design is not repaid in improved reliability.

     

    you wrote:

    "hardware "units" continue to be independent even when put together into a whole, they don't lose their independence and observability when they are linked together."

     

    I think you are referring to something like hardware chips on a pcb board not losing their independence.  But in other cases, like a SoC, the hardware components do essentially lose their independence, much like software components.

     

    While it is generally true both in hardware and software that cost and complexity grows exponentially with the size of a project,  this is largely due to increased interconnections between the parts.  It isn't necessarily true when simply aggregating together components that have well-defined interfaces, as is done with a SoC. 

     

    It used to be that Fortran programs had all their global variables declared in common statements, and complexity therefore grew exponentially with size.  But modern software can be designed in layers and modules with restricted visibility to other layers and modules, so complexity grows more linearly with size.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I've learned to ignore most of what comes from that particular source.  It's mostly highly decorative and self-congratulatory PR, regularly spinning the truth and faithful to the teachings of mushroom management.  But the straw that broke the camel's back for me was incitement of the fanbois against participants who ask inconvenient questions or voice any criticism.  What little credibility remained was destroyed utterly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    @coder27: It's partly true what you say about the components within SoCs losing their independence as hardware units.  This is what happens when hardware is "programmed" into shape rather than assembled from actual physically independent devices.

     

    However, it's not nearly as bad as what happens in software systems assembled out of classes and functions, because the  units in hardware are always static components with narrow interfaces, whereas software units are generally dynamic (even recursive) and very commonly have disastrously wide interfaces.  That results in a combinatorial explosion of complexity.

     

    Curiously, software should be easier to nail down tightly and monitor to any desired degree of granularity than hardware, because software is not bound by debug limitations such as pinout counts and limited cell numbers that restrict the ability of deeply embedded components in SoCs to be monitored effectively.  What's curious is that the relative ease of doing this monitoring in software does not lead to it actually being done, at least not as a matter of course.  Right across the industry, software validation is extraordinarily minimal.  As a freelance contractor I've seen the insides of a lot of companies, and this problem is universal.

     

    It truly is a crisis, and the fact that people consider it NORMAL nowadays that software will fail shows just how deep a crisis it has become.

     

    Morgaine.