Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Download Raspberry Pi OS query
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 706 subscribers
  • Views 2664 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • pi
  • raspberry_pi
  • raspberrypi
Related

Download Raspberry Pi OS query

e14 Contributor
e14 Contributor over 14 years ago
  1. Hi, I have just started to download its OS on another machine, is it really so that it takes more than 12hrs to download its operating software and if so is there anything that I should be aware off while downloading it.
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Unless you have a dial up internet connection, it should download in a few of minutes. A projected time of 12 hours means you have either a dial up connection, a clogged up internet provider, or have connected to a swamped server. The download will likely fail. Try another download method...do you have a bittorrent client?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Yeah thanks for that. It was also my suspicion of my internet connection and after only downloading 3% in around 3hrs of the 8GB + of software of around 48KB per second, I decided to cancel the download. Although as a rule I don’t normally have any length of time issues when downloading any other type of software. Strange. - I don’t have “bittorrent client” installed, do you think that will help. I feel that there maybe something wrong with my downloading procedure that is causing this extremely slow-speed issue. Thanks for responding to my query.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    Hi Violin, is there any chance you are downloading the VM of the Raspberry Pi to experiment on, rather than the OS to use on the Pi itself ?

     

    I know the VM is around 8 Gig, and I think is only hosted on a relatively low power server (s) - it is only the work of one person.

     

    If you want to download the OS for the RasPi itself, you should go here: http://www.raspberrypi.org/downloads

     

    These images are not that big, around 470 Meg.

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to GreenYamo

    Hi Steve and thanks, I did download this link raspberrypi-fedora-remix-14-r1.img.gz in which took only around 13 minutes to download, but in the end it came to “Windows can’t open file”, so I am now not sure in what is going on. - At this very moment in time I am a bit confused in what OS software I exactly need in conjunction with the Raspberry Pi and only hope that as time goes on my understanding will become much clearer with the functioning of this particular dev board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Violin,

      I think you will have better luck with the Debian Squeeze download:

    debian6-19-04-2012.zip

     

    Debian is in better shape than Fedora, and you may find that Windows

    has an easier time unpacking a .zip file than the Fedora .gz file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Violin,

      I think you will have better luck with the Debian Squeeze download:

    debian6-19-04-2012.zip

     

    Debian is in better shape than Fedora, and you may find that Windows

    has an easier time unpacking a .zip file than the Fedora .gz file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks coder27 for the download link suggestion and did download successfully but have absolutely no idea at this stage the connection with “Nero BackItUp & Burn Essentials/Nero Express" and Raspberry Pi dev board. I guess I was expecting some sort of Raspberry Pi GUI or IDE software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Steve for the SD card link. Am I right in assuming that this is the Raspberry Pi bootloader card software that needs to be installed into the Raspberry Pi dev board before anything can be done with it. I am thinking of taking the "Safest/Laziest way” route on this one when available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    Hello Violin, yes, you are correct in that the card needs to be installed in the Pi for it to do anything useful, or in fact *anything*

     

    From what I recall, there is a small amount of boot code on the Graphics chip, that then transfers control of the boot sequence to the SD card. From a PC perspective, you can think of the Bios as being the small boot code on the graphics chip, which then passes this work onto the hard drive, or in the case of the Pi, the SD Card.

     

    You cannot plug a Pi into a TV or Monitor without following one of the guides above to prepare and write a boot image to the SD card. This is also a strength of the system, as you can configure multiple cards to perform multiple actions, for example have one card for Debian and another for openElec or XBMC, which will turn the card into a media server. These are just two examples out of many possible and I suspect that when the Pi is available on demand, these applications will soon multiply. It also means a resilient system and if anything goes wrong, just re-image the SD card and your back on the road again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to GreenYamo

    Thanks Steve. I am starting to get a much clearer picture of this “Raspberry Pi” dev board in which I have ordered but not really knowing what it is that I have really ordered and am waiting for with much anticipation. - The pre-programmed SD card is a “media image” card slotted into the Raspberry Pi and can be influenced by a mouse and/or a keyboard peripheral/s to a computer monitor – or TV.

     

    - At the moment I am taking this posted link “debian6-19-04-2012.zip” as the software writer tool for SD media image card/s, but no media image software has been released as of yet so as to install/burn onto the SD card/s. The Raspberry Pi is a “stand-alone” development board without the requirement of a “PC” for any type operation, other than to write to the SD cards via download links, - hence the no need for any “PC” GUI or IDE, unlike what I am already used too with my long time prototyping with my type of dev boards via PCs. Please correct me if I am wrong with any of this. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    Hello Violin,

     

    The Rasp Pi is really a *very* small computer rather than a Dev board as such. The images used to boot are a port of Linux that is compiled to use the arm processor.

     

    Software has been released to install onto the SD cards, if you see my thrid post down, there is a link to the downloads page of the Foundation (http://www.raspberrypi.org/downloads. I think that you said you have already downlaoded one of those images. As Coder says above, you will probably have better luck with the Debian Squeeze download. Get that, use the Win32diskimager to write it to the card and you will be ready to go.

     

    You are correct in that once you have used a PC to burn the image to the SD card, there is no further need for a PC. You do not 'talk' to the Pi via a GUI or IDE, you connect it to a monitor, keyboard and mouse and you can program it directly. This can be via the command line, or through a GUI.

     

    Any Linux software that has been ported to use the arm processor you should also be able to use.

     

    Hope this helps.