Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Ethernet port turned off after few minutes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 713 subscribers
  • Views 4513 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • ethernet
  • port
  • raspberry_pi
  • raspberrypi
  • off
  • turned
Related

Ethernet port turned off after few minutes

e14 Contributor
e14 Contributor over 14 years ago

I am using 5V 1300mA adapter (http://www.skross.com/product/en/15/USB-Charger/56/World-USB-Charger.html) to power my Pi and another cheaper adapter that gives 5V 800mA.

 

The SD card is KINGSTON 16GB 100X SD10-HC.

 

I plugged in my Ethernet cable into the port and booted off Debian image from http://downloads.raspberrypi.org/images/debian/6/debian6-19-04-2012/debian6-19-04-2012.zip (SSH enabled). I am able to SSH into the Pi remotely and run basic commands, top, ps, ping. After about 15 minutes, the Ethernet LEDs just went off and my SSH session is gone too.

 

Checking the voltage at TP1 with my DMM it reads between 4.75 to 4.8V when the Ethernet is up and 4.9V when the Ethernet is down, i.e. the 3 LEDs marked FDX, LNK and 10M are off.

 

The same symptom is happening with both adapters. I have nothing else plugged into the Pi except the power and Ethernet cable.

 

Could this be another power problem? Anyone else seeing similar issue?

  • Sign in to reply
  • Cancel
  • xchris
    xchris over 14 years ago

    very strange! Is it from the 1st batch? Maybe this has something to do with the re-soldering process of the eth port....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to xchris

    How do I tell if it's first batch? I ordered a couple hours after launch on Feb/29 from element14 and received it May/7.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bodgy
    bodgy over 14 years ago in reply to e14 Contributor

    Look at the serial number it is in date time format.

     

    Off hand I can't recall my serial number (I'm at work at the moment), but there is a post by me here under Pi in Oz that lists my serial number and mine was in the second batch.

     

    OK at home now, as Coder27 says my ethernet jack isLU1S041ALF and the serial code is 2012-03-17 14:19

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Raspberry PiB,

       It sounds to me like a hardware problem, so I'd suggest contacting Farnell for a replacement.

    They have reportedly been very good about promptly replacing faulty units.

     

    Since you received yours on May 7, it would be from the second batch, so there is

    no reason to suspect it has a resoldered ethernet port.  The first batch was sent out

    around April 13, and the second batch around May 1.

     

    You can confirm it's from the second batch by looking for a CE mark sticker on the back.

    The first batch doesn't have that.  As bodgy noted, you can also check the manufacturing

    date encoded in the serial number on the back side.

     

    Also, the first batch has an ethernet jack made by Bothand, that says LU1S041A LF;

    in the second batch it's made by HanRun, and says HR901110A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Also, on the front side of the board, between the power connector and the SD card,

    the manufacturing date is apparently encoded, as 1208 for first batch, and 1213 for

    the second, indicating week 08 and week 13 of 2012, respectively.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=2&t=5889

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • xtramural
    xtramural over 14 years ago

    As someone else in possession of a Pi that seems to hang after a few minutes after booting I had initially considered that it might have a PSU issue but had ruled this out since I had tried a generic powered hub, a Belkin PSU rated at 5V 1A and a Nokia AC-10X rated at 5V 1200mA - all to no avail. WIth all three power PSUs the voltage across TP1 and TP2 seemed to be well within spec and other Pi owners seem to have had success with the likes of the Nokia charger.

     

    What I would really like to see is a definitive statement about the PSUs that are known to be good and/or official PSUs from Farnell that are guaranteed to work. As it is, I'm still unsure of whether or not my Pi woes are power-related and, if so, how I can really tell without the need to invest in bench supplies, test kit over and above a multimeter, etc.

     

    There's also a thread just started up at http://www.raspberrypi.org/phpBB3/viewtopic.php?f=6&t=5900 so you might want to add your voice about the issue over there so those of us suffering from the problem can compare notes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 14 years ago in reply to xtramural

    There is also speculation in the 'Hardware Flaws and Fixups' discussion on here regarding the power supplies.

     

    FWIW, I am using an HTC Desire charger, 5V 1amp and touch wood seems to be OK so far. I did have some booting problems where it just appeared dead, but updated to the latest debian image and that seemed to solve it for me (19th April Image I believe)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Mine should be the second batch then since it's using HanRun HR901110A and the manufacturing date on the board says 1213.  I will have to find the HTC charger to try it out and will report back if that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    If you want to experiment, another thing to try would be a different SD card. One thread on the Pi board here

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=6&t=5900&p=78495#p78495

    reports a temperature sensitivity (will not reboot when hot, but reboots OK if kept cool with a fan). This may occur with specific SD cards (not yet confirmed).  If you have a fan, could try running the fan over the Pi also. If that fixes the problem it would be very interesting to say the least.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    So I tried HTC One X charger rated at 5V 1A but the Ethernet still shuts down after less than 5 minutes. I was able to SSH in before it went down though. I have sent RMA to element14 and they will be picking my unit up tomorrow for inspection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>