Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum HDMI resolution problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 706 subscribers
  • Views 3572 views
  • Users 0 members are here
  • hdmi
  • raspberry_pi
Related

HDMI resolution problem

e14 Contributor
e14 Contributor over 14 years ago

Hi, I've just taken delivery of my Raspberry Pi. I loaded up Debian, hooked it up to my TV via the HDMI connection but the edge of the screen overlaps the screen size. I cannot see the task bar or menu buttons. How can I fix this?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 14 years ago

    Instuctions for others who may be experiencing the same issue with a TV and the Raspberry Pi:

    1. Install a fresh image

    2. start-up the Raspberry Pi and let it set itself up (normal set-up)

    3. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_drive=2 " [exactly as it is here]

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    4. Restart using the command: " sudo shutdown -r now "

     

    That gets the Raspberry Pi to register the TV as a HDMI device. You now have sound! For different resolution:

    5. After you have gone through normal set-up:

    a. Log-in as a normal user (debian image: pi)

    b. Type the command: "sudo nano /boot/config.txt "

    c. Press enter

    d. Type in: "hdmi_group=1 " [exactly as it is here]

    Press Enter

    Type : "hdmi_mode=x " where x = corresponding number of resolution mode. See: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=5851

    e. Then press crtl + o

    f. Press Enter

    g. then press crtl + x

    6. Restart using the command: " sudo shutdown -r now "

     

    Now you have desired resolution and Sound!!!

     

    Happy Raspberry Pi...ing

     

    I hope this solves your problems

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Hi,

     

    I've just tried this. I set hdmi_group=1 and hdmi_mode=19 but that had no effect. I then tried hdmi_goup=2 and hdmi_mode=0x8 but that killed it and I had to start again with a new image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Hi,

     

    I've just tried this. I set hdmi_group=1 and hdmi_mode=19 but that had no effect. I then tried hdmi_goup=2 and hdmi_mode=0x8 but that killed it and I had to start again with a new image.