Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum HDMI resolution problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 706 subscribers
  • Views 3572 views
  • Users 0 members are here
  • hdmi
  • raspberry_pi
Related

HDMI resolution problem

e14 Contributor
e14 Contributor over 14 years ago

Hi, I've just taken delivery of my Raspberry Pi. I loaded up Debian, hooked it up to my TV via the HDMI connection but the edge of the screen overlaps the screen size. I cannot see the task bar or menu buttons. How can I fix this?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Maybe I could change the settings on the TV but there are no options that I can find to do so. Does anyone know anything about Panasonic Viera's?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Kev,

     

    Also: Can you tell us if your TV is registred as a DVI device or HDMI device?  If yes, then follow the instuctions I posted above.  If no, then you might not be putting in the right commands or putting them in wrong.  All commands DO NOT have spaces.

     

    Then:

     

    You have to check whether or not your TV supports that resoultion.

     

    See this link on how to do that:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=5&t=5851

    1. Run “tvservice –m CEA” to give a list of CEA supported modes.

     

    To do this, you must first change your directory to: /opt/vc/bin  (to do this enter command in terminal: "cd /opt/vc/bin")

    then type: "tvservice –m CEA" (or ./tvservice –m CEA if it doesn't work)

    then the Raspberry Pi will show a list of supported formats.  Use http://www.raspberrypi.org/phpBB3/viewtopic.php?f=5&t=5851 to get the commands of the supported format. Once you find the supported formats,

     

     

     

    Fergus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Thanks for the reply Fergus. I followed your instructions and found that mode 19 is supported (at least I think it is, the left of the screen is not visible so all I can see is:

     

              mode 1: 640x480 @60Hz, progressive

              mode 2: 720x480 @60Hz, progressive

              mode 3: 640x480 @60Hz, progressive

    ative)  mode 4: 1280x720 @60Hz, progressive

              mode 5: 1920x1080 @60Hz, progressive

              mode 6: 720x480 @60Hz, progressive

              mode 7: 720x480 @60Hz, progressive

              mode 17: 720x576 @50Hz, progressive

              mode 18: 720x576 @50Hz, progressive

    ative)  mode 19: 1280x720 @50Hz, progressive

              mode 20: 1920x1080 @60Hz, progressive

              mode 21: 720x576 @50Hz, progressive

              mode 22: 720x576 @50Hz, progressive

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Thanks for the reply Fergus. I followed your instructions and found that mode 19 is supported (at least I think it is, the left of the screen is not visible so all I can see is:

     

              mode 1: 640x480 @60Hz, progressive

              mode 2: 720x480 @60Hz, progressive

              mode 3: 640x480 @60Hz, progressive

    ative)  mode 4: 1280x720 @60Hz, progressive

              mode 5: 1920x1080 @60Hz, progressive

              mode 6: 720x480 @60Hz, progressive

              mode 7: 720x480 @60Hz, progressive

              mode 17: 720x576 @50Hz, progressive

              mode 18: 720x576 @50Hz, progressive

    ative)  mode 19: 1280x720 @50Hz, progressive

              mode 20: 1920x1080 @60Hz, progressive

              mode 21: 720x576 @50Hz, progressive

              mode 22: 720x576 @50Hz, progressive